Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog LCR 4-Wire Kelvin Adapter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 6 Feb 2021 2:11 AM Date Created
  • Views 7913 views
  • Likes 8 likes
  • Comments 9 comments
  • lcr
  • multicomp pro lcr
  • kelvin measurement
  • kelvin clamps
  • multicomp pro
  • measurement
  • 4-wire
Related
Recommended

LCR 4-Wire Kelvin Adapter

fmilburn
fmilburn
6 Feb 2021

This is a follow-up to my review of the Multicomp Pro Handheld LCR MeterMulticomp Pro Handheld LCR Meter.  In that review it was noted that the meter does not come with Kelvin clamps and that the manufacturer did not appear to offer them.  In this post I describe a set of DIY Kelvin clamps.

image

Thanks to Shabaz and Jan Cumps for the design suggestions in the comments of the original post.

 

Design Features

 

The design consists of a PCB for adapting the Kelvin clamps to the LCR meter and a 3D printed enclosure.

 

PCB Design

image

  • ENIG finish
  • 4-Wire connection of clamps
  • Guard connections for shielded cable
  • Connections on bottom of PCB, Faraday shield on top with stitching to bottom
  • Openings for zip-ties for strain relief
  • 4-wire connection footprint allows 0603 and larger parts to be soldered directly to the PCB for testing
  • Designed so that adapter cannot be inserted incorrectly

 

The Multicomp Pro Handheld LCR is a rebranded Hantek 1833C meter.  Because the "fingers" that attach the adapter to the LCR vary from instrument to instrument this adapter may not fit other LCR models.  The PCB was fabricated by OshPark and the Gerber files can be found here.  The cost for 3 is approximately $16 including shipping if ordered from OshPark.

 

Kelvin Clamps

 

image

 

There is a very good post by Shabaz on how to build your own Kelvin (4-Wire) Test Leads that can be found here.  I bought a shielded pair with BNC connections off of Amazon for $13 (with a coupon) and was surprised to find they were well shielded and the core wire of a decent diameter.  The clamps themselves are OK for the use I will give them but not of professional quality.  The BNC connections were removed and the leads were cut to 40 cm and soldered onto the PCB.

 

I recommend soldering the shielding to the guard footprints first.  Be careful as the connections are close together and test for undesired shorts between connections after soldering.

 

Enclosure

 

{gallery} Enclosure

image

Bottom

image

PCB

image

Top

image

 

  • Print consists of two parts, top and bottom.
  • Requires two 3mm bolts and threaded inserts.
  • Bolts are inserted into a recess in the bottom, must be cut to approximately 18 mm in length

 

The enclosure was designed with Fusion 360 and the STL files can be found here for those who would like to print it.  The closest bolt length I had at hand was too long so they were cut to length.  Threaded inserts were used to allow multiple opening and closing of the enclosure but threaded screws could be used if that is not required.

 

Completed Project

 

image

 

The project looks and works well.  If this was something that was to be done on a larger scale the enclosure could be modified for a 20 mm long bolt (which I did not have on hand) but otherwise there isn't much I would change for now.  Comments and suggestions are always welcome.

 

Associated Post

 

Quick Review: Multicomp Pro Handheld LCR Meter

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago in reply to fmilburn +5
    ... I think I will try and make some tweezers next. They may not be 4-wire though. Mine relies on the flex of the plastic for the flex action. There are no hinges or springs: The little plastic lips on…
  • fmilburn
    fmilburn over 5 years ago in reply to genebren +4
    genebren wrote: I have a client that builds Kelvin probe sets for older model HP meters and sells them ebay for ~$250.00, so there might be a great business opportunity for you in the probe business. Too…
  • Andrew J
    Andrew J over 5 years ago +4
    Great job Frank. I think tweezers would be good for small SMD parts.
Parents
  • Andrew J
    Andrew J over 5 years ago

    Great job Frank.  I think tweezers would be good for small SMD parts.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Andrew J
    Andrew J over 5 years ago

    Great job Frank.  I think tweezers would be good for small SMD parts.

    • Cancel
    • Vote Up +4 Vote Down