Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog Precision analog opto-isolation amplifier using HCNR200/201
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mahmood.hassan
  • Date Created: 4 Oct 2018 3:04 PM Date Created
  • Views 8237 views
  • Likes 6 likes
  • Comments 4 comments
  • analog opto-isolated
  • backtoanalogch
  • current sense measurements
  • smps
  • precision amplifiers
  • voltage measurement
  • opto-isolated
  • optocouplers
  • diytestinstruch
Related
Recommended

Precision analog opto-isolation amplifier using HCNR200/201

mahmood.hassan
mahmood.hassan
4 Oct 2018
image

Test Instrumentation

Enter Your Electronics & Design Project for a chance to win a Grand Prize for Originality, a Tool Set, and a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

We can easily find many types of digital optocouplers but its very rare to see any analog optocoupler application especially in hobby electronics. Even though its very essential in many type of analog circuits especially in current and voltage monitoring/measuring circuits where input and output side should have isolation. If someone is measuring/monitoring the high DC voltages or current ,and its also driving inductive loads, then it can easily damage MCU or any other measuring hardware. To solve this sort of problems analog optocouplers are used.

Here I am sharing circuit of one of analog optocoupler using easily available components.

 

BOM

ICs:

1 x HCNR200 or HCNR201

2 x LT1097 (or any other good op-amp)

Transistor:

1 x 2N3906 (or any other compatible PNP transistor)

Diode:

1 x 1N4150 (or any other compatible diode)

Capacitors:

2 x 10uF (optional)

4 x 0.1uF

1 x 47pF

1 x 33pF

Resistors:

1 x 50k pot

2 x 10k pot (optional)

1 x 200k ±1

1 x 174k ±1

1 x 33k

1 x 6.8k

1 x 2.2k

1 x 270R

 

Testing procedure

Apply ± 5/10/12/15V supply to both input and output side op-amps. It can work with wide range of dc supply but for that;

minimum supply voltage > (maximum input signal voltage + (op-amp supply - maximum op-amp output voltage for that supply))

 

For LT1097;

minimum supply voltage  > (maximum input signal voltage + 1.2V)

After applying separate power supply to both op-amps (for example ±15V) apply constant voltage (0≤ VIN ≤13.8) at VIN terminal. Now test the voltage at VOUT terminal the voltage should be equal to input voltage or use VR1 to make it equal to input. Similarly test it for different input voltages.

 

Circuit shown in FIG. 1 & 3 is unity gain circuit which mean output voltage will be equal to input voltage.

It only work with positive input voltages (VIN ≥ 0) regardless of single or dual supply of ap-amp.

All the resistors used in this circuit are with ±1% tolerance.

This circuit is also tested using lm741, lm358 dual op-amp IC and it worked well.

 

Applications

  • Low cost analog isolation
  • SMPS feedback loop, SMPS feedforward
  • Monitor motor supply voltage

.

.

.

.

.

image

FIG. 1: Schematic

 

image

FIG. 2: PCB Layout

.

.

.

image

FIG. 3: Circuit Source (HCNR200/201 datasheet)

Circuit Testing and Demo videos: tinyMonster - Analog Precision opto-isolator

Attachments:
imageHCNR200_201.pdf
imageLT1097f.pdf
  • Sign in to reply
Parents
  • clow006
    clow006 over 6 years ago

    Hi Hassan,

     

    I am working on a university project and came across your post.

    I would like to try out the octocoupler you designed.

    Possible to get the Eagle file from you?

     

    Best regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clow006
    clow006 over 6 years ago

    Hi Hassan,

     

    I am working on a university project and came across your post.

    I would like to try out the octocoupler you designed.

    Possible to get the Eagle file from you?

     

    Best regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mahmood.hassan
    mahmood.hassan over 6 years ago in reply to clow006

    tinyMonster - Analog Precision opto-isolator

    Details are available here.

    And I used the circuit given in HCNR datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clow006
    clow006 over 6 years ago in reply to mahmood.hassan

    Noted. Thanks!