Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog Project PITS
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: three-phase
  • Date Created: 13 Nov 2018 7:50 PM Date Created
  • Views 3812 views
  • Likes 10 likes
  • Comments 9 comments
  • mcgg relay
  • photodiode
  • current pickup
  • comparator
  • scits
  • diytestinstruch
Related
Recommended

Project PITS

three-phase
three-phase
13 Nov 2018
image

Test Instrumentation

Enter Your Electronics & Design Project for a chance to win a Grand Prize for Originality, a Tool Set, and a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Introduction

 

PITS is a Pickup Indicator Test System I am developing for use with injection test sets on older electronic analogue designed protection relays. This concept is not original, Omicron have such a product for use with their test set. The unit is very expensive and to my knowledge can only be used on Omicron test sets. Megger do not offer a pickup indicator detector for their test sets.

 

image

 

This version I am building, I intend to make universal so that it will function with both the Omicron and Megger test sets.

 

Protection Relays

 

The MIDOS MCGG relay is a standard overcorrect protection relay installed throughout the 1980s and 90s. They are available in a variety of formats from single phase units to a three phase and earth format that I will be demonstrating the PITS with.

 

It succeeded the old style electromechanical relays such as the Alstom CDG, but is itself now superseded by multifunction digital designs like the Micom series and more lately by numerical multifunction designs like the Multilin series by GE, that are a fully microprocessor design.

 

imageimage

Back to the MCGG relay. Each phase and earth fault element are set in exactly the same manner using the column of dip-switches assigned to it. The status of the elements is shown by the bank of LEDs above the dip-switches.

 

The top eight dip switches define how much current is required for the relay to detect an over-current defined as the pickup current, Is. This is a ratio of the current rating of the relay, this rating will be either 1A or 5A, for my relay it is 1A as stated on the relay nameplate.

 

The value of the dip-switches is added up and multiplied by the current rating. In my case, the dip-switches add up to 1 (0.1 + 0.1 + 0.8), so Is the pickup current is 1 x 1A, which equals 1A.

 

The manufacturer permits a +10% tolerance to this pickup level, so the relay would be expected to pickup between 1A and 1.1A. This is indicated by the bottom, green LED for the relevant element to light up, identified as I>Is.

 

The next three dip-switches, coloured black, define the trip curve for the timing function of the relay. The basic trip curves are defined in the IEC 947 standard, Standard Inverse (SI), Very Inverse (VI), Extremely Inverse (EI) or Long Term Inverse (LTI). The basic trip curve works in conjunction with the six blue dip-switches below them, that defines the time multiple, in terms of Is to be applied to the trip curve.

 

Alternatively the trip curve dip-switches can be set to a definite time function of 2, 4 or 8 seconds (D2, D4 and D8 respectively). With a definite time function set, the time multiple has no effect.

 

So my relay is set to 0-1-0 which selects the Extremely Inverse Curve. The time multiple is set to 0.325. So, if I inject 5A into the relay, I can read off the nominal trip time on the Extremely Inverse plot in the graph as about 3.25 seconds. To get the actual operating time, I multiply this by the TMS setting of 0.325. So the relay should trip after 1.09s +/- 9.5% for an EI curve as defined by the manufacturer.

 

image

 

When the input current exceeds the combination of the trip curve and time multiple, the middle LED, t, is lit and a contact is closed on the back of the relay and the feeding breaker is tripped open.

 

The final lower bank of dip-switches, separated from the upper column, set the instantaneous trip function of the relay. This is set as multiples of Is from 1 to 31, or set to infinity to turn the function off.

 

If this value is exceeded, then the top LED for the element, INST, is turned on and a separate contact of the relay is closed, that can be used to trip open the feeding breaker. The manufacturer specifies the instantaneous trip as a maximum of 35ms.

 

On my relay, the instantaneous element is set to 24 (8 + 16). So at 24 times the Is setting of 1A, i.e. 24A, the relay will trip under 35ms.

 

Injection Testing Concept

 

image

 

An injection test set will inject a chosen current into the input circuit of the element and wait for a trip response coming back from the relay.

 

The test set then records the current applied and the operating time, so it can be verified that these match the specifications provided by the manufacturer.

 

Testing the delayed trip and the instantaneous trip times is therefore easy as each of these operate a contact that can be fed into the test set.

 

As the pickup setting only operates an LED, then I use a manually operated switch to signal to the test set when the relay has picked up and dropped off.

 

To do this means I have to slow the ramp rate down, to give me time to react  and operate the switch. There can also be issues if the switch contacts bounce and the drop-off current is missed, meaning that the test has to be repeated.

 

This doesn’t affect the testing an individual relay to any great extent, but when faced with a switchboard containing 30 relays, the extra time taken starts to add up.

 

The intention of PITS, is to detect the operation of the pickup LED and feed it back into the test set. This will remove the possibility of contact bounce from affecting the testing and allow me to speed up the ramp rates to reduce testing time.

 

PITS Requirements

 

The design requirements for PITS are as follows;

                    1. Compatible with different manufacturer’s test sets
                    2. High speed operation - less then 100us
                    3. Volt free contact output to test set - up to 24V DC
                    4. Remove contact bounce
                    5. Battery operated
                    6. Interchangeable mounting for LED pickup

 

1. Making the unit operate form its own source and having a volt free output contact, will make the unit independent of the injection test set so that it can be used on different test sets.

 

2. Most test sets can time down to 1ms, therefore the unit will need to transfer the LED signal faster than this to ensure that test results are not affected.

 

3. Setting a test set to detect a volt free contact initiates the test set to source a voltage for the contacts. The default setting for this voltage is 24V DC on the test sets available to me.

4. Instead of using a relay for the output, which would be compatible with multiple voltage levels, but potentially introduce contact bounce, I intend to utilise a MOSFET to provide the output signal.

 

5. Whilst testing, there is generally mains power available around the switchgear and protection panels. However, at least two sockets are already required, one for the test set and another for the  laptop. My preference is for a battery operated unit to reduce the reliance on mains. Initially an18650 cell would be my choice, therefore voltage control and a charging circuit will also be required.

 

6. MCGG relays have a steel front, therefore mounting of the LED detector should easily be achieved using magnets. Other types of relays have either aluminium of plastic front faces. Therefore, I plan to make the LED detector pluggable to allow it to be swapped out for different mounting arrangements.

 

Initial Design

 

Detection of the LED will be achieved by a simple comparator circuit that is triggered by a photodiode mounted infant of the LED on the relay. To mount the photodiode, I have some donut magnets that go around the LEDs, the photodiode can then be mounted onto the back of the magnet using some rubber tap washers.

 

image

 

The initial photodiode used was an S5972 from Hamamatsu. At that point in time, I hadn’t really appreciated that the physical size of a photodiode affected its sensitivity and the diodes differed in the light wavelengths they responded best to.

 

Using the S5972, I never really achieved stability in the detection circuit. When the resistor network for the comparator was adjusted to achieve a level at which the circuit would detect the green LED, the circuit was so sensitive, it would operate at the normal illumination levels found within switch rooms.

 

A test with the S5972 against the relay whilst just measuring the photodiode resistance showed the level of instability. Against a green LED, the photodiode was reading around 50MOhms and stayed open circuit on some LEDs. In comparison, the photodiode dropped to between 2.2 and 6.5MOhms when against a red LED.

{gallery} My Gallery Title

image

Green LED Test

image

Red LED Test

Deciding that this was one of my issues, I swapped to using an SLD-70BG2 photodiode from Silonex and achieved much better results with the resistance tests.

 

image

 

The table below identifies the main specifications of each of the photodiodes.

 

Parameter

Hamamatsu S5972

Silonex SLD-70BG2

Spectral range

320 to 1000nm

400 to 700nm

Maximum sensitivity

800nm

550nm

Active area

0.5 sq. mm

9.8 sq. mm

Rise time

2ns

4us

Junction capacitance

3pF

180pF

 

The next issue to overcome was the relatively high resistance across the MOSFET  of 780 Ohms when the comparator switched on.

 

Assistance was provided by Rod to increase the pull down resistor value on the MOSFET to increase the Vgs voltage and cause the MOSFET to conduct more. The IRF510 I had chosen needed a Vgs of 10V to turn it on fully which the comparator circuit could not achieve only operating from a 5V supply.

 

Switching the resistor up to 980kOhms reduced the on resistance of the MOSFET down to 22Ohms. The binary inputs of test sets are very low burden, so although not quite right, the 22Ohms resistance is adequate for my application.

 

By this time I had added an LED indication to the circuit to show when the comparator had switched over, as my mounting method of the photodiode obscured the LED on the relay. I attempted to use the opposite output of the comparator chip to do this and managed to break the circuit and stop it from working completely.

 

Jon came to the rescue identifying that I had connected up the pnp transistor incorrectly, and offered an alternative circuit. With this implemented, the detection circuit was back up and running with the added benefit of the MOSFET resistance now being dropped further to 1.3Ohms.

 

 

Many thanks to 14rhb and jc2048 for their assistance, the full discussion can be found at;

 

https://www.element14.com/community/thread/65315/l/project-pits-problem

 

Prototype Circuit

 

 

The prototype was built up on veroboard ready to be tested against the relay and test set.

 

image

Due to my limited selection of components, some of the resistor values were fudged and are not quite the values stated in the schematic.

 

Initially, the output to the test set is connected through 4mm safety sockets to take standard test leads and the photodiode is connected to the circuit via a 2.1mm DC power plug and socket.

 

The circuit is a basic comparator. The reference voltage on pin 2 is set by R2 and R3, with RV1 providing an element of adjustment, although with the current setup, this is no longer required.

 

R1 provides the pull up for the photodiode, so that pin 3 is at 5V when the photodiode is off. When the photodiode detects light, its resistance drops and the voltage at pin 3 of the comparator goes below pin 2 and turns the output on.

 

The output of the comparator drives the gate voltage for the MOSFET. On advice, R5 value has been raised tp give a higher gate voltage to the MOSFET.

 

The opposite output of the comparator is used to sink the current for the transistor base and light the LED.

 

 

imageimage

 

A video of the prototype at work compared with the way I currently carry out a pickup current test using a manual switch into the test set.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Current BOM

 

This is the list of the current parts used in the prototype board.

 

Item

Quantity

Farnell Part Number

Price

AD8561 Comparator

1

9603867

£4.85

10k Potentiometer

1

1141404

£1.42

270R 250mW 5% Resistor

1

9339353

£0.0205

620R 250mW 5% Resistor

1

9342109

£0.0325

100k 250mW 5% Resistor

1

9339078

£0.024

150k 250mW 5% Resistor

1

9339205

£0.0208

300k 250mW 5% Resistor

1

9341714

£0.0313

1M 250mW 5% Resistor

1

9339086

£0.023

2N39052N3905Transistor

1

1357340

£0.176

IRF510 MOSFET

1

1653658

£0.583

5mm Red LED

1

1855506

£0.179

SLD-70 BG2A Photodiode

1

1219006

£6.66

Donut Magnet

1

———

£7.16

Tap Washer

2

———

£1.55

2.1mm DC Jack

1

2353931

£1.42

2.1mm DC Plug

1

2455456

£1.42

4mm Socket Black

1

1011401

£2.52

4mm Socket Blue

1

1011403

£2.95

Verobaord 122x102mm

1

1536938

£5.57

 

Total for Prototype

£36.61

 

As the project progresses, the number of parts and costs will rise, but I can't see me hitting the price of a unit from Omicron for quite some time.

 

Work in Progress

 

I have played a bit with KiCad to produce a PCB, the original one made before the modification to the transistor / LED circuit seems to have come out reasonably well. This will now have to be redone following on from the circuit modifications.

 


imageimage

 

Currently I am struggling to import the PCB outline, kindly supplied by Hammond, into KiCad, so that I can make the most use of the case layout. The outline was being pulled into KiCad approximately 10% larger than the actual sizes when measured with the dimensioning tool.

 

Originally, I thought this was a problem with KiCad, but today I opened the file at work in DWG Viewer and used its dimension tool and measured the same 10% difference. Looks like I will need to draw it out myself and export to DXF format.

 

I also need to build up a couple more holders for the photodiodes. One will be a horizontal support bar for a photodiode across each element of the relay. Another will be supported off a suction cup for mounting onto relays with plastic housings. I have yet to find all the parts for this.

 

Obviously, to utilise PITS out in field works, it will need a case. Unfortunately, I have done my usual trick of selecting a case that might be a bit too small for the project.

 

image

 

I have an 18650 cell and a charging board with built in DC booster to provide the 5V supply. The on/off switch is a momentary switch to match the case, so unless I find a latching switch, I will need to construct a latching circuit to use with it. This would be another little learning opportunity for me, so I may just stick with the momentary switch.

 

Depending on space, I may combine the output and photodiode connections into one multi-way connector, or drop the output down to 2mm sockets.

 

I had purchased a 2 pin socket with a plug and lead for the sensors to provide a more robust solution. I also like the availability of a protective cap for the socket when it is not in use. As with the other items though, this puts pressure on the case size.

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 7 years ago +6
    Donald, You are a genius, this is a great project (and well written up ). I'm assuming you are an electrical engineer by trade (I cannot imagine anyone would start looking at measuring the accuracy of…
  • genebren
    genebren over 7 years ago +5
    Donald, I really like the cleverness of your design (especially the magnetic holders for the photodiode). I looks like you have worked out (with the help of some community members, yeah!) a lot of the…
  • shabaz
    shabaz over 7 years ago +4
    Hi Donald, Very interesting project! It has uses beyond your scenario too - there could be many instances where legacy machines with indicators need to be integrated into some system. Excellent project…
Parents
  • three-phase
    three-phase over 7 years ago

    LibreCAD has come to the rescue. With this I have managed to create an outline of the PCB to maximise the space within the Hammond case. Compared to the other CAD packages I have used, it wasn't the most intuitive, but will a little help from the forum, a couple of hours saw a reasonable result.

     

    A 10uF decoupling capacitor has been added close to the supply pin of the comparator as detailed in the datasheet and recommended by jc2048.

     

    I also put a cutout in the PCB where I aim to fit the single 18650 cell. I have obtained some Keystone 590 battery clips that will provide the connection from the PCB onto the cell. I am yet to create the footprint for these for the PCB, so they currently aren't on board.

     

    image

     

    The circuit has been updated to include a latching circuit courtesy of EEVblog #262 or on youtube. This circuit is untested, I had ordered the parts, but UPS seemed to only deliver half the order last week and left the rest in transit, better luck this week.

     

    I have left an area at each end of the PCB unpopulated so that I can install the connectors at one end and the battery charger and boost circuit board at the other. However, I feel the the soft latch circuit should come between the battery charger and the boost circuit to allow the unit to be charged whilst switched off. This means, I will not be able to use the pre-built board, so I am now looking at building the circuits onto the PCB using the MC34063A for the boost circuit and the MCP73831 for the charging circuit.

     

    Updated PCB - needs battery clips adding, but the shape is good;

    image

     

    Updated schematic;

    image

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to three-phase

    Hi Donald,

     

    That's a really nice looking design! Neat idea to have a push-switch. When I used that style of enclosure, I'd ended up putting a slide-switch on the side, but the switch ended up being very flush, because of the thickness of the case : (

     

    I've not checked the video, and wasn't sure how the on/off capability worked (will the supply rail on the right side be connected to something?), but for a known working circuit, there is this Maxim partMaxim part. But, it's surface-mount (but a large SOT-23-6). It may look odd if the rest of the circuit is through-hole.

     

    That 590 clip is really good, I used it on a 'smart doorbell' project, but I made a mistake on the positive contact side.. I forgot to remove the ground plane on the side of the clip. There is just thin solder resist protecting it from shorting : ( so when you come to do yours, hopefully you won't make the same mistake I made!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to shabaz

    That's quite an interesting device and would save a bit of space if it comes to a crunch. The boost circuit is also a surface mount device and I may look to move the MOSFETs to surface mount, if I start to struggle for space.

     

    My alternative would be to have a second PCB mounted in the opposite half of the case.

     

    Thanks for the heads up on the battery clip, I will watch out for that when I get the footprint drawn out.

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 7 years ago in reply to shabaz

    That's quite an interesting device and would save a bit of space if it comes to a crunch. The boost circuit is also a surface mount device and I may look to move the MOSFETs to surface mount, if I start to struggle for space.

     

    My alternative would be to have a second PCB mounted in the opposite half of the case.

     

    Thanks for the heads up on the battery clip, I will watch out for that when I get the footprint drawn out.

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down