Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Forum Project PITS Problem
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 10 answers
  • Subscribers 20 subscribers
  • Views 4045 views
  • Users 0 members are here
  • current pickup
  • comparator
  • scits
Related

Project PITS Problem

three-phase
three-phase over 7 years ago

I have been trying to build up a Pick-up Indicator Test System (PITS) to detect the overcurrent indicator on protection relays I test, for the project14 test instrumentation.

 

Once  I figured out that there are some photo diodes that respond better to green LEDs than others, I managed to get the circuit working. However, I then decided to add an output indicator off the negated output of the AD8561 comparator chip I was using. After adding this, both outputs of the comparator remain low and the LED is on all of the time.

 

When I drop out R6, the 10k resistor to the pnp transistor base, the circuit starts to work again.

 

Anybody have any ideas what I am doing wrong? The only thing I can think of doing is to increase the size of R6, I had originally calculated this as 14k for a 1mA base current, but from my limited selection, 10k was the closest I had.

 

I also find that when turned on, the MOSFET has a resistance of 780 ohms, which seems a little high to me?

 

image

 

image

 

Kind regards

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 7 years ago +9 verified
    Your transistor is upside down - you've got the collector and emitter swapped. A transistor will work like that, but the gain is very much less than if you use it the right way round so you'd only ever…
  • Dudley
    Dudley over 7 years ago in reply to dougw +5 suggested
    better now?
  • three-phase
    three-phase over 7 years ago in reply to 14rhb +4 suggested
    Hello Rod, Many thanks for your help. I have read through the data sheet for the AD8561 and it does not say much about the outputs and if they are differential or inverse from one another. I have just…
Parents
  • dougw
    0 dougw over 7 years ago

    I would flip Q2 (emitter to +5).

    That opamp may not drive high enough to fully turn on the FET.

    Switching R5 to be a pull-up instead of a pull down should help, but it may need to be adjusted to get the optimum thresholds.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 7 years ago

    I would flip Q2 (emitter to +5).

    That opamp may not drive high enough to fully turn on the FET.

    Switching R5 to be a pull-up instead of a pull down should help, but it may need to be adjusted to get the optimum thresholds.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • three-phase
    0 three-phase over 7 years ago in reply to dougw

    Thans for the suggestion Doug, playing about with the circuit given to me by Jon has brought the gate voltage up to 4.51V, so I don't think I need to convert to a pull up resistor, but is still useful to know.

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down