The Holiday Special
  • Challenges & Projects
  • Project14
  • The Holiday Special
  • More
  • Cancel
The Holiday Special
Blog FLiP Connected X-Mas Ornament
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Holiday Special to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 18 Dec 2017 2:32 AM Date Created
  • Views 1566 views
  • Likes 3 likes
  • Comments 1 comment
  • x-mas ornament
  • bluez
  • parallax flip
  • raspberry pi
  • ws2812b
  • holidayspecialch
  • hc-05
Related
Recommended

FLiP Connected X-Mas Ornament

jomoenginer
jomoenginer
18 Dec 2017

image

The Holiday Special

Enter Your Project for a chance to win $100 Shopping Carts, Gifts to Give, and a 3D Printer Prize!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

FLiP Connected X-Mas Ornament

 

Hi,

 

Here is an X-Mas project I have been working on.  This is a Bluetooth connected Ornament that uses a Parallax FLiP board, WS2812B RGB LED Module and a Velleman HC-05 to control the color displayed in the Ornament.  The Ornament was cerated using a Clear DIY Plastic Hanging Ornament, paint, mini X-mas tree and Styrofoam for the fake snow.  The Parallax FLiP is a DIP form factor board which has a Parallax Propeller processor and was coded using their SimpleIDE in C.  Communication from the FLiP with the HC-05 was performed using the fdserial library from Parallax. Remote connection is from a Raspberry Pi using BlueZ and rfcomm to create a virtual serial interface to the HC-05 and Python was used to send command line commands to control the WS2812B through the HC-05.  A Parallax Serial LCD is used just for debug purposes to ensure the commands made it to the FLiP.

 

If I were honored enough to wind the 3-D Printer, I would certainly use it to create the much needed enclosures for the the projects I have been working on as well as perhaps fix a few items around the house such as the knob on the Toaster.

 

 

The Sam's STEAM Kit I would look to donate to one of the under privileged schools in the area where the students might not have access to such items.

 

Project Items

 

DIY X-Mas Ornament

  • Walmart Clear DIY Plastic 4" Ornament
  • https://www.walmart.com/ip/Clear-DIY-Plastic-Globe-Hanging-4-Inch-Round-Ornament-Decoration-Paintable-Fillable-Clear-4-Inch-DIY-Plastic-Globe-w-Hanging-String-Crafters-Square-S/281310148?wmlspartner=wlpa&selectedSellerId=11121&adid=22222222227112224969&wl0=&wl1=g&wl2=c&wl3=233998737977&wl4=pla-385820201205&wl5=9032551&wl6=&wl7=&wl8=&wl9=pla&wl10=117084546&wl11=online&wl12=281310148&wl13=&veh=semApple Barrel Outdoor Gloss Paint - White
  • Glitter Glue
  • Glue Gun
  • Styrofoam Packaging material (for fake snow)

FLiP Circuit

  • Parallax FLiP - https://www.parallax.com/product/32123
  • Parallax WS2812B RGB Module - https://www.parallax.com/product/28085
  • Parallax Serial LCD - https://www.parallax.com/product/27977
  • Velleman HC-05 Bluetooth Module - https://www.velleman.eu/products/view/?id=435518
  • Parallax SimpleIDE - https://learn.parallax.com/tutorials/language/propeller-c/propeller-c-set-simpleide

 

Rasberry Pi

  • BlueZ
  • rfcomm
  • Python
  • Good source for configuring the Raspberry Pi for the HC-05:
    • https://myraspberryandme.wordpress.com/2013/11/20/bluetooth-serial-communication-with-hc-05/

 

Example of how to scan and connect to the HC-05 from a Raspberry Pi:

 

Scan for devices:

sudo hcitool scan
Scanning ...
  98:D3:32:20:C9:FC HC-05

 

Connect to the HC-05 device:

sudo rfcomm connect hci0 98:D3:32:20:C9:FC 2>&1
Connected /dev/rfcomm0 to 98:D3:32:20:C9:FC on channel 1
Press CTRL-C for hangup

 

Send a command to the RGB LED:

NOTE: In this case this will cause the RGB to Fade in and out in Blue

sudo su -c "echo 'LEDD' > /dev/rfcomm0"

 

In my project, this is all handled via a Python script by passing command line commands to the script.  This Initiates the Bluetooth connection, sends the command, and then kills the connection so it does not stay active.

 

Example:

os.system("sudo rfcomm connect hci0 98:D3:32:20:C9:FC 2>&1 &")
time.sleep(2)

os.system("""sudo su -c \"echo \'LEDD\' > /dev/rfcomm0\" """) 
time.sleep(2)

os.system("sudo pkill --signal SIGINT rfcomm")

 

My script is a bit more interactive than this but this gives an idea of how the commands are being sent.

 

This is still breadboarded and I intend to put the FLiP circuit in a case as well as code a Javascript interface so the commands can be send from a webpage.

As always, time is my enemy.

 

Here is a video of what I have thus far.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
Parents
  • genebren
    genebren over 8 years ago

    What a fun idea.  I could easily see a bunch of these on a tree.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    What a fun idea.  I could easily see a bunch of these on a tree.