• Products and Partners
    Products and Partners
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
The World in Motion
  • Challenges & Projects
  • Project14
  • The World in Motion
  • More
  • Cancel
The World in Motion
Blog Pulse Width Modulation a Speed Equalizer(5): The plan didn't survive first contact.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The World in Motion to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 31 Jul 2022 9:55 PM Date Created
  • Views 2860 views
  • Likes 6 likes
  • Comments 10 comments
  • motor projects
  • worldinmotionch
  • pwm
Related
Recommended

Pulse Width Modulation a Speed Equalizer(5): The plan didn't survive first contact.

colporteur
colporteur
31 Jul 2022

I did the first field tests with a HO scale locomotive today with limited success. The locomotive speed was controllable by using PWM but the whine from the motor is not acceptable for operational use.

In 1871 Prussian Field Marshal Helmuth von Moltke the Elder wrote an essay about military strategy. The following is an English translation, "No plan of operations extends with any certainty beyond the first encounter with the main enemy forces. Only the layman believes that in the course of a campaign he sees the consistent implementation of an original thought that has been considered in advance in every detail and retained to the end."

It appears I am the layman in Moltke's quote. The motor used for bench testing was not a locomotive motor but rather a 12VDC surplus motor. It did produce a whine during testing but only at a lower speed. I never gave it much thought. The locomotive motor when powered from PWM whines at all speeds. In addition, the maximum speed is slower with PWM than with the train power supply. Looking online, there are some examples of PWM producing a whine when used to power a motor. 

My first thought was the PWM frequency. Could a higher PWM frequency eliminate the whine?

The default PWM frequency for pin 3 ( pin used for PWM) is 490 Hz. Pin 4 has a default frequency of 980Hz. Using the PWM signal from pin 4 eliminated the whine with a loss of speed control. Using a speed code value of 127 the locomotive didn't move. At a value of 128, the locomotive moved at maximum speed. On the lower PWM frequency, (I can't recall the speed values) there was a greater range of control. I could get a slow speed as well as a top speed but with the whine.

This first contact's poor success has given me cause to make some changes. For any further bench testing, I will be using a locomotive motor and not my bench surplus motor. Initial google search suggests PWM frequency changes from defaults are possible but don't appear to support a frequency between 490Hz and 980Hz. I have yet to garner an understanding of why using the 980Hz frequency results in a loss of speed control.

I thought my plan was sound but it appears to need some tuning. Maybe a different motor driver module is required? Would a filter cap on the module output help? I'm not sure at the moment. I'm open to suggestions as I bandage my wounds and prepare for another attempt.

  • Sign in to reply

Top Comments

  • robogary
    robogary over 4 years ago +1
    Industrial AC & DC motor drives have a similar issue. I can also hear the whine of an electric vehicle H bridge. Those controls have features to change the switching frequency to adjust audible noise,…
  • colporteur
    colporteur over 4 years ago +1
    Error on my part. The website that reference pin 4 as 980Hz is wrong! Looking at the spec sheet pin 4 doesn't support PWM it is pin 5 that is PWM at 980Hz. Something I will need to investigate.
Parents
  • shabaz
    shabaz over 4 years ago

    Hi Sean,

    If the software allows it, you could push the frequency up to (say) 10 kHz, if the rest of the circuit allows it. Ideally higher than 20 kHz would be possible, it depends on the circuit (some might not be able to switch power at this rate) and what the software is capable of. 490 / 980 Hz is extremely low, I'm surprised the PWM library defaults to that. The PWM is audible for a couple of reasons but they are related. One is the frequency, but that alone isn't the cause, because it's to do with the PWM being used directly for the motor, with no smoothing. The easiest way will be to find an inductor (perhaps 10 mH) and put it in series with the motor, and place a capacitor across the motor (perhaps 1 uF). It will look like an LC filter, The values are just guesstimates, but an OK starting point. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 4 years ago

    Hi Sean,

    If the software allows it, you could push the frequency up to (say) 10 kHz, if the rest of the circuit allows it. Ideally higher than 20 kHz would be possible, it depends on the circuit (some might not be able to switch power at this rate) and what the software is capable of. 490 / 980 Hz is extremely low, I'm surprised the PWM library defaults to that. The PWM is audible for a couple of reasons but they are related. One is the frequency, but that alone isn't the cause, because it's to do with the PWM being used directly for the motor, with no smoothing. The easiest way will be to find an inductor (perhaps 10 mH) and put it in series with the motor, and place a capacitor across the motor (perhaps 1 uF). It will look like an LC filter, The values are just guesstimates, but an OK starting point. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 4 years ago in reply to shabaz

    (can't edit)

    Just saw @robogary response, that's a great idea to use a transformer winding as a test, if you don't have an inductor handy.