The World in Motion
  • Challenges & Projects
  • Project14
  • The World in Motion
  • More
  • Cancel
The World in Motion
Blog Received Project14 World in Motion Reward
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The World in Motion to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: misaz
  • Date Created: 22 Nov 2022 1:09 PM Date Created
  • Views 2699 views
  • Likes 9 likes
  • Comments 10 comments
  • worldinmotionch
  • wishlist
  • reward
Related
Recommended

Received Project14 World in Motion Reward

misaz
misaz
22 Nov 2022

Hello Element14 community.

About month ago I was selected as Grand Prize winner of Project14 World in Motion competition for my Duratool Storage Cabinet Upgrade. Thank you for selecting me. I won electronics components from Farnell in value of 200 USD. Last week I received first part of my reward. Some components was backordered because they get out of stock between I send basket and element14 ordered it, so I am looking forward for about 1/5 later but most components already flooded my desk. In this blog I want to share list of parts which I ordered and describe my ideas why did I ordered them.

Some parts I chosen from my long-term wishlist and some of them I ordered for immediate use.

Microcontrollers: 8-pin STM32 MCU

Buy Now

I love microcontrollers. I use them in almost all my projects. So, I decided to order some interesting dev boards. In previous months I spend my time with very advanced and high-performance microcontrollers. For example, it was Renesas RA6M4 which you have seen in my project. But I was thinking about it and most of time I use these MCU because they have some specific peripheral (Ethernet in case of RA6M4) and otherwise I use them very briefly. Usually, these MCUs are big overkill. So, I decided to go with some lower-end MCUs and selected some interesting boards for experimenting with. I chose three MCU devboards.

First is STM32G0316-DISCO. It is $10 evaluation board for 8-pin STM32 microcontroller. I have experiences with STM32, but I have never used these very low-pin parts. It has some challenges because for example Reset pin is shared with other GPIOs and requires special care in special configuration. I personally think that in most case it is better to use TSSOP20 instead SOIC8 because sizes are similar, but TSSOP20 have more pins because it has smaller pitch. But low-pin MCUs are cool to me, so I want to play with it and possibly use it for some tasks in my projects.

image

In the meantime I already used it. You can see it as part of my VEML3328 Last-Minute Entry to the Summer of Sensors Design Challenge.

Microcontrollers: Modern AVR DB

Buy Now

Second microcontroller evaluation board which I received is AVR128DB48 Curiosity Nano board. ATMega16 was my first microcontroller (in 2014) and AVR allowed me to grow up and I still love these MCUs even I do not use them frequently anymore. AVR128DB48 is one of the newest AVR MCU. It has newer architecture, and it is manufactured using modern technology which result to much better properties (for example you can run it at full speed when powering as low as 1.8 V).

image

Many things changed in AVR world since I was playing with ATMega16. Board has onboard debugger so last week I used breakpoint with AVR microcontroller first time in my life. MCU now support two powering rails, so you can some ports power by lower voltage than is main voltage (usualy 3.3V as main voltage and 1.8V on VDDIO2). Other cool feature of Curiosity board is that main voltage is software adjustable, so you can try it at different voltages. I tried 2.5V and works like a charm. If you are interested in more details, then I recommend reading baldenginner’s 7 reasons why I like the ATmega128Dx MCUs.

Microcontrollers: Low-cost Bluetooth Low Energy

Buy Now

The last microcontroller development board which I ordered is Silicon Labs BG22-EK4108A with Wireless Gecko MCU. Board is cool because it cost only $10 and except Bluetooth LE capable MCU has Segger J-Link OB debugger. For 10 dollars you may think it has some entry level Cortex-M0+ MCU but opposite is true. MCU is very modern ARM Cortex-M33 with TrustZone clocked at high 76.8 MHz. It is more than for example STM32 DISCO mentioned above offers. I think it is good deal and I am looking forward for playing with this MCU.

image

New Breadboard + High Quality (near Zero Ohm) Wires

Next part in my basket was breadboard. Some of my projects (for example my previous Digitally Adjustable Power Supply) are very huge and utilizes multiple breadboards. But my oldest breadboard is from 2014 and over years some contacts get very weak. Sometimes it is lottery and already cost me several hours of debugging. So, I ordered new breadboard:

image

If you remember my blogs as part previous Experimenting with MAX40080 Current Sense Amplifier (Blog #10) I faced issue with my wires which had very high resistance. As part of competition I used wires form other devkit but I have only few of this wires. Now it changed and I ordered new better wires for use cases when resistance is important:

image

I already tested them. Design with these wires is much more clear. You can see it as part of my VEML3328 Last-Minute Entry to the Summer of Sensors Design Challenge next to STM32G031 disco.

Product Name Manufacturer Quantity Buy Kit
MC001795, Breadboard, 830 Tie Points MULTICOMP 1 Buy Now
MC001810, Jumper Wire Kit, Multicolour, 2 mm - 125 mm, 22 AWG, 140 Piece MULTICOMP 1 Buy Now
 

MAX78000FTHR Upgrade

Maybe you remember my previous reward from Project14 competition: Received Project14 7-segment Display Competition Reward

As part of reward I ordered incredible MAX78000FTHR board. Board come with pin headers for soldering. But I noticed some confusion with Adafruit Feather standard. Some shields exposes sockets (for example MAX25405EVKIT) and some exposes pins (MAX41470EVKIT). For being able connect both types to the board I decided to do not soldered bundled pin headers but instead I ordered pin sockets with extended terminals as part of this review. I ordered both 12-pin and 16-pin variant. Both are from Samtec. Part numbers are: SSQ-112-03-T-S and SSQ-116-03-T-S.

image

After soldering to the board:

image

Now I can connect both types of shields (one from bottom, second type from top).

Another upgrade is that I want to try power it by battery. Board has JST connector with 2mm pitch and I did not find any compatible battery with this connector. So, I instead ordered battery with different connector, compatible connector and precrimped wires. I did not received battery yet (which is interesting because it is in stock and order contained line number dedicated to the item, but it was skipped in received package). Except battery, connectors and precrimped wires was in package:

image

Product Name Manufacturer Quantity Buy Kit
SSQ-116-03-T-S, PCB Receptacle, 2.54 mm, 1 Rows, 16 Contacts, THT, SSQ SAMTEC 1 Buy Now
SSQ-112-03-T-S, PCB Receptacle, 2.54 mm, 1 Rows, 12 Contacts, THT, SSQ SAMTEC 1 Buy Now
MIKROE-2759, Li-Polymer Battery, Add-On Board, 3.7V, 190mAh MIKROELEKTRONIKA 1 Buy Now
01SPHSPH-26L300, Cable Assembly, Crimp Terminal Socket to Crimp Terminal Socket, 11.8 ", 300 mm, Blue JST 10 Buy Now
PHR-2, Connector Housing, PH, Receptacle, 2 Ways, 2 mm, BPH and SPH Series Crimp Contacts JST 100 Buy Now
 

Turning nRF52840 Dongle to Devkit

The other item which I ordered in previous basket (and decided to upgraded it) is nRF52840 dongle. I upgraded it in following way:

  • Added 120 pF capacitors for tuning NFC antenna
  • Soldered ARM Cortex-M 10-pin JTAG connector for connecting debugger
  • Soldered special pinheads for using it on the breadboard

As part of reward, I ordered parts for first and third bullet. JTAG connector I already had. The more interesting are pinheads. Because JTAG connector is at the bottom I need special very long pin headers. I chosen pinheads from Samtec. Part number is: TSW-120-17-T-S.

image

This pin head I broken to two 10-pin and soldered to the board.

image

Fully inserted to breadboard it looks as follows:

image

As you can see there are space for JTAG connector and cable.  About two millimetres of gap remained, so my computation of required length was correct and I am satisfied.

Product Name Manufacturer Quantity Buy Kit
TSW-120-17-T-S, Pin Header, 2.54 mm, 1 Rows, 20 Contacts, THT, TSW SAMTEC 1 Buy Now
FTSH-105-01-L-DV-K, Pin Header, 1.27 mm, 2 Rows, 10 Contacts, SMD SAMTEC 1 Buy Now
FFSD-05-D-12.00-01-N, Ribbon Cable, 10 Ways, 12 ", 1.27 mm SAMTEC 1 Buy Now
CGA2B2C0G1H121J050BA, SMD MLCC, 120 pF, 50 V, 0402, ± 5%, C0G / NP0 TDK 10 Buy Now
 

NFC and Tuning Capacitors

Recently I decided to make my own NFC Tags. I want to use them as part of next Project14. For this reason, I ordered 13 pcs of one of the cheapest NFC tag available on the market. Part number is ST25TA02KB-PC6H5. They are in 5-pin very small SMD package, but as far I successfully soldered two of them.

NFC Tags requires capacitors in values about tens of pico farads for tuning antenna. Because I was not sure what values I will need I ordered all in range 40 – 200 pF (except values which I already own) values in 0603 package and available at Farnell in stock. For summary I ordered:

  • 56 pF
  • 68 pF
  • 82 pF
  • 100 pF
  • 120 pF
  • 150 pF
  • 180 pF

 image

I will post photos of my assembled tags containing NFC chips and capacitors later as part of my next project. Blush

For my experiments with NFC, I also ordered STEVAL-SMARTAG1 and X-NUCLEO-NFC03A1 NFC Reader shield but because they are out of stock, I did not receive them yet. Currently missing reader block my project but according to website it should be restocked at the end of month, so there should be sufficient time for completing project.

Product Name Manufacturer Quantity Buy Kit
X-NUCLEO-NFC03A1, Expansion Board, NFC Card Reader STMICROELECTRONICS 1 Buy Now
STEVAL-SMARTAG1, Evaluation Board, NFC Dynamic Tag Sensor Node, ST25DV64K NFC Tag STMICROELECTRONICS 1 Buy Now
ST25TA02KB-PC6H5, RFID, READ/WRITE, 13.567MHZ, UFDFPN-5 STMICROELECTRONICS 13 Buy Now
CC0603JRNPO9BN560, SMD MLCC, 56 pF, 50 V, 0603, ± 5%, C0G / NP0 YAGEO 10 Buy Now
0603N680J500CT, SMD MLCC, 68 pF, 50 V, 0603, ± 5%, C0G / NP0 WALSIN 10 Buy Now
885012206078, SMD MLCC, 150 pF, 50 V, 0603, ± 10%, X7R WURTH ELEKTRONIK 10 Buy Now
MC0603B121K500CT, SMD MLCC, 120 pF, 50 V, 0603, ± 10%, X7R MULTICOMP PRO 10 Buy Now
GA0603A101JXBAC31G, SMD MLCC 100 pF, 100 V, 0603, ± 5%, C0G / NP0 VISHAY 30 Buy Now
C0603C820J5GACAUTO, SMD MLCC, 82 pF, 50 V, 0603, ± 5%, C0G / NP0 KEMET 10 Buy Now
0603N181G500CT, SMD MLCC, 180 pF, 50 V, 0603, ± 2%, C0G / NP0 WALSIN 10 Buy Now
 

Experimenting with Gesture Sensors components

Currently I am working on projects as part of Experimenting with Gesture Sensors Design Challenge. I ordered some parts for this contest. Details about need for these parts I will post in blog post as part of Experimenting with Gesture Sensors Design Challenge soon.

As part of this reward I ordered:

  • 1pcs of Maxim Integrated (ADI) MAX25405 Gesture Sensor (chip)
  • 5pcs of OSRAM SFH 4248-Z IR LED
  • 5pcs of OSRAM SFH4249 IR LED
  • 5pcs of Infineon BSD840N dual-channel NMOS transistor

For some reason I received all but SFH4249 IR LED. Because I received 4248 IR LED I am still satisfied.

image

Product Name Manufacturer Quantity Buy Kit
MAX25405EQP/VY+, Gesture Sensor MAXIM INTEGRATED 1 Buy Now
SFH4249, IR LED, 950 nm, 50 °, PLCC, 50 mW/Sr, 12 ns, 12 ns AMS OSRAM GROUP 5 Buy Now
SFH 4248-Z, IR LED, 950 nm, 30 °, SMD, 100 mW/Sr, 12 ns, 12 ns AMS OSRAM GROUP 5 Buy Now
BSD840NH6327XTSA1, Dual MOSFET, N Channel, 20 V, 880 mA, 0.27 ohm, SOT-363, Surface Mount INFINEON 5 Buy Now
 

Soldering goodies

I decided to upgrade my soldering toolbox. I ordered 3 tips (Duratool D02261, D02262 and Multicomp MP000023). After I received them, I noticed they are not the same size as tip used by my soldering iron, so they are useless to me now, but maybe in the future I get compatible soldering iron.

image

Next soldering goodie was new soldering wick. I already used it for desoldering and cleaning and it is nice. It is much better than Chinese alternative which I used for years.

image

Next soldering related goodie which I receoveid as part of reward for free is tip cactivator from Weller:

image

And finally, I ordered 3 heat shrink tubes. As far I received two of them. Third get out of stock in meantime when I send basket and when Element14 ordered it for me, so middle size I will receive later.

image

This was last part which I ordered for regular use. But because some dollars remained in my budget I ordered some parts which I do not need them immediately but I want to test and play with them and possibly use them sometime in the future.

Product Name Manufacturer Quantity Buy Kit
MP000023, Soldering Tip, Conical, 0.6mm MULTICOMP PRO 1 Buy Now
D02261, Soldering Iron Tip, Conical, Chisel, 2 mm DURATOOL 1 Buy Now
D02262, Soldering Iron Tip, 45° Bevel, 3 mm DURATOOL 1 Buy Now
423, Desoldering Braid, Oxide Free Copper, #1, 1.5 m L x 0.8 mm W, SuperWick 400 MG CHEMICALS 1 Buy Now
TIP ACTIVATOR, Tip Activator, Low Temperature, Lead Free, 25g WELLER 1 Buy Now
PP002758, Heat Shrink Tubing, 2:1, 0.099 ", 2.5 mm, White, 3.9 ft, 1.2 m MULTICOMP PRO 1 Buy Now
PP002781, Heat Shrink Tubing, 2:1, 0.06 ", 1.5 mm, Brown, 3.9 ft, 1.2 m MULTICOMP PRO 1 Buy Now
PP002795, Heat Shrink Tubing, 2:1, 0.138 ", 3.5 mm, Green, 3.9 ft, 1.2 m MULTICOMP PRO 1 Buy Now
 

High-power N-Channel MOSFETs

Buy Now

All my MOSFETs which I have are rated to less than 1A. It is because I generally work with very low currents, but I already faced situation when I need more. So now I ordered three units capable of 80 A. Part number is IPP034N03LGXKSA1. It is marked as NRND on Infineon website but still offers good Price-performance ration.

image

Signal Relay

Buy Now

I have idea about one project which will use two relays but I never find enough time for completing this project. Now I did one step further and ordered 2pcs of Axiom (TE) IM01TS Relay.

image

VEML3328 Color Sensor

Buy Now

VEML3328 is color sensor. Something like single-pixel camera. It was mentioned in Optical Sensors Quiz and I was interested in it. This sensor is also present on board which were recently RoadTested. But I missed this RoadTest due to lack of free time. Because I was still interested in playing with this sensor, I ordered it now as part of this reward.

image

It did not take very much time and now it is on my breakout which I designed, ordered and received from OSHpark in meantime:

image

In meantime I already play with it. You can see it as part of my VEML3328 Last-Minute Entry to the Summer of Sensors Design Challenge next to 8-pin STM32.

MEMS Microphone

Buy Now

The other SMD Sensor is MEMS microphone. I have already used some hardened on EVKITs but I never have any on breakout for general purpose use with any MCU. So now I have one:

image

I already made breakout but due to lack of free time I did not solder and test it yet.

MAX16935 DC/DC Step Down Regulator

Buy Now

I used this regulator in several projects including project for which I received this reward. Because my stock is running low and some dollars remained in my budget, I ordered one. One pin is bend but this is not big issue since it is in TSSOP package. It is not the exact same part number which I have. It differ in preset voltage and has no spread spectrum capability but none of these is issue for my hobby projects. Part number is MAX16935RAUE/V+

image

OLED Display Module

Buy Now

As far I had only Nokia 5510 compatible SPI display. Now I ordered new modern I2C OLED display. It’s resolution is 64 × 48 px, which is exactly the same as in case of my old Nokia 5510 display.

image

You can see it as part of my VEML3328 Last-Minute Entry to the Summer of Sensors Design Challenge next to 8-pin STM32G0 and VEML3328. Display works but some libraries requires fix of pixel mapping because columns are not connected to signals 0 – 63, but they are mapped to the 32 – 95. Display controller has command which can reflect this and map it to the standard 0 – 63 range of memory area.

2x7-pin IDC Connector

Buy Now

The last connecter in my basket is IDC connector. I used most of my stock of these connectors in project for which I won competition. So, I ordered one for future project. Part number is Samtec TST-107-01-G-D.

image

0603 LEDs

As far I had only red 0603 LED. For my Duratool Storage Box Upgrade project I ordered amber 0603 LEDs for distinguishing failures (red) and standard indications (amber) but I still did not have other collors. As part of reward, I ordered green, blue and yellow LEDs. My future projects will be more colourful. Part numbers are: Multicomp MP008282 (Green), MP008278 (Yellow) and MP008276 (Blue).

image

After soldering to breakout and adjusting resistors, they look as follow:

image

Product Name Manufacturer Quantity Buy Kit
MP008276, LED, Blue, SMD, 0603 [1608 Metric], 20 mA, 3.4 V, 470 nm MULTICOMP PRO 10 Buy Now
MP008278, LED, Yellow, SMD, 0603 [1608 Metric], 20 mA, 2.4 V, 595 nm MULTICOMP PRO 10 Buy Now
MP008282, LED, Green, SMD, 0603 [1608 Metric], 20 mA, 2.4 V, 575 nm MULTICOMP PRO 10 Buy Now
 

Resistors

Last cents of my basket I spend for resistors. I extended my stock of 10K and 100K resistors in 0603 package by 40 new pcs. Except these resistors I ordered also 0-ohm jumpers in 0603 package and 4×33-ohm resistor network.

Product Name Manufacturer Quantity Buy Kit
MCWR06X000 PTL, Zero Ohm Resistor, Jumper, 0603, Thick Film, 100 mW, 1 A, SMD MULTICOMP PRO 30 Buy Now
CRG0603F10K/10, SMD Chip Resistor, 10 kohm, ± 1%, 100 mW, 0603, Thick Film, General Purpose NEOHM - TE CONNECTIVITY 40 Buy Now
MR06X1003FTLV, SMD Chip Resistor, 100 kohm, ± 1%, 125 mW, 0603, Thick Film, General Purpose WALSIN 40 Buy Now
CAY10-330J4LF, Fixed Network Resistor, 33 ohm, Isolated, 4 Resistors, 0804, Convex, ± 5% BOURNS 10 Buy Now
 

Summary

And this is all. As far reward come in 5 packages, but some parts are still on backorder. When I was sending order all parts were in stock but with current situation, stock statuses can change very quickly. After I receive them, I will post second part blog. Currently it is scheduled to February 2023. Blush

This reward is super cool to me. It brought me a lot of fun and I guess it will do the same in the future.

If you have any feedback regarding my choice, feel free to write in comments below. I would also like to hear what would you buy for 100 or 200 USD from Farnell/Newark? Do you know about any interesting but less known part? Some interesting sensor, chip, devkit, tool or something like this? These comments are always inspirative to me. If you want to win your own 100 or 200 USD shopping cart then go to Project14 page and join actually opened contest.

At the end I would like to thank Element14 for selecting me grand prize winner and sending me the reward. I would like to thank Tariq Ahmad for organizing these competitions. At the end I would also thank you for reading this blog.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 3 years ago +1
    Very nice haul. Now you are all set for more projects. I have ordered (on backorder) a Teensy 4.1 from Newark.
  • shabaz
    shabaz over 3 years ago +1
    Good idea with the JST ready-crimped cables. Way cheaper (and safer) to buy those than attempt to crimp the battery connections with inexact crimp tools : )
  • misaz
    misaz over 3 years ago in reply to genebren

    Thank you for feedback. I also think so. It is 49 parts in total of 429 pieces and I will use them in at least 5 projects as I plan now. Value is exactly 200 USD. In fact it was 5063 CZK because I am based in Czech Republic and selected parts on Czech Farnell localization. Maybe it was also caused by timing. When I was ordering parts, Czech currency was exteremely strong (several years peak). If I should select parts now I get about 2% parts less becaus exchange rate changed since I was selecting parts. When selecting parts Iwas also forced to redesign my shopping cart because at the time of selecting Farnell switched into "maintanence mode" for one day and after they brought it online again I was surprised. They repriced almost every part in my cart.

    But after all I am satisfied and components which i received are nice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 3 years ago

    Nice job on shopping.  It looks like your some great value on your shopping money.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 3 years ago in reply to shabaz

    Thank you for feedback.

    Yes this was exactly the idea behind. I do not have any crip tool for these connectors, so I was considering ordering crimp tool (I did not find exact for these parts, so I was considering alternative) or crimp them in a DIY way, but after I found this precrimped wires, I decided to go this way. Disadvantage is price, wires are OK, but PHR-2 connector housings I had to order in quantity of 100 (received 101 pieces, one for free) which is minimum order quantity and price of 100 housings was 4.19 GBP. I think it is too much if I take in account that I need only one piece and it is just a dummy 2-pin connector... Many product on farnell have more hobby-friendly MOQ, but in this case they set 100 as MOQ. But decided to order them and I am looking forward for receiving battery. Then I plan to cut the original connector of the battery and solder these new wires and inserting them to the connector which exactly fits with MAX78000FTHR (this I already tested). My idea is to improve my skils with low-power applications and try onboard fuel gauge as part of PMIC, sleep modes of MAX78000 FTHR and so on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Good idea with the JST ready-crimped cables. Way cheaper (and safer) to buy those than attempt to crimp the battery connections with inexact crimp tools : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 3 years ago in reply to dougw

    Nice to hear that it works. Thank you for reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>