Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21835 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hi ipv1 ,

     

    I  looked into this and this is a known issue:

     

    BeagleBoneRegistered AI - Frequently Asked Questions (FAQ)

     

    They recommend adding a larger heat sink and cooling via fan.   

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to tariq.ahmad

    My investigations showed much the same. My questions are:

     

    1. How was this not caught during testing ? Some minor overheating might be missed but shutting down as described on many of the comments makes it obvious that there is a serious problem.

    2. This is happening when you are only running the OS on the ARM Cortex-A15 cores.  What happens to the temperature when you start using some mixture or all of the ARM Cortex-M4s cores,

          DSPs, EVEs and PRUs too?

    3. If it needs a bigger heat sink and fan just running the OS why doesn't it HAVE a bigger heat sink and fan (see 2.).

     

    After reading the earlier comments in this discussion and checking for other comments on the web I hopped over to Ebay and bought a couple of 25mm fans. The heat sink on the AI is 25mm and

    it looks like there are threaded holes to attach the fan with. I'm not sure how you mount a larger heat sink  other than a adhesive thermal pad or thermal epoxy. There is an adhesive thermal pad

    between the heat sink and SoC but I'm not a big fan of thermal pads and in this case I would much rather have a heat sink that uses mount points on the PCB and a wafer thin layer of quality thermal

    paste.

     

    It also looks like it could use some serious thermal management on the OS side. I'll give them the benefit of the doubt and hope that somebody is looking into this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    The trick is to find that Cape Fan.  I have not been able to locate it.

     

    From the SRM link I provided earlier, the suggested fan is one that screws to the top of the heat sink; X15FANKIT.  The Cape version seems like a cleaner option tough but certainly would draw some juice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    As I understand, the fan cape still isn't released (just from grapevine so I could be wrong). It does look nice, in that video.

    The X15FANKIT fan has 2.8mm holes (going by the part name in the photo of the fan), maybe they just suggest forcing the M3 screws through.

    I've been searching at home to look for a suitable fan, but only came up with a 25mm fan (also with 2.8mm holes, but M3 could be threaded through it I reckon) and a 50mm fan, and 50mm is too big to fit between the connectors. Maybe this 5V 40mm fan5V 40mm fan could be suitable (i.e. if the BB-AI has some acrylic sheet or something mounted on top), it has 80mA current consumption.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to shabaz

    "But, since they knew that people would also want to run it immediately (i.e. without needing additional heat management), there is a small heatsink already mounted, and with threads to attach to a custom solution if required."

     

    The problem is that the small heat sink "to allow running it immediately" does not work. The custom solution is called a fan, and from the ongoing discussions I've read it is required right out of the box for even minimal operation.

    Software frequency throttling should allow it to run without a fan and it will be useful later for overall power management but why it was not implemented or implemented properly (I have no idea which is correct) before shipping

    product "that people could run immediately" is a very good question. At least it should be a rather quick and easy fix. For now I have a couple of 25mm 10K RPM fans on order (from Ebay) and I will not even think about powering

    up my AI until one is installed. At 10K RPM it will probably scream like a banshee, luckily it will be a very small banshee.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to gdstew

    I think ultimately that the BB-AI would operate in two (or more) modes, e.g (1) without the fan, any throttling could be more aggressive, or would run at a slower rate., and (2) with the fan cape (or if configured otherwise) then the BB-AI would operate in a higher performance, or a sustained performance mode.

    That seems plausible, especially since some of the suggestions discuss upgrading the software image, to allow people to run the BB-AI without any fan or additional heatsink. The fan cape has been planned for a long time, so that too gives credence to the thought that they were aware that two modes would be used in software.

    gdstew  wrote:

     

    .. but why it was not implemented or implemented properly (I have no idea which is correct) before shipping

    product "that people could run immediately" is a very good question. At least it should be a rather quick and easy fix.

     

    You're right, it would have been a better experience for users if it was in the shipped image. Perhaps it just missed some integrating and testing window for their release timeframe. Presumably even without the fix, the BB-AI won't self-destruct, so the software release didn't need to match the hardware release timeframe. Again I'm just speculating (but it seems semi-plausible).

     

    The first thing I do with a BeagleBone Black is to download the latest image, but then I'm used to that. Maybe with the BB-AI, there could be an assumption (true or not I don't know, not checked to see any release notes) that the pre-installed image is still very close to the released image, since it is a new product. I too intend to install a fan, but maybe a 40mm one, in the hope that it is quieter.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to shabaz

    I've got a couple of 40mm fans but what I found was they have large motor hubs and very small blades which puts the blades too far away from

    most of the heat sink for my liking although the SoC is offset from center by quite a bit and that may help. That and it will require some kind of

    special mounting bracket or modified prototype cape. I hadn't thought about modifying a prototype cape until I wrote this and I have a couple

    of Adafruit capes so I might do that if the 25mm fan doesn't work well enough. I was originally thinking about using tall nylon machine screws

    for a temporary solution with the 40mm fan so I could get it up and running fast. The inside of the GPIO headers are a few mm more than

    40mm apart and that could used to help wedge the fan in and prevent it from "walking" around too much.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to gdstew

    gdstew  wrote:

     

    I've got a couple of 40mm fans but what I found was they have large motor hubs and very small blades which puts the blades too far away from

    most of the heat sink for my liking

    That's a good point.. subconsciously that must have been bothering me too, so I've been thinking of trying to make the area larger (with an aluminium plate). The height of the heatsink that comes attached to the BB-AI clears the height of the USB connector too, so quite a large plate could be glued on top. It might be inefficient though.. I'll try it anyway, and if it doesn't cool sufficiently, I'll switch to the 25mm fan.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    The actual location that the blades are pointing to is not very critical. The goal is to keep the air flow going so that the hot air gets evacuated and replaced by cold air. The air volume plays the bigger role here.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > And again, so far this is not even close to running it under full load

     

    Apparently the GUI environment runs by default on the BeagleBone AI, and disabling this helps the temperatures to subside somewhat.

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to jomoenginer

    > The trick is to find that Cape Fan.  I have not been able to locate it.

     

    The official one is a couple of months away, so I'm told.

     

    Until then, mayermakes has been designing an add-on board image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > luckily it will be a very small banshee.

     

    Seems appropriate for Halloween - Projects and Videos

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > luckily it will be a very small banshee.

     

    Seems appropriate for Halloween - Projects and Videos