Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21870 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • ipv1
    ipv1 over 7 years ago

    At this moment, my BB Ai no longer works. I removed the pull-up resistor which Jan Cumps mentioned as a solder bridge, but the board booted the same way to heat up the same way as before. Then I ran a sudo apt dis-upgrade and after rebooting, the board never booted up again.

    I added the pull-up again but no go.

     

    I also tried booting from an image but no go.

     

    So

    a. Don't remove the solder-bridge

    b. Don't run updates.

     

    I will try and use the serial interface to see if uboot is doing something or if the board itself is dead. I am hoping for the former but it may be the latter due to overheating.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to ipv1

    Kind of an expensive board to be putting a soldering iron to it which I would suspect violates the warranty.

     

    Does your board have a heat sink and or fan on the main processor?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to jomoenginer

    The board has a full heat sink on the SoC. But is hard to tell if any thermal paste. Mine gets hot with very little usage. But the heating issue is not as bad as ipv1 .

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to clem57

    Is it possible to remove, add new solder paste and replace the heatsink?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to 14rhb

    A little bit of heat works. A hairdryer or hot air blower on low temperature ...

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    I'm still going back-and-forth on what to do, but am currently thinking of leaving the heatsink attached (too scared to try to remove it : ) and then glue a larger aluminium plate (maybe just 1mm thick?) to it, using double-sided thermal tape.

    Then, there are quite low-profile heatsinks that are 20x20x2.5mm, so I could try gluing (say) four of those to the top of the aluminium plate, i.e. for 40x40mm total area or slightly more. Then, have a 40mm fan on the acrylic cover blowing down on those heatsinks. That way the larger fan is blowing over more surface area.. I'm not too good with thermodynamics so this is just experimental!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to shabaz

    I too thought that might be the safer option. I was looking at mine last night and I am going to make a heatsink that fits into the existing slots - I reckon five 60mm x 30mm high x 1~2mm thick aluminium plates. I'd use some thermal paste and bend the fins slightly to get a good friction fit. Then as 'belt and braces' I'd add a fan.

     

    I'll post any progress.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb

    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over the top for my DC fan and add some thermal grease on the final assembly.

     

    I think I've just fed my Beagleboard a new bone so I'm going to call it the "Beagleboard's Bone" and might even shape those aluminium fins accordingly image

     

     

    {gallery} Beagleboard's Bone

    image

    BeagleboardAI: Heatsink

    image

    BeagleboardAI: Heatsink

    I'll spin that U.Fl antenna around as well.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to 14rhb

    Wow! 14rhb that is industrial strength. I would call it a "heavy duty, harder than a Bone" Do you know what it weighs with that on it?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to clem57

    Thank you image

     

    It's only aluminium and probably won't register on the kitchen scales but I'll have a go at weighing it.

     

    The downside will be not being able to use capes on this board.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    That should do it : ) Very cool look! Also, it looks like the end may be about 20mm square, so in theory you could even mount a fan sideways, to leave the slots visible and not covered by a fan.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    That should do it : ) Very cool look! Also, it looks like the end may be about 20mm square, so in theory you could even mount a fan sideways, to leave the slots visible and not covered by a fan.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • 14rhb
    14rhb over 7 years ago in reply to shabaz

    Thank you. That is a very good idea - blowing the air through (towards the ethernet) will have a clearer flow than downwards. The end measures 15mm so it is still possible. I could also add two more fins on the outside of the stack.

    • Cancel
    • Vote Up +3 Vote Down