Project14
  • Challenges & Projects
  • More
Project14
Polls Project14 | Live Stream & MATRIX Creator Giveaway: You Decide the Topics!
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 26 Feb 2019 8:36 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 3656 views
  • Likes 0 likes
  • Comments 22 comments
Related
Recommended

Project14 | Live Stream & MATRIX Creator Giveaway: You Decide the Topics!

Thank you for Voting!  Live Stream Title has been Announced:

 

Home Automation Using the MATRIX Creator: an element14 Story: Episode 1

 

Presented by Community Members! 

 

Special Guest MATRIX Labs and a Project14 Show & Tell from Sean_Miller  & gam3t3ch !

 

Keep the conversation flowing and feel free to vote on a topic of interest to you.  You could still win a MATRIX Creator for making this discussion memorable!

 

We'll be giving away MATRIX Creators for questions that lead to a great discussion!

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • samreen.islam
    samreen.islam over 7 years ago in reply to samreen.islam +7
    Additionally, MATRIX OS has been deprecated and is no longer supported, but you can check out our documentation to see how to use our other library layers MATRIX HAL (C++), MATRIX Core (JavaScript and…
  • jomoenginer
    jomoenginer over 7 years ago +4
    Knowing when or if they plan to fix the dead links on their site and github repos would be helpful. Some sort of schematic of the board would be handy as well; although I do understand it is a closed architecture…
  • fyaocn
    fyaocn over 7 years ago +4
    Just got one MATRIX Creator. Really great design and ongoing development. Even the FPGA bit-stream code is open sourced in github. But really take efforts to understand each part of the sensors and parts…
Parents
  • fyaocn
    fyaocn over 7 years ago

    There have been some problems with MATRIX installation. It appears that some file missing (possibly, systemd-sysv ) in the Sketch Mirror site, even I have changed /etc/apt/source.list sereral time.

    So the matrixio-creater-init can not be installed with package.

    It would be better if build from source would be released later, for more other OS like Ubuntu or Centos on RP3.

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fyaocn
    fyaocn over 7 years ago

    There have been some problems with MATRIX installation. It appears that some file missing (possibly, systemd-sysv ) in the Sketch Mirror site, even I have changed /etc/apt/source.list sereral time.

    So the matrixio-creater-init can not be installed with package.

    It would be better if build from source would be released later, for more other OS like Ubuntu or Centos on RP3.

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vimarsh_
    vimarsh_ over 7 years ago in reply to fyaocn

    Ya I am facing the same issue.

    Although if I flash the image matrix provides. The Matrix_Dev_Day_final then it works

    but on fresh linux, it causes errors in installation

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • samreen.islam
    samreen.islam over 7 years ago in reply to fyaocn

    Hello,

     

    You are having trouble with the Picroft installation? Have you tried --fix-missing like it suggests in the terminal? Sometimes that helps.

     

    Best,

    Samreen

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • samreen.islam
    samreen.islam over 7 years ago in reply to vimarsh_

    Hi vimarsh_,

     

    Are the errors you are referring to similar to the ones F. Yao posted?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to samreen.islam

    The address that is failing does not appear to be the one for the mirror that is added to the .list files.

    nslookup www.ustc.edu.cn
    
    
    Non-authoritative answer:
    Name: www.ustc.edu.cn
    Address: 218.104.71.168

     

    Also, there is a new snapshotindex.txt that was updated yesterday so perhaps if there was an issue the server was being backed up.

    http://mirrors.ustc.edu.cn/raspbian/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 7 years ago in reply to samreen.islam

    I have tried almost all the solution.

    --fix-missing is to save time for Dependancy Resolve.

    It really takes me time to find out that,

    a) The HAL lib for matrix Creator is good, but the problem is in Raspbian Strech. There have been many new features other than that of Jessie. Especially after including SNAP installation. The www.ustc.edu.cn  is one of mirror sites for raspbian, it synchronizes everyday with MAIN retro.

    After rull out the possiblility of ANTI-VIRUS or other Proxy SCREEN MECHNISM, it can be concluded that in this case, some files missing in the RASPBIAN site. So, there is little you can do other than waiting for new UPGRADE from RASPBIAN mirrors.

    b) Here is the assumption,

    Since apt-get intall maxtrio-creator-init fails without apt-get install upgrade first, you can test by not strictly defining version of DEPENDACY PACKAGES.  It may works. And test the HAL package in other Debian-like OS, it may works. I will test later in ubuntu-Mate and Debian-ARM.