Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects - Enchanted Clock (#3)
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
  • Author Author: dwinhold
  • Date Created: 4 Apr 2015 11:11 PM Date Created
  • Views 909 views
  • Likes 6 likes
  • Comments 4 comments
  • enchanted_objects
  • enchanted_clock
Related
Recommended

Enchanted Objects - Enchanted Clock (#3)

dwinhold
dwinhold
4 Apr 2015

Hello everyone,

 

So I have been programming the Arduino for enchanted clock I'm building (Work in progress). I am still having issues with the SAMA5D4 Xplained, I may have to change to an RPi if time starts to get tight. I really don't want to do this as our sponsors have been very generous and I don't want to let them down.

 

So to update where I am at. I have decided that for the clock to stay in time due to the inconsistency in a wood clock, I have made a binary clock. This clock will be integrated with my wood clock and through servos it will re-set it to the correct time. Below is a picture of the Binary Clock on the breadboard working. I will make a PCB board cape for final product. The time on the Binary Clock will be seen as well as the wood clock time.

 

image

 

 

Schematic:

image

Clock Code:

 

#include <Wire.h>
#include <RTClib.h>
#include <TimerOne.h>

byte numPins = 5;
byte ledPins[] = {2, 5, 8, 10, 12};

byte hourLeds[][2] = {{1, 3}, {3, 1}, {0, 3}, {3, 0}};
byte minLeds[][2] = {{4, 2}, {3, 4}, {2, 3}, {1, 2}, {0, 1}, {2, 0}};
byte secLeds[][2] = {{2, 4}, {4, 3}, {3, 2}, {2, 1}, {1, 0}, {0, 2}};

RTC_DS1307 RTC;

int hour, min, sec;

void setup()
{
  Wire.begin();
  if (! RTC.isrunning())
  {
    RTC.adjust(DateTime(__DATE__, __TIME__));
  }
  Timer1.initialize(20000); // uS
  Timer1.attachInterrupt( refresh );
}

void loop()
{
  static long lastTick;
  long thisTick = millis();
  if (thisTick > lastTick + 500l) // every 0.5 seconds
  {
    DateTime now = RTC.now();
    hour = now.hour();
    min = now.minute();
    sec = now.second();
    lastTick = thisTick;
  }
  refresh();
}

void refresh()
{
  int s = sec;
  int m = min;
  int h = hour;
  for (int bit = 0; bit < 6; bit++)
  {
    if (s & 1)
    {
      setLed(secLeds[bit]);
     // delay(10);
    }
    s = s >> 1;
    if (m & 1)
    {
      setLed(minLeds[bit]);
    }
    m = m >> 1;
    if (h & 1 && bit < 4)
    {
      setLed(hourLeds[bit]);
    }
    h = h >> 1;
   }
   allOff(); // so last led not brighter
}

void setLed(byte pins[])
{
  byte plusPin = ledPins[pins[0]];
  byte minusPin = ledPins[pins[1]];
  allOff();
  pinMode(plusPin, OUTPUT);
  digitalWrite(plusPin, HIGH);
  pinMode(minusPin, OUTPUT);
  digitalWrite(plusPin, LOW);
}

void allOff()
{ 
  for (byte pin = 0; pin < numPins; pin++)
  {
    pinMode(ledPins[pin], INPUT);
  }
}

 

Servo controller and timing sensor to be programmed into the script, this is for the clock only (so far).

 

My big focus is on the wooden clock, this is a huge part in the whole project. I will update mid week with photos of the progress.

 

Dale & Chrystal Winhold

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +2
    Good job. Like the idea of a binary clock.
  • Workshopshed
    Workshopshed over 11 years ago +2
    It took me a while to work out the LED wiring but I got it eventually, very cunning.
  • mcb1
    mcb1 over 11 years ago +2
    How long did it take you to work out that wiring. I had a headache just trying to follow it ... full marks. Mark
  • dwinhold
    dwinhold over 11 years ago in reply to mcb1

    When i started the wiring I had hair, I now am bald!! I have done a PCB cape with CADsoft, I will upload the .brd File for those who would like it. My family thinks the binary clock is pretty cool, but confusing. For those who don't know how to read the time off of the binary clock, here is a quick description:

     

    BInary language works on 0's and 1's, on or off. The first light is 0 or 1, the second is 0 or 2, third is 0 or 4... Etc. So, if the seconds line = 001101 this would be 44 seconds. Explained: with the 3rd, 4th and 6th light on you add 4 + 8 + 32.

    the hour line only has 4 lights as we only need to goto 12, eg.. 0011 = 12 or 1010 = 5

     

    TIme on my clock in picture:

    110000 : Seconds

    010100 : Minutes

    0111 : Hours

     

    14:10:03 or 2:10:03 pm

     

    Easy, eh!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    How long did it take you to work out that wiring.

    I had a headache just trying to follow it ... full marks. image

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    It took me a while to work out the LED wiring but I got it eventually, very cunning.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    Good job. Like the idea of a binary clock.