Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - Remodelling the Enchanted Cottage
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
  • Author Author: Workshopshed
  • Date Created: 21 Mar 2015 9:59 PM Date Created
  • Views 2363 views
  • Likes 7 likes
  • Comments 8 comments
  • enchanted_cottage
  • enchanted_objects
Related
Recommended

Enchanted Objects Design Challenge - Remodelling the Enchanted Cottage

Workshopshed
Workshopshed
21 Mar 2015

The way things were

Matilda'a father had worked his life in the coal mine so she was no stranger to a bit of hard labour. As a child she'd played at being a miner, smashing rocks in the back yard of their terraced house with a small hammer.

 

Today she had a much bigger hammer. She'd already supported up the archways with props and removed the old fashioned glass thermometer, so it was just a case of removing the front wall. A bit of persuasion with a sledge hammer and the front wall was turned to a pile of rubble. As she stared at the burnt out shell of a house she thought back to how it was when they first moved into their woodland cottage.

 

The cottage was a strange design with two arches at the front. A long beam spanned the house and pivoted in the middle. The beam was linked to a twisted shank of cord made from "cat gut" although they had been assured that no cats had been harmed in it's making. The cord had a strange property and acted as a simple hygrometer, when the air was damp the cord loosened and unwound moving the beam but when it was dry it twisted back up and moved the beam in the opposite direction.

 

Matilda had never liked that beam, it moved her in an arc and meant that there needed to be a large gap in the front wall.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A new beginning

Hans sketched out a rough schematic of the new control system, the power to the cottage was erratic so they did not want to rely on a main supply, the YUN did not have a regulator so Hans knew he was going to need some kind of circuitry for that and perhaps it would be good to charge the battery when there was power available. "Perhaps we could put some solar panels on the roof", he thought out loud. "One step at a time" suggested Matilda and Hans agreed.

 

image

A visit to the Town Faire

After her exertion, Matilda took a well deserved break and went with Hans to visit the town faire. Between the stalls and rides Matilda spotted something from her childhood. The town historical society had restored one of the old locomotives that pulled the coal wagons. She marvelled at how it's linkages converted the linear motion of the pistons into rotary motion for the wheel. When she got home she sketched out a mechanism for connecting up the servo to the movement in and out of the house.

image

Next Enchanted Objects Design Challenge - Matilda is not happy

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +2
    I do like the mechanical cuckoo clocks, there's one outside the old Swiss Centre in Leicester Square and I've also seen some in Germany and Switzerland. The company that made my object started out as workshop…
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1 +1
    Like Matilda having that beam and a hole in the front of the wall is one of the things I dislike about the traditional approach. I made a prototype of the mechanism with split pins and card, I need to…
  • crjeder
    crjeder over 11 years ago +1
    WoW your are raising the bar by a huge margin. I probably won't be able to keep up!
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1

    Cheers Mark a good suggestion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    I need to measure their current draw to be able to size my battery appropriately

    Don't forget the large capacitor so that the start current of the servo motor doesn't cause glitches....

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    Hopefully will be looking at the servos this week, I need to measure their current draw to be able to size my battery appropriately.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to crjeder

    Well it is a marathon rather than a sprint so I'm only planning a post per week for the first few weeks. At the end if I have the content it will get published as it comes.

    I uncovered a bug with the E14 CMS in that posts are shown in created rather than published order so that might mean some of the things I've already drafted will have to get copied and pasted into new posts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 11 years ago

    WoW your are raising the bar by a huge margin. I probably won't be able to keep up!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>