Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Blog [real_time_monitor] Real Time Player Monitoring System Post#1 : Introduction
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
  • Author Author: ravi_butani
  • Date Created: 2 Dec 2014 4:30 AM Date Created
  • Views 2337 views
  • Likes 2 likes
  • Comments 10 comments
  • analog_devices_inc
  • tektronix
  • real_time_monitor
  • sudden_impect
  • electrolube
Related
Recommended

[real_time_monitor] Real Time Player Monitoring System Post#1 : Introduction

ravi_butani
ravi_butani
2 Dec 2014

Table of Contents

Next >>


First of All I would like to Thank Elemen14, Tektronix, Analog Devices, Leeds Beckett University and Electrolube for showing potential in my application and selecting the same for this challenge..


In my first blog post I would like to introduce my project proposal for your suggestions and feedbacks... 


Project proposal: Designing of low cost and battery powered wearable sensor module to stream and monitor, vital body parameters of sport person on Android/IoS Smartphone and MacOS/Windows/Linux PC  using WiFi or on MacOS/Windows/Linux PC using long range Sub GHz transceiver at monitoring station.

Vital body parameter includes,

  1. Real time three axis acceleration data of impact on head(Helmet), Chest and spinal column of sport person.
  2. Real time ECG Heart rate and body temperature.


Targeted sports: Football, American Football, Ice hockey, Car racing, Bike racing, Ski run and any other sport that required real time monitoring of sport person vital health parameter in field.
Description: The system consists of two subsystems.

  1. Wearable sensor modules
    1. Chest belt
    2. Helmet
  2. Long range Sub-GHz RF receiver module at monitoring station. (optional if WiFi range is not sufficient in large sport field like ski runs, mountain biking etc…)

1.  A. Wearable sensor module as chest belt :

  • Battery operated wearable chest belt includes High-g (ADXL377) and Low-g (ADXL362) accelerometer on chest and back, AD8232 heart rate monitor with ECG probes and ADT7420 and ADT7320 body temperature sensor.
  • It also works as hub for other Helmet sensor module connected to this chest belt using wire (or wireless if it is inconvenient).
  • CC3200 WiFi module will be used for transmitting all real time data to Monitoring Station (Smart Phone/PC) using UDP protocol to ensure data transfer at near real time. (I am targeting 500kbps data rate).
  • If WiFi range is not sufficient, The module can transfer data to monitoring station using Long range Sub-GHz transceiver (This is my PlanB).
  • Electrolube clear polyurethane resin will be used to mold the sensors to ensure convenient of player, Survival of system in multiple impacts, Water resistance and increase reuse cycle.
  • This module will be powered by 3.7V rechargeable lithium battery and able to provide at least 120 Minutes of battery backup that will be sufficient in most of sports.
  • To ensure ease of use of the system, This module have simple push button to turn it on.
  • This module also provide alert of critical situation on monitoring station as well as using blinking of LED on module itself.
  • Design and programming will be completely open source and I will try my best to design Arduino like liberary for this system.

1.  B. Wearable sensor module at Helmet:

  • ADXL377 and ADXL362 Accelerometer based module will be designed to measure acceleration / impact experienced on players head and mounted on helmet.
  • This module sends data to chest belt module by wire (or wireless if it is inconvenient).

2.  Long range Sub-GHz RF receiver module at monitoring station:

  • This module is optional and only used if WiFi range is not sufficient in large sport field like ski runs, mountain biking etc…).
  • By plugging this module in Laptop/PC USB port, all real time data will be available for analysis and visualization on Laptop/PC.

High level block diagram of system is given below....image

Software:

  • Soft ware application for Smartphone and Laptop/PC will be designed using Java and Qt for provide graphical interface for visualize and analyze real time data.
  • Option for storage of data will be also provided so further detailed analysis on data carried out. This application will be completely opensource.

imageimage

Above images shows wearing of modules...
Usage of components provided by organizers:

  1. AD8232-EVALZ : As heart rate monitor
  2. EVAL-ADUCM350EBZ : AFE for other sensors
  3. EVAL-ADT7320FBZ : Body temperature sensor
  4. EVAL-ADXL375Z/ EVAL-ADXL375Z-M/ EVAL-ADXL377Z : High-g acceleration/ sudden impact measurement.
  5. EVAL-ADXL362Z /EVAL-ADXL362Z –MLP : Low-g acceleration measurement.

Here all this evaluation kits are used for initial prototyping purpose only but at final stage of development all important parts from kit will be integrated on standalone PCB to increase reliability of system, Improve form factor, Reduce cost and Make it wearable in true sense.

  • Electrolube UR5562 and UR5041 - polyurethane resin for molding system parts on Helmet/ Chest belt.
  • Tektronix TDS1202B-EDU DSO : Will be helpful as measuring instrument in prototyping process.

Budget utilization:

  1. ECG Probes (10 nos.) : $50
  2. PCB Design and fabrication: $100
  3. CC3200 Launch pad and LiPo Battery : $50
  4. Misc prototyping Components : $100
  5. Pair of Long range Sub-GHz RF transceiver: $50

 

Your feedback and suggestions are heartily welcome...

 

Thanks,

 

Ravi

  • Sign in to reply

Top Comments

  • sunnyiut
    sunnyiut over 11 years ago +1
    Hello Ravi, it sounds awesome to me. however, I am not so sure, but may be lithium-ion battery will be better than li-po for this project. Because you don't require too much current at an instance in your…
  • DAB
    DAB over 11 years ago +1
    Very good Post. All I would ask is for you to use a little larger type for the description. When you get older, you will understand. DAB
  • ravi_butani
    ravi_butani over 11 years ago in reply to sunnyiut +1
    Completely agree with you... for Lithium battery selection.
  • tomaja
    tomaja over 11 years ago in reply to mcb1

    Yes, those protective bags are good, I agree. I forgot about them... might be a good choice to use one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to tomaja

    Adafruit have a series of LiPo that are 1C (ie only discharge at the single amp/hr rate) and include overcurrent protection.

     

    Most accidents happen when they have been dropped and or overcharged.

    You can also get proper bags which some RC car racing clubs insist on the cars and batteries having.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 11 years ago in reply to ravi_butani

    Hi Ravi,

    I plan to use a Li-Fe battery since it's much safer for wearable electronics (Lithium iron phosphate battery - Wikipedia, the free encyclopedia). Li-Po batteries are not very safe, they're inflammable and sometimes they even explode if mechanically damaged or overcharged or even when discharged too much.

    Well, maybe I'm too cautious but I'll try to get a proper Li-Fe battery for this project image I already have one but it's much bigger than required for this project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ravi_butani
    ravi_butani over 11 years ago in reply to sunnyiut

    Completely agree with you... for Lithium battery selection.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ravi_butani
    ravi_butani over 11 years ago in reply to DAB

    Thanks... DAB ur suggestion accepted.... From next post I will use big fonts...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>