![]() | An Open-Source platform to create digital devices and interactive objects that sense and control physical devices. | Arduino Tutorials |
| Arduino Projects |
Commercial Uses of Arduino - 5 Webinar Series
5 Free Webinars about commercial uses of Arduino and the new Arduino MKR range, starting Wednesday 19th of September. Also, don't forget our Arduino MKR giveaways.
The first webinar has now ended. to watch this recording. recording.
Continue joining Massimo and Dominic in our 5 Part Webinar Series below to explore the full range of commercial uses of Arduino, from using Arduino in to prototype, to using them within your production products.
We will also cover
- The new Arduino MKR Range
- What things to consider in an industrial or commercial enviroment
- Data Logging
- IIoT Security
- Computer Vision
- Introduction to FPGA with the Arduino Vidor 4000
- IIoT connectivity such as LoRa, NB-IoT, SigFox or WiFi
- RS-485, CAN, and Ethernet connectivity for your Arduino Projects
Our Speakers:
Massimo Banzi Interaction Designer, Teacher, Maker, Bottleneck Co-founder of Arduino | Dominic Pajak Product person. Engineer. Retro computing geek |
Project14 | Clustered MCUs: Anything Goes with Two or More MCUs!
Dates and Register for Free:
Arduino MKR: IoT prototype to production
| Wednesday 19th September 19:00 GMT 13:00 CDT
to watch this recording. recording. |
Arduino MKR and wireless IoT connectivity
| Wednesday 3rd October 19:00 GMT 13:00 CDT |
Industrial IoT applications with Arduino MKR
| Wednesday 16th January 2019 19:00 GMT 13:00 CDT |
Arduino MKR Vidor 4000 – democratizing FPGA
| Wednesday 31st October 19:00 GMT 13:00 CDT |
Commercial IoT applications with Arduino MKR
| Wednesday 14th November 19:00 GMT 13:00 CDT |
Current Contests:
Theme: Auto Hacks and Beyond!
| Auto Hacks and Beyond with the MKR WiFi 1010 Board and CAN Shield | ||
|---|---|---|
| Winners Announcement: Auto Hacks and Beyond: Show Us How You Would Use the Arduino MKR WiFi 1010 Board and CAN Shield! | Arduino Projects | |
Arduino MKR WiFi 1010 Board | Arduino MKR CAN Shield | |
![]() | ![]() | |
| Buy NowBuy Now | Buy NowBuy Now | |
The MKR WIFI 1010 is equipped with an ESP32 module from U-BLOX. It speeds up and simplifies prototyping of WiFi based IoT It aims to speed up and simplify the prototyping of WiFi based IoT applications using the ESP32 module and low power consumption. The board is composed of three main blocks:
The MKR WIFI 1010 includes 32-bit computational power, a rich set of I/O interfaces, and low power Wi-Fi with a Cryptochip for secure communication using SHA-256 encryption.
The Arduino Software (IDE) simplifies code development and programming. Ideal for IoT battery-powered projects in a compact form.
Its USB port can be used to supply power (5V) to the board. It has a Li-Po charging circuit that allows the Arduino MKR WIFI 1010 to run on battery power or an external 5 volt source, charging the Li-Po battery while running on external power. Switching from one source to the other is done automatically. | With this shield you can easily connect to a CAN (Controller Area Network) Bus. Discover new possibilities of interaction between your Arduino MKR Board and the CAN ecosystem.
The MKR CAN shield can simplify the connection of the MKR boards with industrial systems and especially with automotive applications.
This shield opens a new set of possible applications like smart vehicles, autonomous cars and drones. A CAN connection also provides the possibility to connect a MKR board directly with several types of industrial grade sensors, motors and displays.
The MKR CAN shield allows a MKR board to connect to the CAN bus using the MCP2515 SPI to CAN chip.
The Arduino MKR CAN Shield uses the MCP2515 chip by Microchip. This chip is an industry standard.
The switch close to the CAN bus connector allows to enable or disable the termination resistor. | |
| ||
Arduino MKR WiFi 1010 Pinout, SAMD21 Pin Mapping, Tech Specs, Github Links, Schematics, and More!
Theme: Clustered MCUs
Anytime from now until October 15th, the Clustered MCUs you can win an MKR1000 kit, an MKR to Uno Adapter Shield, and an Arduino Uno by coming up with the craziest combination of two or more microcontrollers.
| Project14: Clustered MCUs | ||
|---|---|---|
| Project14 | Clustered MCUs: Anything Goes with Two or More MCUs! | Clustered MCUs | |
![]() | ![]() | |
| Buy NowBuy Now | Buy NowBuy Now | |
The kit is based around the MKR1000—a powerful board that combines the functionality of the Zero and the Wi-Fi Shield—and enables Makers to add connectivity to their designs with minimal prior networking experience.
Each bundle includes: 1 Arduino MKR1000 board, with header soldered. 1 micro USB cable, 1 400-point breadboard, 70 solid-core jumper wires, 1 9V battery snap, 1 stranded jumper wire, 6 phototransistors, 3 potentiometers (10 kilohm),10 pushbuttons,1 temperature sensor (TMP36),1 tilt sensor, 1 alphanumeric LCD (16 x 2 characters), 1 bright white, 34 LEDs (1 bright white, 1 RGB, 8 red, 8 green, 8 yellow, 3 blue), 1 small DC motor (6/9V), 1 small servo motor, 1 piezo capsule (PKM17EPP-4001-B0), 1 H-bridge motor driver (L293D), 1 octocouplers (4NE5), 2 MOSFET transistors (IRF520), 5 capacitors (100uF), 5 diodes (1N4007), 3 transparent gels (R,G,B) 1 male pin strip (40 x 1), 20 resistors (220 ohm), 5 resistors (560 ohm), 5 resistors (1 kilohm), 5 resistors (4.7 kilohm), 20 resistors (10 kilohm), 5 resistors (1 megohm), 5 resistors (10 megohm)
Included Projects: I Love You Pillow, Puzzle Box, Pavlov's Cat, The Nerd, and Plant Communicator, |
| |
Submission Deadline: Submit any project that combines two or more microcontrollers from now until October 15th! | ||
Theme: The Smarter World Challenge
| The Smarter World Challenge: Build a Smarter World with the MKR WAN 1300 Board and Relay Proto Shield | |||
|---|---|---|---|
The Smarter World Challenge | Arduino Projects | ||
![]() | ![]() | ||
|
| ||
| Buy NowBuy Now | Buy NowBuy Now | ||
Arduino MKR WAN 1300 allows you to add Lo-Ra connectivity to your projects with minimum previous experience in networking. It is based on the:
Its design allows you to power the board using two 1.5V AA or AAA batteries or external 5V. Switching from one source to the other is done automatically.
It features 32 bit computational power similar to the MKR ZERO board, the usual rich set of I/O interfaces, low power Lo-Ra communication and the ease of use of the Arduino Software (IDE) for code development and programming.
All these features make this board the preferred choice for the emerging IoT battery-powered projects in a compact form factor. The USB port can be used to supply power (5V) to the board. The Arduino MKR WAN 1300 is able to run with or without the batteries connected and has limited power consumption. | The MKR Relay Protoshield allows you to easily add relays to your MKR board based project. The shield provides two relays:
The shield also provides easy connection by means of screw terminal blocks to A1 to A4 analog inputs, I2C and supply voltages.
| ||
| |||
Here is a GitHub Link to Getting Started with the MKR WAN 1000:
https://github.com/gonzalocasas/arduino-mkr-wan-1300
Here is a GitHub link that provides an APIs to Communicate with LoRa and LoRaWAN Networks:
https://github.com/arduino-libraries/MKRWAN
Upcoming Contests:
Theme: You Decide the FPGA Theme
A Poll where You Decide the FPGA Theme will take take place and include the Following:
| Arduino MKR Vidor 4000 (on board FPGA) | Arduino ETH Shield | |
|---|---|---|
![]() | ![]() | |
| Buy NowBuy Now | Buy NowBuy Now | |
| Are you developing a project for an environment where wireless connections are unavailable or would be inefficient?
The MKR ETH shield allows to have a wired Ethernet connection between your MKR board and your network or the Internet. This is particularly useful for devices located where either electromagnetic noise is a problem or there are special safety requirements. |
| Arduino MKR MEM Shield | Arduino MKR Relay Shield |
|---|---|
![]() | ![]() |
| Buy NowBuy Now | Buy NowBuy Now |
The Arduino MKR MEM shield will allow you to add more flash memory and storage. It provides 2-megabytes of flash memory. It also includes a slot for adding a microSD card to store several gigabytes of storage. This can allow you to store data for later analysis. | The MKR Relay Protoshield allows you to easily add relays to your MKR board based project. The shield provides two relays called RELAY1 and RELAY2 commanded by pin 1 and pin 2 respectively. The shield also provides easy connection by means of screw terminal blocks to A1 toA4 analog inputs, I2C and supply voltages. Operating voltage 3.3V (supplied from the host board) Two relays with NO, COM and NC connections Works with battery powered board Screw terminal blocks for easy connections Carry current: 2 A Max. operating voltage: 125 VAC, 60 VDC Max. operating current: 1 A Max. switching capacity: 62.50 VA, 30W |
| Arduino MKR RS 485 | Arduino MKR Connector Carrier |
|---|---|
![]() | ![]() |
| Buy NowBuy Now | Buy NowBuy Now |
Thanks to this shield, you can now connect your MKR board to any of the industrial systems that using the RS 485 protocol. The MKR 485 shield is the ultimate expansion that allows MKR boards to connect to almost any legacy industrial system, such as industrial PLCs, controllers, drives and HMIs. Old industrial systems (e.g., machinery, heating systems, and conveyors) can to turned into IoT devices through a serial connection using the MKR 485. | Do you have several components to connect to your project and would rather use connectors instead of soldering? The Arduino MKR CONNECTOR CARRIER provides Seeed Studio's Grove connectors to your MKR board. The MKR CONNECTOR CARRIER shield is an essential tool for rapidly prototyping activity. It allows you to connect easily and quickly sensors with Grove connectors. This shield can allow you to build applications with different IoT connectivities by simply changing the MKR board and with almost no changes to the code. |
Make ANY of the Above MKR Themes a "Panini" by mixing and matching FROM following MKR shields to Your Project!*
*This applies to Auto Hacks, Smarter World Challenge, and the Upcoming FPGA Contest.
| Arduino MKR ETH Shield | Arduino MKR Connector Carrier |
|---|---|
![]() | ![]() |
| Buy NowBuy Now | Buy NowBuy Now |
Are you developing a project for an environment where wireless connections are unavailable or would be inefficient? The MKR ETH shield allows to have a wired Ethernet connection between your MKR board and your network or the Internet. This is particularly useful for devices located where either electromagnetic noise is a problem or there are special safety requirements. | Do you have several components to connect to your project and would rather use connectors instead of soldering? The Arduino MKR CONNECTOR CARRIER provides Seeed Studio's Grove connectors to your MKR board. The MKR CONNECTOR CARRIER shield is an essential tool for rapidly prototyping activity. It allows you to connect easily and quickly sensors with Grove connectors. This shield can allow you to build applications with different IoT connectivities by simply changing the MKR board and with almost no changes to the code. |
| Arduino MKR MEM Shield | Arduino MKR Relay Shield |
|---|---|
![]() | ![]() |
| Buy NowBuy Now | Buy NowBuy Now |
The Arduino MKR MEM shield will allow you to add more flash memory and storage. It provides 2-megabytes of flash memory. It also includes a slot for adding a microSD card to store several gigabytes of storage. This can allow you to store data for later analysis. | The MKR Relay Protoshield allows you to easily add relays to your MKR board based project. The shield provides two relays called RELAY1 and RELAY2 commanded by pin 1 and pin 2 respectively. The shield also provides easy connection by means of screw terminal blocks to A1 toA4 analog inputs, I2C and supply voltages. Operating voltage 3.3V (supplied from the host board) Two relays with NO, COM and NC connections Works with battery powered board Screw terminal blocks for easy connections Carry current: 2 A Max. operating voltage: 125 VAC, 60 VDC Max. operating current: 1 A Max. switching capacity: 62.50 VA, 30W |
| Arduino MKR RS 485 | |
|---|---|
![]() | |
| Buy NowBuy Now | |
Thanks to this shield, you can now connect your MKR board to any of the industrial systems that using the RS 485 protocol. The MKR 485 shield is the ultimate expansion that allows MKR boards to connect to almost any legacy industrial system, such as industrial PLCs, controllers, drives and HMIs. Old industrial systems (e.g., machinery, heating systems, and conveyors) can to turned into IoT devices through a serial connection using the MKR 485. |
The Grand Prize
After all the the MKR boards and shields have been sent out we'll be awarding an Arduino Engineering Kit to the best project that shows how an engineer would use the MKR line to repurpose an existing project or a new project.
| Arduino Engineering Kit - MATLAB/SIMULINK | ||
|---|---|---|
![]() | ![]() | |
| Buy NowBuy Now | ||
Each Arduino Engineering Kit includes:
BOARDS
ELECTRICAL COMPONENTS
| COMPONENTS
| |
The Arduino Engineering Kit is the ideal solution for university students, providing a state-of-the-art, hands-on incorporation of Arduino technology in an educational setting.
The kit is primarily for three types of users:
The Arduino Engineering Kit covers fundamental engineering concepts, key aspects of mechatronics, and MATLAB and Simulink programming.Included projects challenges students intellectually and helps develop physical engineering skills — and they’re just fun to do.
The kit is sold in a hard plastic, stackable tool box for storage and years of reuse. Inside the box is an easy-to-use Arduino MKR1000 board, several customized parts, and a complete set of electrical and mechanical components needed to assemble all three projects | ||
You Have Until December 18th, 2018 to Complete Your Project to Qualify for the Grand Prize!























-
luislabmo
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
luislabmo
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children