Enroll in the RoadTest: Richtek Synch. Step-Down Converter EVB_RT6204GSP
Click here to join the live webinar now
password: element14
| {tabbedtable} Tab Label | Tab Content |
|---|---|
| About This Webinar | RT6204 is a buck step-down voltage regulator for applications with very wide input voltage range. In this webinar we will highlight some features of RT6204, show some applications where RT6204 can be used, and explain how to design the RT6204 application circuit. Richtek has also developed a Fast Load Transient tool that can be used to quickly test the stability of voltage regulators. The use of the tool is explained with an example application of RT6204.
RT6204 is a buck step-down voltage regulator RD0004 Load Transient Tool |
| The Presenter | Presenter:Roland van Roy
Roland is the Field Application Manager for the Richtek Europe region. He has worked in consumer electronics and power electronics field in Europe and Asia for more than 25 years. |
| Webinar Recording |
|