Webinars, Training and Events
  • Learn
  • More
Webinars, Training and Events
Forum Circuit Isolation, Ground Loops, and Avoiding Component Failures
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Webinars, Training and Events to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 1054 subscribers
  • Views 650 views
  • Users 0 members are here
Related

Circuit Isolation, Ground Loops, and Avoiding Component Failures

rscasny
rscasny over 8 years ago

Why do electronic circuits employ circuit isolation?

 

Well, there are a lot of sensor applications where it is useful for the sensor to have no direct galvanic electrical connections with the system to which it is supplies data. One reason this is so is to avoid the risk of dangerous voltages or currents from one half of the system causing a catastrophic failure in the other half. Another reason is to eliminate ground loops.

 

Perhaps the most common way to employ circuit isolation is with utilizing transformers (magnetic isolation). Opto-isolators are yet another way. They are made up of an LED and a photocell (optical isolation).  Another way is using small high voltage capacitors (capacitive isolation). 

 

As you gain electronics knowledge you will see more and more uses for digital isolators. The figure below presents a very simple isolator application. Here the entire circuit constitutes a  low-voltage system in which a digital isolator connects the SPI interface of a controller with the SPI interface of a data converter.

image

ISOLATED SPI INTERFACE

 

To learn more about the need for circuit isolation and digital isolators, I encourage you to sign up for the webinar: TI Webinar: Understanding Capacitive Isolation Technology for Industrial Applications

 

 

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago

    Jan Cumps and I have been running some projects for a while using TI Digital isolators at there main interface too, here is the DC Programmable Load project as an example Programmable Electronic Load  and also an earlier tutorial I published on E14 a while back https://youtu.be/BvIQ0b2gUFs

     

    Both using the I2C specific version but utilizing the same isolation technology, they work exceedingly well so I recommend watching this webinar if you can

     

    If you have other more pressing questions, you can also ask Jan or Myself

     

    Peter

     

    Oh, they also make excelent level shifters for driving systems perched on top of say mains or other high voltage (Relative to the Control system), this can be hundreds or in some cases over 1000V difference, just make sure you design the PCB appropriately image to handle creapage and arcing

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago

    Jan Cumps and I have been running some projects for a while using TI Digital isolators at there main interface too, here is the DC Programmable Load project as an example Programmable Electronic Load  and also an earlier tutorial I published on E14 a while back https://youtu.be/BvIQ0b2gUFs

     

    Both using the I2C specific version but utilizing the same isolation technology, they work exceedingly well so I recommend watching this webinar if you can

     

    If you have other more pressing questions, you can also ask Jan or Myself

     

    Peter

     

    Oh, they also make excelent level shifters for driving systems perched on top of say mains or other high voltage (Relative to the Control system), this can be hundreds or in some cases over 1000V difference, just make sure you design the PCB appropriately image to handle creapage and arcing

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer