Webinars, Training and Events
  • Learn
  • More
Webinars, Training and Events
Polls Take the PYNQ Poll: You know Python, but Do You Know PYNQ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Webinars, Training and Events to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 4 May 2019 5:06 PM Date Created
  • Last Updated Last Updated: 20 May 2020 3:06 PM
  • Views 1834 views
  • Likes 0 likes
  • Comments 11 comments
Related
Recommended

Take the PYNQ Poll: You know Python, but Do You Know PYNQ?

If you are a member of element14 and you're an embedded developer (or learning the craft), you probably know Python.

 

But do you know PYNQ (as in PINK)?

 

PYNQ is an open-source framework that makes programmable SoCs easier-to-use and more accessible to new FPGA users through a browser-based development environment for Python.

 

Sound interesting?

 

Want to learn more?

 

Then attend our PYNQ webinar on May 8th, called: Unlock the Power of FPGAs through Python: Building Reconfigurable Embedded Systems with PYNQ

 

If you attend the webinar, you'll learn how to get a free PYNQ-Z2 boardPYNQ-Z2 board

 

 

Don't forget to take the PYNQ Poll!!!

  • scasny
  • community survey
  • scasny_web
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • weiwei2
    weiwei2 over 6 years ago +5
    i use c, c++, c# much more than Python. But nowadays many things are good to start with Python. Pynq is one. However, i prefer to use distribution like Anaconda to deal with Python
  • genebren
    genebren over 6 years ago +3
    I am not a hater of newer languages, but I am very happy with C/C++. Learning a new language is just one of those things that I just can not seem to find the time for. Gene
  • Gough Lui
    Gough Lui over 6 years ago +3
    That should probably say ... "Other; please explain in comments (and I can't wait to attend the webinar) " I'd have to agree that I'm happy with C myself, but I can see that Python is quite popular and…
  • genebren
    genebren over 5 years ago in reply to ipv1

    Greetings!

     

    While the vast majority of my programming has been in C, I have used C++ on some projects.  In one my most memorable projects, I was following the lead of my manager, who was an absolute master in the concepts of reuse, where he had over the years constructed (and reused on several projects) a framework that allowed remote control of the device, which proved to me invaluable.  We could peek and poke into memory, call function/procedures, load functions into memory and call them, etc.  He constructed this framework in C++.  My main part of the project was image processing, which used a lot of C++ function template for sorting and the such, that made the coding much easier (it also used a lot of memory as there was a lot of overhead to these functions).

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 5 years ago in reply to genebren

    genebren Hi!

    You mentioned that you are content with C++ and so I have to ask. What is your application area for the language?

     

    I am asking from the work point of view. Though I am an electronics designer who if proficient at a bunch of languages, I am looking for the correct way to 'resume' my skills.

     

    Thanks in advance.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago

    Pynq is something I need to learn. The syntax is python like which is good. The unique features are embedded in the libraries. For me that is a doable learning curve. So into the bucket list.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago in reply to baldengineer

    Thanks, James. That makes it clearer - and makes a lot more sense. I just watched your video on the road test too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 6 years ago in reply to Fred27

    [Python] does seen a strange match for FPGA developmentIt does seem like a strange match up at first, but not so much when you see how it works together. Python isn't used for developing the FPGA, or what the Zynq calls the "programmable logic" layer. IP is still developed using the Xilinx Vivado toolchain.

     

    Python is used to load overlays which contain the FPGA/PL IP. It then acts as the glue between the hard ARM-A9 core and the FPGA core.

     

    In that context, Python makes much more sense. FPGA blocks are developed in VHDL/Verilog/RTL/HLS/etc. Code on the application processor, with the PYNQ image, runs Python under linux. The tight bindings accelerates gluing a hardware FPGA operation to a software function. The main example I looked at was OpenCV. The FPGA/PL layer communicates with HDMI and USB passing data over to the ARM processor. There, some Python code uses OpenCV to do facial recognition. It takes about 20 lines of Python code to make it work.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • leakun
    leakun over 6 years ago

    For zynq(unless we are using just the PS), C hardly can be used. It has support via the old HLS and currently SDSOC. PYNQ's Python is somewhat matching SDSOC in simplicity in my opinion but for a maker PYNQ is more welcoming. My client who try to use zynq for image processing have spent up to a year just to accomplish the image pipeline with VHDL and hardware prototype while the PYNQ can be used side by side for the algorithmn development to be carried out concurrently while waiting for the hardware prototype to be ready.

     

    But now there is a major and cheaper contender in the form of NVIDIA Jetson Nano at $99

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • weiwei2
    weiwei2 over 6 years ago

    i use c, c++, c# much more than Python. But nowadays many things are good to start with Python. Pynq is one. However, i prefer to use distribution like Anaconda to deal with Python image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago in reply to Fred27

    Answering my own question - it looks like your can run PYNQ on any Zynq board, but there will be some effort required building an SD card image. Only the Pynq Z1 and Z2 boards have prebuilt images available.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago

    I'm not a huge fan of Python and it does seen a strange match for FPGA development. I'll be watching the webinsr with interest to see if I can be convinced.

     

    The hardware looks nice, but I assume that the PYNQ framework will run on any Zync board such as the MiniZed

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 6 years ago

    That should probably say ...

    "Other; please explain in comments (and I can't wait to attend the webinar)"

     

    I'd have to agree that I'm happy with C myself, but I can see that Python is quite popular and has a lot of conveniences (as well as subtle pitfalls as well, which I'm learning about as I occasionally fall into them). I think it's a good thing that more languages are given the chance to be intimate with hardware - there have been various microcontroller boards which can be programmed in Lua, dotNet, VB, JavaScript, etc. I guess it's a good thing that lets prototype creators use what they are familiar with so that they don't (necessarily) have to learn an entirely different language ... many students nowadays are not necessarily starting with C anymore even though I think they probably should ...

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>