Learning Center
  • Learn
  • More
Learning Center
Blog 8Bit adder from discrete transistors
  • Blog
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Learning Center to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: RobinTheMaker
  • Date Created: 14 Nov 2024 1:50 PM Date Created
  • Views 7581 views
  • Likes 12 likes
  • Comments 6 comments
  • logic gate project
  • ciruit design
  • transistor
  • logic gates
  • pcb
  • adder
Related
Recommended

8Bit adder from discrete transistors

RobinTheMaker
RobinTheMaker
14 Nov 2024
In this project I tried to build the simplest calculater possible from discrete transistors in order to learn more about digital logic on the most basic level.

 started experimenting with single transistors on bread boards, building simple logic gates. The next step was to assemble the logic gates into a full adder. At first I used multiple different types of logic gates like in the following image.

image

I made the circuit on a breadboard and even build a second one to hook together. They worked as expected although the leds on the output were quite dim. But I didn't let that stop me and pushed trough with creating a PCB and ordered it. After hours of assembling half the board with 72 out of 144 transistors and twice as many resistors, I plugged it in only to see that the adders worked on their own but the carry out voltage was to low to turn on the next transistor. 

I created a simulation of the circuit with CircuitJS which showed me, that with my current architecture there are some cases where the voltage drop across the transistors is to great to turn on the next transistor. 

After some research I found an alternate design that only uses NOR gates that are very simple to implement with a single transistor and three resistors per gate. This effectivly cut the total number of transistors in half and made the design actually work. This time I tested everything in with simulations before ordering and assembling a PCB.

imageimage

I got the PCBs and was very exited because I had never ordered ones with ENIG imersion gold finish and together with the purple it just looks amazing. This is a show piece after all and I am planning on building a nice wooden enclousure for it. 
I started the assembly progress by first soldering the USB C with some solder paste and a hot air gun and then continued on to the first full adder. After soldering 9 transistors and over 30 resistors I had enough components on the board to test basic functionality. But after flicking the switches in all possible combinations all the output led's stayed dim and unlit and the panic started creeping in.
After a quick probing session with the multimeter I turned to the schematic and board layout in KiCad to reference some things. I found the coulprit quite fast. I don't know how it happend or how I never noticed it but at some point I messed up the connection between footprint and schematic. The pin numbers didn't mach up correctly. In the schematic the base of the transistor is pin number 1. On the physical part of the BC547b transistor the base is the middle leg but on the footprint the pins are numbered from left to right making the the base the left most pin.So after a short rage I came back to my senses and researched if there is a npn transistor with similar characteristics to the BC547b but the weird pin out I accidentally created. The only one I could find that might fit is the SC945 but I have to rotate it 180 degrees to make it align with the correct pins. 
I will post another update once I receive the new parts. Until then remember to double check your footprints even if they seem very simple.

GitHub

  • Sign in to reply

Top Comments

  • DAB
    DAB over 1 year ago +1
    One of my first purchases from the surplus market was an old RTL board from some computer, back in the 1960's. So your going back to that era for a project brought a smile to my face as I remembered…
  • Stuart_S
    Stuart_S 11 months ago +1
    We did this circuit in one of our digital practicals at Uni a while back (that was converted to VHDL) , build a half adder and full adder (half adder with carry). Our add with carry features two XOR, two…
Parents
  • Stuart_S
    Stuart_S 11 months ago

    We did this circuit  in one of our digital practicals at Uni a while back (that was converted to VHDL), build a half adder and full adder (half adder with carry). Our add with carry features two XOR, two ANDs and an OR -which appears as one of your bit adding modules. Maybe there's an exercise here using De-Morgan's theorem to reduce the chip count.  image

                                  Half Adder

    image

                         Full Adder

    I've included the truth tables and simulations for reference and support

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Stuart_S
    Stuart_S 11 months ago

    We did this circuit  in one of our digital practicals at Uni a while back (that was converted to VHDL), build a half adder and full adder (half adder with carry). Our add with carry features two XOR, two ANDs and an OR -which appears as one of your bit adding modules. Maybe there's an exercise here using De-Morgan's theorem to reduce the chip count.  image

                                  Half Adder

    image

                         Full Adder

    I've included the truth tables and simulations for reference and support