Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum PARALLEL CURRENT
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 1040 subscribers
  • Views 3789 views
  • Users 0 members are here
Related

PARALLEL CURRENT

salesm21
salesm21 over 8 years ago

Recently been thinking about the ways current flows through a parallel circuit and it confuses me. So all connections on a parallel circuit are at equal potentials with the source. So no two components are getting anymore or less energy than the others. However based on the resistive nature of that branch will determine the current that is pushed through that part. So id like to simplify this by taking two circuits with equivalent parts. Both circuits have a DC source of 10V and each has 5 resistors equaling 5 ohms each. In series each resistor would draw away not current but the energy that is propelling electrons down the conductor. The circuit has .4A of current.  In a parallel circuit all five have 10volts dropped on them and therefore each has its own current (In this case they would all be identical but each is drawing a separate current.) My question is where does all the extra current come from? Is it front the extra paths or was it always in the source?

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +4 suggested
    All current comes from the source that is providing the potential (assuming that it is an ideal source, with no series resistance). In the initial steps of understanding electronics the supply is ideal…
  • mcb1
    mcb1 over 8 years ago +3 suggested
    My question is where does all the extra current come from? Ohms law assumes the supply voltage and current is whatever your figure ends up. 5 x 5ohm resistors in series across 10v will be I=E/R = 10/25…
  • jw0752
    jw0752 over 8 years ago +1 verified
    Hi Mitchell, Many years ago when I was just starting in electronics I first encountered Ohms law. Using the formula I determined that I should be able to get an awesome flash of current by putting a dead…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Mitchell,

    Many years ago when I was just starting in electronics I first encountered Ohms law. Using the formula I determined that I should be able to get an awesome flash of current by putting a dead short across a 6 volt lantern battery. I got everything set up for the experiment and using a piece of 12 Gauge wire I made the connection. Needless to say there was no spectacular current. At the time there was no internet and I had no one around me that knew anything about electricity so the reason why my experiment failed remained a mystery to me for some time. I remember the aha moment when I eventually came across the idea of internal resistance in all power sources. Under normal operating conditions the internal resistance is low enough compared to the external resistance so that it is irrelevant. However as the external resistance gets lower and approaches the internal resistance it becomes a greater and greater factor. You can calculate the internal resistance by seeing how much the voltage of the battery drops when put it under an external load. Calculate the current in the circuit by measuring the voltage drop across the load and divide it by the resistance of the load. Next divide the voltage drop of the battery by the current and you will get an approximation of the internal resistance of your source at this current level. Keep in mind that the resistance of a source may not be linear with respect to external current as there are several factors that produce the internal resistance.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago

    Hi Mitchell,

    Many years ago when I was just starting in electronics I first encountered Ohms law. Using the formula I determined that I should be able to get an awesome flash of current by putting a dead short across a 6 volt lantern battery. I got everything set up for the experiment and using a piece of 12 Gauge wire I made the connection. Needless to say there was no spectacular current. At the time there was no internet and I had no one around me that knew anything about electricity so the reason why my experiment failed remained a mystery to me for some time. I remember the aha moment when I eventually came across the idea of internal resistance in all power sources. Under normal operating conditions the internal resistance is low enough compared to the external resistance so that it is irrelevant. However as the external resistance gets lower and approaches the internal resistance it becomes a greater and greater factor. You can calculate the internal resistance by seeing how much the voltage of the battery drops when put it under an external load. Calculate the current in the circuit by measuring the voltage drop across the load and divide it by the resistance of the load. Next divide the voltage drop of the battery by the current and you will get an approximation of the internal resistance of your source at this current level. Keep in mind that the resistance of a source may not be linear with respect to external current as there are several factors that produce the internal resistance.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer