Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum PARALLEL CURRENT
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 1040 subscribers
  • Views 3787 views
  • Users 0 members are here
Related

PARALLEL CURRENT

salesm21
salesm21 over 8 years ago

Recently been thinking about the ways current flows through a parallel circuit and it confuses me. So all connections on a parallel circuit are at equal potentials with the source. So no two components are getting anymore or less energy than the others. However based on the resistive nature of that branch will determine the current that is pushed through that part. So id like to simplify this by taking two circuits with equivalent parts. Both circuits have a DC source of 10V and each has 5 resistors equaling 5 ohms each. In series each resistor would draw away not current but the energy that is propelling electrons down the conductor. The circuit has .4A of current.  In a parallel circuit all five have 10volts dropped on them and therefore each has its own current (In this case they would all be identical but each is drawing a separate current.) My question is where does all the extra current come from? Is it front the extra paths or was it always in the source?

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +4 suggested
    All current comes from the source that is providing the potential (assuming that it is an ideal source, with no series resistance). In the initial steps of understanding electronics the supply is ideal…
  • mcb1
    mcb1 over 8 years ago +3 suggested
    My question is where does all the extra current come from? Ohms law assumes the supply voltage and current is whatever your figure ends up. 5 x 5ohm resistors in series across 10v will be I=E/R = 10/25…
  • jw0752
    jw0752 over 8 years ago +1 verified
    Hi Mitchell, Many years ago when I was just starting in electronics I first encountered Ohms law. Using the formula I determined that I should be able to get an awesome flash of current by putting a dead…
Parents
  • genebren
    0 genebren over 8 years ago

    All current comes from the source that is providing the potential (assuming that it is an ideal source, with no series resistance).

     

    In the initial steps of understanding electronics the supply is ideal (no limitations).  As you move forward in your understanding of electronics you will view sources as having real word limitations (some source resistance and some maximum current available).

     

    When you have resistors in parallel, they act as a single resistor, i.e your 5 resistors of 5 ohms each.  The equivalent resistance is 1 ohm. So for your example the total current flowing through the load would be 10A.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • genebren
    0 genebren over 8 years ago

    All current comes from the source that is providing the potential (assuming that it is an ideal source, with no series resistance).

     

    In the initial steps of understanding electronics the supply is ideal (no limitations).  As you move forward in your understanding of electronics you will view sources as having real word limitations (some source resistance and some maximum current available).

     

    When you have resistors in parallel, they act as a single resistor, i.e your 5 resistors of 5 ohms each.  The equivalent resistance is 1 ohm. So for your example the total current flowing through the load would be 10A.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer