Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum Experimenting with Op Amps: active full-wave rectifier
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 1033 subscribers
  • Views 12840 views
  • Users 0 members are here
  • opamp
  • analogue
  • analog
Related

Experimenting with Op Amps: active full-wave rectifier

Jan Cumps
Jan Cumps over 3 years ago

The Art Of Electronics features a set of practical op-amp circuits. They have several full-wave rectifiers. I'm trying the simplest one. You don't need fancy devices. A pair of 741s will do.

The circuit:

image
image source: my copy of the book. fair use.

Looking at the node where the arrow points to:

  • for positive values, the first op-amp is an inverting buffer.
  • for negative values, the op-amp output has a  0.6V dc bias, the right side of  the feedback resistor will be at 0 V (ground). 
    hint: the 0.6 V output is generated by the op-amp to drive the inverting input to the same value as the + input (ground), effectively clamping the output to 1 diode drop above ground.

image

Looking at the second op-amp:

  • it is an op-amp with a summing node. Two signals at the inverting input are summed and inverted. The amplification factor is defined by the input resistor and the feedback resistor.
  • for the input signal, the amplification = -1 * R/R = -1 (the input resistance equals the feedback resistance, resulting in the -1 amplification factor, doubling and inverting the signal)
  • for the signal coming from op-amp 1, the amplification = -1 * R / (R/2) = -2 (the input resistance is half the feedback resistance, resulting in the -2 amplification factor)
  • it is an inverting amplifier for the input. Both positive and negative signals are amplified by -1.
  • for the signal coming from the first op-amp, it acts as a -2 amplifier.
  • for positive inputs, this results in  Vin * -1 + Vin * -1 * -2 = -Vin + 2Vin = Vin ->  result: Vin, positive Vin comes out as positive Vin (see comment)
  • for negative inputs, this results in Vin * -1 (making Vin positive)  + Vin * 0 * -1 -> result -Vin: negative Vin comes out as positive Vin

image

Here is the result: The blue line is the output. Underneath it, you see the input. The output overlaps the input for the positive part. It inverses the negative part. No diode drop.

image

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +5
    If you are puzzled by the circuit, there is a way to understand it: Build the first op-amp circuit and feed a sinus into it. Try it with and without the vertical diode. Try to understand why it is…
  • anniel747
    anniel747 over 3 years ago in reply to Jan Cumps +4
    Deleted
  • javagoza
    javagoza over 3 years ago in reply to anniel747 +4
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    Measurements when the input is  -6 V dc.

    image

    You can see here that for negative inputs, the op-amp generates 0.6 V dc output to try and keep the - input at ground level (same level as + input).
    It generates just enough so that the output - the horizontal diode drop brings the input to ground.
    The vertical diode will not conduct in this scenario. To the circuit it looks as if it isn't there. This brings the node left of the 5K to 0 V (ground) 

    The second op-amp, the inverting summing amp, has different gain for both inputs. The gain = -(Rfeedback / Rin)
    For the original -6 V input, with gain -1 (-10K/10K), we'd get +6 V output.
    For the 0 V signal coming from the first circuit, with gain -2 (-10K/5K), we'd get 0V output
    Summed up, this is +6 V output.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago

    Measurements when the input is  -6 V dc.

    image

    You can see here that for negative inputs, the op-amp generates 0.6 V dc output to try and keep the - input at ground level (same level as + input).
    It generates just enough so that the output - the horizontal diode drop brings the input to ground.
    The vertical diode will not conduct in this scenario. To the circuit it looks as if it isn't there. This brings the node left of the 5K to 0 V (ground) 

    The second op-amp, the inverting summing amp, has different gain for both inputs. The gain = -(Rfeedback / Rin)
    For the original -6 V input, with gain -1 (-10K/10K), we'd get +6 V output.
    For the 0 V signal coming from the first circuit, with gain -2 (-10K/5K), we'd get 0V output
    Summed up, this is +6 V output.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    Measurements when the input is  +3.23 V dc.

    image

    You can see here that for positive inputs, the horizontal diode does not conduct, and the 10K feedback resistor comes into play.
    The 3.24 V input is inverted, and its inverse is passed to circuit 2.

    The second op-amp, the inverting summing amp, has different gain for both inputs. The gain = -(Rfeedback / Rin)
    For the original +3.23 V input, with gain -1 (-10K/10K), we'd get -3.23 V output.
    For the -3.23 V V signal coming from the first circuit, with gain -2 (-10K/5K), we'd get +6.46V output
    Summed up, this is +3.23 V output.