Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum Experimenting with Op Amps: active full-wave rectifier
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 1033 subscribers
  • Views 12842 views
  • Users 0 members are here
  • opamp
  • analogue
  • analog
Related

Experimenting with Op Amps: active full-wave rectifier

Jan Cumps
Jan Cumps over 3 years ago

The Art Of Electronics features a set of practical op-amp circuits. They have several full-wave rectifiers. I'm trying the simplest one. You don't need fancy devices. A pair of 741s will do.

The circuit:

image
image source: my copy of the book. fair use.

Looking at the node where the arrow points to:

  • for positive values, the first op-amp is an inverting buffer.
  • for negative values, the op-amp output has a  0.6V dc bias, the right side of  the feedback resistor will be at 0 V (ground). 
    hint: the 0.6 V output is generated by the op-amp to drive the inverting input to the same value as the + input (ground), effectively clamping the output to 1 diode drop above ground.

image

Looking at the second op-amp:

  • it is an op-amp with a summing node. Two signals at the inverting input are summed and inverted. The amplification factor is defined by the input resistor and the feedback resistor.
  • for the input signal, the amplification = -1 * R/R = -1 (the input resistance equals the feedback resistance, resulting in the -1 amplification factor, doubling and inverting the signal)
  • for the signal coming from op-amp 1, the amplification = -1 * R / (R/2) = -2 (the input resistance is half the feedback resistance, resulting in the -2 amplification factor)
  • it is an inverting amplifier for the input. Both positive and negative signals are amplified by -1.
  • for the signal coming from the first op-amp, it acts as a -2 amplifier.
  • for positive inputs, this results in  Vin * -1 + Vin * -1 * -2 = -Vin + 2Vin = Vin ->  result: Vin, positive Vin comes out as positive Vin (see comment)
  • for negative inputs, this results in Vin * -1 (making Vin positive)  + Vin * 0 * -1 -> result -Vin: negative Vin comes out as positive Vin

image

Here is the result: The blue line is the output. Underneath it, you see the input. The output overlaps the input for the positive part. It inverses the negative part. No diode drop.

image

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +5
    If you are puzzled by the circuit, there is a way to understand it: Build the first op-amp circuit and feed a sinus into it. Try it with and without the vertical diode. Try to understand why it is…
  • anniel747
    anniel747 over 3 years ago in reply to Jan Cumps +4
    Deleted
  • javagoza
    javagoza over 3 years ago in reply to anniel747 +4
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    It's a useful circuit that I used a lot in the 70s and 80s. I was wondering why I use it  a lot less now - and the answer is that I am much more likely to feed signals straight into a fast ADC in a micro and do the rectification in maths.

    I first saw this circuit in the National Semiconductors Linear Applications book (1972). This was where I learned about Op Amps in my (distant) youth. It's a great collection of Op Amp circuits.

    Just for fun try scoping the output of A1 and high frequencies and with a low amplitude signal - you might not be so happy with the 741 !

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett
    michaelkellett said:
    National Semiconductors Linear Applications book (1972)

    https://archive.org/details/bitsavers_nationaldaLinearApplicationsHandbook_19605588/page/n97/mode/2up?view=theater

    page 98

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to michaelkellett
    michaelkellett said:
    National Semiconductors Linear Applications book (1972)

    https://archive.org/details/bitsavers_nationaldaLinearApplicationsHandbook_19605588/page/n97/mode/2up?view=theater

    page 98

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    (I burned half the weekend reading that book)