Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum Current question
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 1039 subscribers
  • Views 1984 views
  • Users 0 members are here
Related

Current question

salesm21
salesm21 over 8 years ago

Attatched I have a photo of a small circuit I set up (I know its simple but I am just starting out) and realized something weird. When I put my test leads over my resistor I got very low resistance on my resistor which I thought would take the majority of the drop since the led offers little resistance. Also odd was when I turned my MM onto amps the DC power supplies current reading went up. Why is that? image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago +3
    You've got a 3.2V voltage source (your PSU) driving a resistor and LED in series. The LED behaves like a diode with quite a high forward voltage drop. I found a nice cheap blue LED a bit like yours on…
  • jw0752
    jw0752 over 8 years ago +3
    Hi Mitchell, If you turned your meter to current measurement with the leads hooked across the resistor you would have put a short across the resistor effectively taking it out of the circuit. Since the…
  • salesm21
    salesm21 over 8 years ago in reply to jw0752 +1
    John, So as I understand it, if the meter wants to know current it creates a path of little resistance so that all the current is read through the meter. However how does this work in a parallel circuit…
Parents
  • jw0752
    jw0752 over 8 years ago

    Hi Mitchell,

    If you turned your meter to current measurement with the leads hooked across the resistor you would have put a short across the resistor effectively taking it out of the circuit. Since the circuit would have less resistance the current would go up. The resistor is important in LED circuits as it acts like a limit so that the current of the LED can't go higher than the LED can tolerate.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • salesm21
    salesm21 over 8 years ago in reply to jw0752

    John,

    So as I understand it, if the meter wants to know current it creates a path of little resistance so that all the current is read through the meter. However how does this work in a parallel circuit? If my branch all of the sudden has 0 resistance all my current will drop across that branch and ill have none across the other branches. How do you effectively measure that?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to salesm21

    When using the Ammeter properly it is always necessary to break the circuit and put the ammeter in series with the rest of the circuit. You are correct the Ammeter has a very low precision resistor across its leads and the meter reads the voltage drop across this resistor and displays the output as Amps or milliamps.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 8 years ago in reply to salesm21

    When using the Ammeter properly it is always necessary to break the circuit and put the ammeter in series with the rest of the circuit. You are correct the Ammeter has a very low precision resistor across its leads and the meter reads the voltage drop across this resistor and displays the output as Amps or milliamps.

     

    John