Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Documents Audio Op Amps
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: randogless
  • Date Created: 14 Nov 2018 4:50 PM Date Created
  • Last Updated Last Updated: 2 Jan 2024 5:46 PM
  • Views 13688 views
  • Likes 20 likes
  • Comments 88 comments
Related
Recommended

Audio Op Amps

Op Amps Profile 3

Audio Amplifiers amplify input audio signals to voltage and power levels required by the speaker element of an audio system. In the 1960s, audio amplifiers were made of vacuum tubes and transformers, which were replaced with solid state devices like BJTs, FETs, and MOSFETs in the 1970s. Today's audio amplifiers use highly efficient ICs capable of producing high fidelity sound in small and lightweight packages. In this learning module, we cover the essentials of audio amplifier ICs, with a focus on the most popular Class-D amplifiers, their characteristics, output filter design, and applications.
Related Components | Test Your Knowledge

2. Objectives


Upon completion of this learning module, you will be able to:

  • Understand the basic concepts, architecture, and characteristics of audio amplifiers
  • Explain the different classes of audio amplifiers
  • Discuss the output filter design for Class-D audio amplifiers
  • Describe Class-D audio amplifier applications

3. Review

Back to Top

An audio amplifier is a type of operational amplifier that has a number of stages to deliver enough power for an output device such as a loudspeaker. Audio amplifiers are also known as power amplifiers, which amplify both voltages and current. To review the operation, connection, configurations, and characteristics of op-amps, please visit the two previous learning modules in this series: Low Power Op-Amps and Specialty Op-amps for High Voltage and Precision Applications.

4. Characteristics

Back to Top

The following are essential characteristics of an audio amplifier:

  • Power ratings
  • Efficiency
  • Noise
  • Total Harmonic Distortion (THD)
  • Bandwidth

5. Classes

Back to Top

Amplifiers are classified in two groups:

  • Group 1: The first group is based on the proportion of each input cycle during which an amplifier passes current (conduction angle). The group consists of Classes A, B, AB, and C.
  • Group 2: The second group consists of switching amplifiers based on digital circuits and pulse width modulation (PWM). This group consists of Classes D, F, G, I, S, and T.

In this section, let us discuss the most common classes of audio amplifiers in more detail.

- 5.1 Class-A Amplifier

Diagram 1
Figure 1: Example of a Class-A Amplifier

Class-A amplifiers consist of a single transistor that is connected in a common emitter configuration. It is more linear compared to other classes and produces a less distorted output. The major disadvantage of Class-A amplifiers is the low efficiency, which is typically less than 35%. Even if there were no bias signal, all output devices would conduct over the complete cycle. It results in significant amounts of power loss, heat dissipation, and a decrease in efficiency.

- 5.2 Class-B Amplifier

Diagram 2
Figure 2a: Example of a Class-B Amplifier
Diagram 3
Figure 2b: Output Waveform  and Crossover Distortion

The Class-B amplifier uses NPN and PNP transistors as shown in Figure 2A. Each transistor is active in only one-half cycle, with a 180° conduction angle of the input signal. Since it dissipates less power, efficiency is improved, typically to 78.5%. Class-B amplifiers reduce the heating problem associated with Class-A. In addition, Class-B amplifiers have a higher gain than Class-A amplifiers. The transistors conduct only when the input signal is higher than the base-emitter voltage. Therefore, no power is consumed at zero input. The disadvantage of a Class-B amplifier is the crossover distortion as it uses complementary transistors for each half of the waveform (Figure 2B).

- 5.3 Class-AB Amplifier

Diagram 3
Figure 3: Example of a Class-AB Amplifier

The Class-AB amplifier combines the advantages of both Class-A and Class-B configurations. The biasing is achieved by the forward voltage drop of the two compensating diodes, as shown in Figure 3. Both transistors slightly conduct without any input signal and eliminate any crossover distortion present in Class-B amplifiers. For low power outputs, this design operates as a Class-A amplifier, and for larger current outputs, it changes to a Class-B amplifier. Its efficiency is less than 78.5%.

- 5.4 Class-D Amplifier

Diagram 4
Figure 4: Class-D amplifier block diagram

The Class-D amplifier is a switching amplifier or a pulse width modulation (PWM) amplifier. Figure 4 shows a basic Class-D amplifier block diagram. The comparator modulates the audio signal with the sawtooth waveform generated by the wave generator circuit. The comparator output is the modulated digital form of the analog input audio signal. This digital signal is fed to the switching stage to amplify the signal further to drive speakers. A low pass filter reshapes this signal back to its analog shape.

Class-D amplifiers feature low noise, low distortion, wide bandwidth, and high-power output. The Class-D amplifier minimizes power consumption and thermal dissipation. Its efficiency is greater than 90%.

6. Class-D Modulation

Back to Top

In a Class-D amplifier, the input audio signal is converted into a PWM signal using modulation. A PWM signal is constructed by comparing the audio input signal to a triangular reference signal. This reference signal has a higher fundamental frequency (or carrier frequency) than the audio signal. The PWM is classified as AD modulation and BD modulation.

- 6.1 AD Modulation

In this technique, the carrier signals are in opposite phases as shown in Figure 5. There is no common-mode signal, since both outputs switch simultaneously in the opposite directions. Common-mode DC voltage is generated due to the average value of the PWM switching. This DC voltage appears on both sides of the load. Hence, there is no power dissipation across the load.

Diagram 5a
Diagram 5b
Figure 5: AD modulation in BTL Class-D Amplifier

The amplifier switches at the PWM frequency with a 50% duty cycle across the load, which causes significant current flow and power dissipation into the load. So, an LC filter is necessary to decrease the current and to provide better efficiency.

To further improve the efficiency of Class-D amplifiers, TI developed a proprietary modulation scheme, implemented in the high-power TPA3221 Class-D amplifier called High-Efficiency AD modulation (HEAD). To learn more, please visit the Related Components page of this learning module. HEAD modulation differentiates itself with benefits such as reduced idle power losses, improved EMI performance, and less pop noise. These benefits make HEAD useful in wireless speaker applications.

- 6.2 BD Modulation

In this technique, the carrier signals are in the same phase as shown in Figure 6. This modulation has common-mode content in its output.

Diagram 6a
Diagram 6b
Figure 6: BD Modulation in BTL Class-D Amplifier

The BD modulation switching technique modulates the duty cycle of the difference of the output signals such that its average signal corresponds to the input analog signal.

- 6.3 Hybrid Modulation

Hybrid Modulation is designed for minimized power loss without compromising the THD+N performance, and is optimized for battery-powered applications. With Hybrid modulation, TAS5825M detects the input signal level and adjusts the PWM duty cycle dynamically based on PVDD. Compared with traditional PWM modulation, hybrid modulation dynamically maintains differential switching with several common duty options. Hybrid modulation achieves ultra-low idle current and maintains the same audio performance level as BD Modulation. The benefits of Hybrid PWM modulation include:

  • Higher efficiency for longer battery lifetime
  • Good THD+N performance
  • Ultra-low idle power dissipation and idle noise

7. Class-D Configurations

Back to Top

Class-D audio amplifiers often support multiple output configurations in a single device, which provides added flexibility for the end application. In this section, let us discuss three common configurations of Class-D amplifiers.

- 7.1 Bridged-Tied Load (BTL)

Diagram 7
Figure 7: Stereo (Two-Channel) BTL Class-D Amplifier

In the BTL configuration, one amplifier drives one side of the load and gives an inverted signal to the other amplifier, which drives the other side of the load.  It results in twice the voltage swing across the load and quadruples the power (P = V 2 / R). The voltage across the load must be measured differentially because the load is not ground-referenced.

- 7.2 Parallel Bridge-Tied Load (PBTL)

A Parallel Bridged-Tied Load (PBTL) is an output configuration that takes a stereo BTL amplifier and connects the outputs in parallel for a mono channel. In this configuration, the output voltage is the same, but the output current is doubled because each output shares the load current. The PBTL often allows lower-impedance loads to be driven with higher output power when compared to a BTL of the same supply voltage.

Diagram 8a
Diagram 8b
Figure 8: PBTL Class-D Amplifier, Output Configurations

- 7.3 Single-Ended (SE)

In a single-ended (SE) configuration, only half of the signal swing is available because only one output is used to drive the load. However, this configuration can allow for four channels with a single stereo BTL amplifier as shown in Figure 8. Some amplifiers also allow a combination of one BTL and two SE channels for support of 2.1 audio systems with a single device.

Figure 9
Figure 9: Four Single-Ended Outputs

The PWM modulation introduces a DC voltage equal to half of the supply voltage at the output of the LC filter. The speaker is referenced to ground. A DC blocking capacitor is required to avoid the DC voltage across the speaker.

8. Protection

Back to Top

Excess voltage, current, temperature, and other factors like electromagnetic interference beyond the specification/rating of the amplifier device can damage it and impact performance. This is one of the reasons why Class-D audio amplifiers are integrated with system protection; these features help to create reliable audio designs. In this section, let us discuss some of the integrated protection features.

Overcurrent Protection:

Class-D amplifiers feature overcurrent protection. When the output current exceeds the threshold limit, the amplifier is shut down, and sends a signal to the host processor. In addition, some amplifiers offer cycle-by-cycle current (CBC)  limit, which instead of shutting down will adjust the output cycle by cycle, so if it is just a temporary peak, the amplifier will keep playing instead of shutting down. More information on this feature can be found here: Overload and Short Circuit Current Protection.

Over-Temperature Protection:

Each Class-D amplifier has temperature limitations specified by the manufacturer. Exceeding those limits results in overheating of the device. When the temperature of the amplifier exceeds a specified level, the amplifier shuts down to prevent overheating. Some amplifiers have more sophisticated thermal protection; they send a warning to the host before shutdown so they can reduce the gain or prevent the thermal shutdown. For example, the TAS5825M supports thermal foldback, which actually has 4 levels of warnings at different temperatures to give several chances at adjusting the output to prevent thermal shutdown.

Amplitude Modulated (AM) Interference Avoidance:

Certain switching frequencies introduce AM interference and harmonics affecting the performance of the amplifier. This AM avoidance feature allows the designer to program the switching frequency of the amplifier to avoid the interference.

Voltage Protection:

Irregular power line conditions such as over voltage, under voltage, voltage fluctuations, overload, and short circuits can damage silicon devices. Protection against these faults is built into Class-D amplifiers.

Automatic Gain Limiter (AGL):

Because of input signal variations, the output of the amplifier may cross the supply rails,  resulting in clipping of the output which would affect the audio integrity. Class-D amplifiers feature an automatic gain limiter to linearly vary the gain and compress the signal amplitude when the output exceeds a specified threshold voltage.

DC Offset Protection:

Short circuits or the presence of rail voltage directly in the amplifier output may cause damage to the speaker. The DC offset protection circuit continuously receives PWM input signals from the outputs and inspects for any large DC voltage difference which is being reflected on the speaker load. If so, the circuit triggers a channel shutdown signal when the DC offset reaches a preset level.

Excursion Control:

An excursion is a distance that the speaker diaphragm moves in and out from its resting position which is controlled to avoid damage to the speaker. Amplifiers control the excursion via current and voltage sense feedback circuits.

Coil Temperature:

When a speaker plays audio, an amplifier generates heat due to power dissipation. The speaker coil can heat up beyond the specification and get damaged. Amplifiers can be shut down by monitoring the temperature also via current and voltage sense feedback.

9. Output Filters

Back to Top

- 9.1 Type-1 Filter

Figure 10
Figure 10 - Type-1 Filter for AD Modulation

The Type-1 filter is a differential filter which is used for AD modulation (Figure 10). AD modulation has no common-mode content on its outputs, and thus only the differential mode is needed for analysis.

- 9.2 Type-2 Filter

Diagram 11
Figure 11: Type-2 Filter for AD or BD Modulation

The Type-2 filter is a common-mode filter designed for BD or AD modulation amplifiers (Figure 11). Type-2 filters are common mode and can easily convert into their equivalent single-ended form.

- 9.3 Hybrid Filters

Diagram 12
Figure 12: Hybrid Filter for AD Modulation

For some applications, it is beneficial to use a hybrid filter as shown in Figure 12. It combines Type-1 and Type-2 filters for an AD modulation amplifier.

- 9.4 Inductorless Filters

An inductor-less solution, using ferrite bead filters, can be implemented to reduce board space and system cost. For example, the TAS5805MEVM has an inductor-less solution implemented on one amplifier and normal inductors on the other. See the Related Components page of this learning module.

10. Applications

Back to Top

In this section, we feature two Class-D amplifier applications to illustrate examples of the use of audio op-amps in real applications.

- 10.1 Type-1 Filter

Figure 13
Figure 13 - 2.0 (Stereo BTL) System Application Schematic

The TAS5825M is a high-performance, stereo closed loop Class-D with an integrated audio processor with up to 192-kHz architecture. In this 2.0 system (Figure 13), the amplifier provides two channels via the digital input signal. These two channels are amplified and then sent to two separate speakers. In some cases, the amplified signal is further separated based upon frequency by a passive crossover network after the L-C filter.  The two channels are called a stereo pair, with one channel containing the audio for the left channel and the other channel comprising the audio for the right channel.

- 10.2 Differential AD-Mode PBTL System

Figure 14
Figure 14 - Typical Differential AD-Mode PBTL Application

The TPA3220 is a pad-down Class-D amplifier that enables efficient operation at full-power, idle, and standby. The device features closed-loop feedback with a bandwidth up to 100 kHz, which provides low distortion across the audio band and delivers excellent sound quality. The device operates with either AD or low idle-current HEAD modulation. The TPA3220 also achieves higher than 90% efficiency, low idle power (< 0.25W), and ultra-low standby power (< 0.1 W). It is made possible through the use of 70-mΩ MOSFETs, an optimized gate drive scheme, and low-power operating modes.

*Trademark. Texas Instruments is a trademark of Texas Instruments Inc. Other logos, product and/or company names may be trademarks of their respective owners.

Shop our wide range of audio operational amplifiers, including low power, ultra-low noise, low THD+N, and small package op amps, as well as associated development boards.

Shop Now


Test Your Knowledge

Back to Top
Op Amps III
Op Amps III Complete our Essentials Op Amps III: Audio Op Amps course, rate the document, take the quiz...

Are you ready to demonstrate your Audio Op-Amps knowledge?  Then take a quick 15-question, multiple-choice quiz to see how much you've learned from this module.

To earn the Op Amps III: Audio Op-Amps Badge, read through the module, attain 100% in the quiz at the bottom, and leave us some feedback in the comments section.

Essentials logo

  • bluetooth
  • bd modulation
  • audio
  • audio amplifier
  • vacuum tubes
  • power amplifier
  • op_amps
  • wi-fi
  • operational amplifier
  • btl
  • class-d amplifier
  • automotive
  • fault protection
  • trans-conductance
  • trans-impedance
  • head modulation
  • filter
  • ad modulation
  • ti
  • speaker
  • op amps
  • ess_module
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Robert Peter Oakes +6
    for the record (sic): I would love to have a tube amplifier. For the sound, for the looks, for the engineering.
  • DAB
    DAB over 7 years ago +5
    Going through the post took me back many decades. I have not done much with audio since Tech School and I was pleased to see the new improvements to the basic amplifier. Back in my day, the best audio…
  • phoenixcomm
    phoenixcomm over 7 years ago +5
    It was a fun module but to me most of it like uncharted land, as I don't play around with semiconductor amps much, Grew up with tubes and you need tubes for that warmth, the richness, and the harmonics…
Parents
  • jc2048
    jc2048 over 7 years ago

    "It is highly linear..."

    Is that necessarily true for a class A amplifier? Here I've slapped together the example circuit in a simulator

     

    image

     

    with 40mV pk/pk going in, we see about 4V pk/pk coming out

     

    image

     

    we can see immediately that the transfer response wasn't very linear - if it were the positive peak would match the negative after going through the coupling capacitor and driving the 10k load

    to see better I got the simulator to produce a Fourier transform of the output waveform

     

    image

     

    here, in addition to a dc offset, you can see that the 2nd harmonic is only about 25dB down from the fundamental and that there's a bit of 3rd harmonic distortion too: that's probably 6% THD all told.

     

    The linearity does get much better as the input signal gets smaller. That's because as we work on smaller and smaller proportions of the transfer curve it gets to approximate a straight line more and more closely, but it's never actually linear.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 7 years ago

    "It is highly linear..."

    Is that necessarily true for a class A amplifier? Here I've slapped together the example circuit in a simulator

     

    image

     

    with 40mV pk/pk going in, we see about 4V pk/pk coming out

     

    image

     

    we can see immediately that the transfer response wasn't very linear - if it were the positive peak would match the negative after going through the coupling capacitor and driving the 10k load

    to see better I got the simulator to produce a Fourier transform of the output waveform

     

    image

     

    here, in addition to a dc offset, you can see that the 2nd harmonic is only about 25dB down from the fundamental and that there's a bit of 3rd harmonic distortion too: that's probably 6% THD all told.

     

    The linearity does get much better as the input signal gets smaller. That's because as we work on smaller and smaller proportions of the transfer curve it gets to approximate a straight line more and more closely, but it's never actually linear.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 7 years ago in reply to jc2048

    Interesting - it is cool to add objective analysis to discussions that can't be resolved with subjective opinions.

    This analysis also hints at why negative feedback might be helpful in many amplifier designs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to jc2048

    look up Hiraga amp designs! the only space I felt I needed tubes was between the turntable and control amp.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to dougw

    This analysis also hints at why negative feedback might be helpful in many amplifier designs.

    Yes. Once transistors became reasonably priced, the standard way to make a audio power amplifier settled to being AB for the output stage preceded by a dc amplifier with lots of gain and NFB [negative feedback] wrapped around the whole thing.

     

    Although it's a bit of an over-simplification, in essence the audio designers learnt many of the techniques from the early op amp designers. (It's a bit odd, though, calling an audio power amplifier an "audio op amp", even though technically there's a lot in common - no manufacturer, not even the sponser, groups them like this in their product classification). It (NFB) enabled the designers to drive the THD figure down to levels that are silly in relation to what can actually be perceived when listening (that was because the figure always appears in specs and the marketplace drove the figure down because audiophiles thought that it was a useful measure of how good the amplifier was).

     

    But it's the feedback that leads to the good linearity, not the output configuration. Certainly, you could say class A was MORE linear than class B or AB, but I'd disagree with HIGHLY.

     

    Later on, the designers did some quite interesting things with the output stage. Both Technics and Morantz (and possibly others, I don't know the history all that well) came up with designs where there was a hybrid of a very accurate low-powered amplifier and a much cruder high-powered B stage, with the low-powered amp giving good performance through the cross-over area and correcting the high-powered one elsewhere. There were also designs with multiple rails, where the higher voltage rails would come into play with larger signals, to improve the efficiency. I imagine that the added complexity lead to complicated trade-offs, though.

     

    Edited: I think I'm wrong about it being Morantz as well.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to jc2048

    I remember all the hype around multi-rail amplifier architecture and how it handled high dynamic range music, but I don't think I ever saw a schematic of how it was done.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to dougw

    I've never been involved with audio design, so this is all incidental stuff I've picked up along the way and more recently from books as I've been learning about transistor design. I imagine MK would know a lot more because it sounds like he might have designed amplifiers at one time and, if so, he'd have naturally had an on-going interest in the way the circuit configurations gradually evolved. I've got a library book here by John Linsley Hood, who designed amplifiers here in Britain, which is very interesting but it doesn't go into multi-rail (it's got lots of valve (tube) designs, though, which is kind of fun and they're surprisingly easy to understand if you just imagine the active devices as being a weird sort of high-voltage depletion-mode MOSFET. It's not a totally accurate model - the valve is more complex in the transfer function - but it gets you a long way in roughly understanding the circuit functions. Just wish the simulators I've got had a few valve models).

     

    I suspect where I saw it (multi-rail) might have been one of Douglas Self's books (he's another designer who was well known over here from publishing in technical magazines). Both of them designed commercial audio gear, including amplifiers, so their books are very practical.

     

    One interesting curiosity from the Linsley Hood book is that it includes a circuit for an amplifier with a 10W class A output stage. He actually published it in a technical magazine - I would think it was early on, before they really refined the AB and cross-over distortion was still a major problem. He had an active pull-up for the output transistor that was driven by the signal inverted, so on paper, at a quick glance, it looks like a push-pull output, but the lower transistor really was continuously conducting - obviously, being a real amplifier it had plenty of gain ahead of the output stage and NFB around it to get reasonable performance figures. (Don't know how serious it was meant to be - perhaps he just did it because he could or maybe someone dared him to.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rusgray
    rusgray over 7 years ago in reply to jc2048

    jc2048  wrote:

     

    "It is highly linear..."

    Is that necessarily true for a class A amplifier? Here I've slapped together the example circuit in a simulator...with 40mV pk/pk going in, we see about 4V pk/pk coming out...we can see immediately that the transfer response wasn't very linear - if it were the positive peak would match the negative after going through the coupling capacitor and driving the 10k load

    The time-axis skew between the peaks of the input signal and the inverted peaks of the output signal is due to a phase shift, not amplifier non-linearity. All real amplifiers have some phase shift associated with them. The aspect of your presented data plot that shows non-linearity is the shape of the output waveform. Notice how the peaks are wider and the troughs are narrower with respect to the input waveform; that's non-linear distortion (likely caused by square-law amplification characteristics.)

     

    Here's a quick plot I made in NI's Multisim tool, using the same passive values you've chosen, but replacing the transistor model with a generic ideal NPN model having a current gain of 100:

    image

    As we can see from the plot, the idealized transistor placed in the selected topology creates a completely linear amplifier (as we expect.) The obvious conclusion is that your test circuit is showing the non-idealities of the particular transistor you're modeling, not the Class A topology generally.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to rusgray

    I thought that all transistors are in reality non-linear in what we call the linear range. Is it possible to create a linear class A with a transistor that’s for sale?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to rusgray

    Thanks for the response.

     

    Sorry, I wasn't very clear in what I wrote and I can see now how it could be misinterpreted. What I was trying to point to was that the amplitude of the positive peak didn't match the amplitude of the negative peak. If it was a perfect sinewave, then after the ac coupling it would centre around 0V. That it doesn't indicates that the shape of the sinewave is distorted and hence there must be some harmonic distortion present.

     

    From the plot you give, the same occurs with your 'idealized' transistor. I was never taught SPICE (it came along after my time at college), so I'm not familiar with such things as idealized models and what they might consist of. Try doing a Fourier analysis of the resulting waveform and see what harmonics are present. If there isn't some second harmonic distortion there, I would say that it isn't a very good model of a bipolar transistor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rusgray
    rusgray over 7 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    I thought that all transistors are in reality non-linear in what we call the linear range. Is it possible to create a linear class A with a transistor that’s for sale?

    It is my understanding that all transistors suffer from square-law distortion artifacts unless the region of operation is vanishingly small. Because of this, it is not possible to create a truly linear Class A design with a real transistor. It is possible to create extremely low-distortion amplifiers using discrete transistors in other topologies; the company I work for licenses an audio amplifier design with extremely low (-130 dB or lower) THD.

    • Cancel
    • Vote Up +3 Vote Down