Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Documents DC Power: DC-to-DC Converters
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 30 Mar 2021 5:13 PM Date Created
  • Last Updated Last Updated: 27 Feb 2022 11:16 PM
  • Views 10867 views
  • Likes 20 likes
  • Comments 40 comments
Related
Recommended

DC Power: DC-to-DC Converters

element14 Learning Center

 

image

DC Power I: DC-to-DC Converters

Sponsored byimage


1. Introduction | 2. Objectives | 3. Basic Concepts | 4. Analysis | Related Components | Tech Spotlight | Related Blog | Power Management | Giveaway | Test Your Knowledge image

 

1. Introduction

DC-to-DC converters yield precise, constant, and regulated power to various devices, circuits, and appliances. They offer different voltage and power levels to GPUs, CPUs, SoCs, and ASICs used in diverse applications, such as servers, datacom, storage, consumer, and telecom. These converters also find popular use in battery-operated electronic devices such as cellular phones and laptop computers. Based on a new Source-Down technology, a wide range of DC-to-DC converters and MOSFETs, including those with integrated power stages, multi-phase digital controllers, and integrated POL converters are available to achieve the best outcomes. This learning module will discuss some of these converters, the DC-to-DC converter's basic concepts, and use case applications.

2. Objectives

Upon completion of this module, you will be able to:

image Explain the basic concepts, topologies, and key characteristics of DC-DC converters

image Understand Source-Down technology and its benefits

image Discuss different power converter devices and use cases offered by Infineon

3. Basic Concepts
Back to Top

A DC-to-DC converter is a circuit in a power supply that converts a DC voltage level to another DC voltage level. They are classified into two types: linear and switched. Linear DC-DC circuits use linear regulators (LDOs), which function on the concept of a resistive voltage dip to generate and control a particular output voltage. Switched-mode converters are based on the idea of periodically storing the input energy either in an inductor, transformer, any magnetic field component, or in an electric field component like a capacitor, and then releasing it to the output at a different voltage. A closed feedback loop is used to maintain constant voltage output with varying input voltages and output loads. Switched-mode DC-DC is further classified into the categories of isolated and non-isolated converters. Figure 1 shows a simple DC-DC converter circuit with a linear regulator and a switched-mode regulator.

image
image

Figure 1: Linear Regulator and Switched-Mode (Buck) DC-DC Converter

DC-DC converters produce output either lower or higher than the input voltage, and are mainly categorized into three conversion topologies: Buck, Boost, and Buck-Boost.

- 3.1 Buck Converter Topology

image

Figure 2: Buck Converter circuit

A buck converter generates a lower output voltage than the input voltage, and is termed a "step-down" converter. This DC-DC conversion is non-isolating, meaning that there is a common ground between input and output. Figure 2 shows a simple circuit of a buck DC-DC converter. When switch S is on, energy is stored in inductor L as the current flows to the load, and capacitor C is charged. When S is off, the inductor releases the stored energy. The current flows into the load and circulates via diode D, and Capacitor C provides energy to the load. High-frequency switching produces an output proportional to the duty cycle. The switch and the diode shown in the figure are FETs, used as synchronous rectifiers to reduce losses and improve efficiency.

- 3.2 Boost Converter Topology

image

Figure 3: Boost Converter Circuit

Boost converter topology produces a higher voltage than the input voltage, and is also called a step-up converter. Figure 3 shows an elemental boost DC-DC converter circuit. With switch S turned on, the current flows through the inductor L, returning to input via switch S. The inductor stores the energy during this period. With transistor S off, the inductor functions akin to a voltage source in series with the input voltage. The inductor's stored energy is circulated via diode D to load, and this charges capacitor C to a higher level than the input voltage. The on-time of switch S defines the output voltage.

- 3.3 Buck-Boost Converter Topology

image

Figure 4: Buck-Boost Converter

A Buck-Boost converter is a combination of buck and boost circuits, as shown in figure 4. In this topology, the converter output voltage can be higher or lower than the input voltage. S2, L, and D2 make the boost converter work when switch S1 is on. Switch S1, L, and D1 make the buck circuit and work when S2 is off.

- 3.4 Key Parameters and Selection Criteria

A DC-DC converter must operate within the required DC parameters, such as the specified input voltage range, the output voltage range, and the maximum current of output needed for a particular application. The other performance parameters that must be considered are efficiency, output ripples, load regulation, transient response, temperature rating, size, and weight. The switching frequency is another critical parameter that affects efficiency and noise. Higher switching frequency allows smaller external components and lower peak currents and I2R losses, but it also increases core losses, gate-charge currents, and switching losses.

To select the DC-DC converter's peripheral components, we should check the datasheet to ensure each component's suitability for the application. The inductor is determined based on inductance value, DC resistance (DCR), the peak current requirement, and the desired switching frequency. The input capacitor minimizes both peak current extracted from the input supply, and the radiated noise to all other system elements. Ensure that the capacitor has a ripple-current rating proximate to the chosen switching frequency.

- 3.5 Range of DC-DC Converters and MOSFETS

OptiMOSTm Power MOSFET Source-Down

The OptiMOSTm Power MOSFET Source-Down introduced by Infineon comes in an enhanced PQFN package, and is available in Source-Down Center-Gate (optimized for paralleling) and Source-Down versions. The new Source-Down technology has the silicon inverted within the component and offers better thermal performance and lower RDS(on) performance compared to alternative solutions. IQE006NE2LM5, IQE006NE2LM5CG, IQE013N04LM6CG, and IQE013N04LM6 are a few examples from Infineon's OptiMOSTm Source-Down portfolio. All of these are low-voltage power MOSFETs included in the PQFN 3.3x3.3 Source-Down package. They are commonly used in drives, telecom, SMPSs, and servers.

Power Management ICs (PMICs)

Infineon's power management ICs comprise tightly integrated OPTIREGTm and PMBus power management ICs. They monitor, sequence, and execute functional safety support, simplifying design and preserving board space. PMICs are scalable, efficient solutions for multiple applications in the industrial and automotive fields.

image OPTIREGTm PMICs offer integrated, multi-rail power supply solutions for demanding automotive environments. They contribute productive, efficient voltage regulation, including pre-and post-regulator architectures with DC-DC, linear, and tracking regulators. Supervisory features allow automotive ECU design for safety-relevant applications.

image The PMBus PMIC comes with standard PMBus commands, which offer an easy-to-use interface for status and telemetry. It can configure output voltages in 5 mV steps, and a five output Point of Load (POL) digital voltage regulator for FPGAs, ASICs, and other multi-rail power systems. Additional applications comprise CPU multi-rail systems, embedded computing systems, storage systems, and communication.

Switching Regulators

Infineon's Switching Regulators include switching regulators for industrial applications and OPTIREGTm Switchers for automotive applications. OPTIREGTm Switchers endure harsh automotive environments and provide a dedicated feature set to design effective automotive ECUs. The integrated power stages, soft-start feature, and integrated compensation network reduce the needed amount of external components, system costs, and board space. They offer low current consumption in PFM mode at light loads, to optimize efficiency. The switchers detect under-voltage and overvoltage conditions of the output voltage and indicate the same with the reset output signal. The integrated thermal shutdown feature secures the device from overheating.

Industrial Switching regulators span a broad range of industrial, communication, consumer, and multi-market applications. High-efficiency switching DC-DC converters reduce energy consumption, lengthen battery-powered systems' operational life, and minimize system operating costs.

Integrated POL (Point-of-Load) Voltage Regulators

The Integrated POL Voltage Regulators portfolio from Infineon includes Integrated POL Analog Voltage Regulators and Integrated POL Digital Interfaces. The POL converters consolidate a PWM controller, driver, and MOSFETs into a compact, easily usable PQFN package. The patented PWM modulation scheme permits more than 1 MHz switching frequencies to deliver ultra-compact layouts and the smallest bill-of-materials within -40° to 125°C operating temperatures. They feature essential protection functions like pre-bias startup, internal soft-start, hiccup overcurrent protection, and thermal shutdown to provide the needed system-level security during fault conditions.

The digital interface IPOL devices are unified, and the capable DC regulator provides I2C/PMBus, Parallel VID, and Intel SVID.

4. Analysis
Back to Top

DC-DC converters are a crucial component of almost all electronic circuits where different voltages are needed to power diverse circuit components. We will analyze the new Source-Down package innovation and use-case applications using Infineon DC-DC converters and power MOSFETs.

- 4.1 Source-Down Technology

In the Source-Down package, the silicon die is placed inverted inside the MOSFET package. The source potential is attached to the lead frame instead of the drain potential. The silicon gate and source connection of the silicon die are directly connected onto the lead frame, as shown in Figure 5 (on the right). A large copper clip connects the drain from the top. The drain, source, and gate connections remain in the same location as standard PQFN 3.3x3.3 devices, making a drop-in replacement extremely easy.

image
image

Figure 5: Internal construction of a PQFN 3.3x3.3 mm Drain-Down power MOSFET (left) and Source-Down power MOSFET (right)

- 4.2 Source-Down Benefits

The new Source-Down footprints come with several benefits: improved RDS(on), optimized thermal management capabilities, and parallel operation, as described in the following content.

RDS(on): Inverting the die eliminates a few construction limitations. The Source-Down approach relaxes some constraints and enables larger dies, and reduces RDS(on) by 30% compared to a standard MOSFET. Lower RDS(on) is directly linked to the reduction of I2R losses in the application, and leads to greater power densities. It is now possible to replace a Super SO8 (30mm2 PCB area) with a Source Down in PQFN 3.3 x 3.3 (10 mm2), resulting in improved performance.

Thermal Management Optimization: The Source-Down package optimizes parallel operation and thermal management. In applications where the drain is connected to the switched node, like in a buck converter or synchronous rectifiers on the SMPS's secondary side, it is inadvisable to connect the drain pad to a large copper area heatsink. In this case, the sole technique to eliminate losses is via a source copper clip and then to the ground plane, as shown in Figure 6. With Source-Down, the thermal management in ground-referenced set-ups is much easier. The source can be connected to all ground planes using thermal vias, resulting in an improved heat transfer to the ambient.

image
image

Figure 6: Thermal management with "Drain Down" (left) and "Source Down" (right)

Paralleling Made Easy: Higher current capability can be achieved by paralleling devices. With Drain-Down, the distance from drain to source is inadequate to route the gate signal under the device; another PCB layer must connect the gates, as shown in Figure 7. The Center-Gate variant, with its 0.75mm creepage distance (drain to source), offers the possibility to route the gate signal of paralleled devices sans another layer.

image
image

Figure 7: Paralleling with "Drain Down" (left) and "Source Down" (right).

Applications Benefits of the Source-Down package: The low RDS(on) of the Source-Down benefits applications like e-fuses or ORings. Even with a high current of 30A, the Source-Down remains cool at 40.2°C, which results in better reliability and fewer parts in parallel.

Source-Down enhances synchronous rectifier design on an SMPS's secondary side. The switches are generally ground-referenced, as shown in Figure 8.

image
image

Figure 8: Multiple ground-referenced MOSFET

Source-Down optimizes thermal management in buck converters and other half-bridge configurations. Figure 9 illustrates a Drain-Down being used as the high-side and a Source-Down as the low-side switch. Both devices are now linked to big copper areas. The switch node may disconnect from the large copper area, avoiding possible EMI issues.

image
image

Figure 9: Buck converter with a Drain Down/Source Down combination

- 4.3 Applications

The following are a few application examples using these low-voltage power MOSFETs and DC-DC converters.

Powered Tools with OptiMOSTm Source-Down 40 V (IQE013N04LM6): Infineon's IQE013N04LM6 1.35 mΩ, 40 V MOSFET in a 3.3x3.3 PQFN Source-Down package (also available in a Center-Gate version) defies the status quo in form factor and power density in end applications. In power tools, it minimizes the PCB's internal space, enabling an ergonomic tool design. Since the design goal is to achieve the smallest possible form factor of the motor drive circuit, a MOSFET case temperature of ~100°C is permissible under full load. This new IQE013N04LM6 achieves high performance at 400 W of maximum power with an optimized form factor, while meeting the design requirements. Figure 10 shows a block diagram of a battery-powered motor using OptiMOSTm Source-Down low-voltage power MOSFETs.

image

Figure 10: Battery Powered Motor Control

Computing and Data Storage with OptiMOSTm IPOL Buck Regulators: Energy efficiency and costs are a major concern when it comes to computers and data storage. The total system comprises numerous chipsets, such as GPUs, storage controller ICs, CPUs, and memory. All of these can be powered with the OptiMOSTm IPOL Buck regulator. This application illustrates the use of OptiMOSTm IPOL Buck regulators, such as the IR3889 series, operated with a single supply. It utilizes a fast Constant On-Time (COT) control scheme to achieve an accelerated control response. It has programmable switching frequency, selectable current limits, selectable soft-start times, Forced Continuous Conduction Mode (FCCM), and Diode Emulation Mode (DEM) operation. Figure 11 shows a system block diagram of a computing and data storage system with this converter IC's application circuit.

image
image

Figure 11: Computing and Data Storage Block Diagram with IR3889 Application Circuit

Glossary

image Output Ripple: small variations in output voltage. Many circuits are extremely sensitive to any noise on their input supply, so a small amount of ripple in the output voltage is to be expected.

image Current Output: the maximum current a voltage regulator can offer. It depends on the internal power transistor's current-carrying capability.

image Noise: random fluctuations in the output voltage generated by components like transistors and resistors.

image Load Regulation: the regulator's ability to maintain output voltage steadily during load current fluctuation.

image Load Transient: the response of the output voltage to an unexpected step-change in load current.

image Line Transient: the response of the output voltage to unforeseen step-changes in the input voltage.

image Line Regulation: measures variation in the regulator's output voltage due to input variations.

image Efficiency: a measure of wasted power by the regulator. A linear regulator has lower efficiency, as it wastes a lot more power compared to a switching regulator.

image RDS(on): the resistance between the Drain and Source of a MOSFET in ON condition.

image PQFN: Power Quad Flat No-Lead.

image MOSFET: Metal-Oxide Semiconductor Field-Effect Transistor.

image PFM: Pulse Frequency Modulation.

image PWM Pulse Width Modulation.

 

*Trademark. Infineon is a trademark of Infineon Inc. Other logos, product and/or company names may be trademarks of their respective owners.

image

Related ComponentsBack to Top

This supplementary section discusses the types of related components used for prototyping or product development using DC-to-DC converters.

OptiMOSTm Source-Down MOSFETS

 

image

IQE006NE2LM5 OptiMOSTm 25V low-voltage power MOSFET in PQFN 3.3x3.3 Source-Down package

Buy Now

The innovative Source-Down OptiMOSTm low-voltage power MOSFET 25V (IQE006NE2LM5) comes in a PQFN3.3x3.3 package size, making it easy to use in the same PCB routing as the Drain-Down solution. In the same package outline of 3.3x3.3mm, the new Source-Down shows an industry benchmark RDS(on) of 30 percent lower than standard PQFN 3.3x3.3 packages. In addition, Source-Down shows a significant shrinkage in form factor. The same performance as a 5x6mm SuperSO8 is now achievable in a PQFN3.3x3.3, utilizing the PCB real estate more efficiently. Source-Down also offers improved power losses, resulting in superior thermal management. Overall, the new and innovative Source-Down technology enables higher system efficiency and power density in the end application.

image  Transistor Polarity: N Channel

image  Drain Source Voltage Vds: 25V

image  Continuous Drain Current Id: 298A

image  On Resistance Rds(on): 500 µohm

image  Transistor Case Style: TSON

image  Transistor Mounting: Surface Mount

image  Rds(on) Test Voltage Vgs: 10V

image  Threshold Voltage Vgs: 1.6V

image  Power Dissipation Pd: 89W

image  No. of Pins: 8

image  Operating Temperature Max: 150°C

image  Product Range: OptiMOS 5 Series

image MSL:  MSL 1 - Unlimited

 

image

IQE006NE2LM5CG OptiMOSTm low-voltage power MOSFET 25V in PQFN 3.3x3.3 Source-Down Center-Gate package

Buy Now

With Infineon's innovative Source-Down technology, the OptiMOSTm low-voltage power MOSFET (IQE006NE2LM5CG) is available as a Center-Gate footprint version. Placing the gate in the middle of the footprint leads to an optimized source connection. The Center-Gate footprint offers the advantage of optimized and easy parallelization of MOSFETs, as the Center Gate comes with a larger drain to source creepage distance. With this it is possible to connect the gates of multiple devices on a single PCB layer, improving current capability, resulting in higher output levels. In addition, the Source-Down Center-Gate footprint offers high system efficiency and high power density.

image Transistor Polarity: N Channel

image  Drain Source Voltage Vds: 25V

image  Continuous Drain Current Id: 298A

image  On Resistance Rds(on): 500 µohm

image  Transistor Case Style: TSON

image  Transistor Mounting: Surface Mount

image  Rds(on) Test Voltage Vgs: 10V

image  Threshold Voltage Vgs: 1.6V

image  Power Dissipation Pd: 89W

image  No. of Pins: 9

image  Operating Temperature Max: 150°C

image  Product Range: OptiMOSTm 5 Series

 

image

IQE013N04LM6CG OptiMOSTm low-voltage power MOSFET 40V in PQFN 3.3x3.3 Source-Down center-gate package

Buy Now

The IQE013N04LM6CG extends the innovative Source-Down family with the 1.35mOhm, OptiMOSTm power MOSFET 40V in a 3.3x3.3 PQFN Source-Down Center-Gate package. This best-in-class power MOSFET challenges the status quo in power density and form factor in the end application. It features major reduction in RDS(on) of up to 25 percent and superior thermal performance in RthJC.

One target in power tool design is to minimize the internal restrictions of PCB area requirements, enabling an ergonomic design and optimizing the end user experience. Moving the inverter from the handle into the head simultaneously minimizes the volume of the power tool motor housing while keeping the torque of the tool at a reasonably high level for quick and easy action.

image  Transistor Polarity: N Channel

image  Drain Source Voltage Vds: 40V

image Continuous Drain Current Id: 205A

image On Resistance Rds(on): 1.1 mohm

image Transistor Case Style: TSON

image Transistor Mounting: Surface Mount

image Rds(on) Test Voltage Vgs: 10V

image Threshold Voltage Vgs: 1.6V

image Power Dissipation Pd: 107W

image No. of Pins: 9

image Operating Temperature Max: 175°C

image Product Range: OptiMOS Series

image MSL:  MSL 1 - Unlimited

 

image

IQE013N04LM6 OptiMOSTm low-voltage power MOSFET 40V in PQFN 3.3x3.3 Source-Down package 

Buy Now

Infineon has extended its innovative Source-Down family with the IQE013N04LM6 1.35mOhm, 40V in a 3.3x3.3 PQFN package. This power MOSFET optimizes the end user experience by challenging the status quo in power density and form factor. It features major reduction in RDS(on) of up to 25 percent and superior thermal performance in RthJC.

One target in power tool design is to minimize the internal restrictions of PCB area requirements, enabling a more ergonomic design. Moving the inverter from the handle into the head minimizes the volume of the power tool motor housing while simultaneously keeping the torque of the tool at a reasonably high level for quick and easy action.

image Transistor Polarity: N Channel

image Drain Source Voltage Vds: 40V

image Continuous Drain Current Id: 205A

image On Resistance Rds(on): 1.1mohm

image Transistor Case Style: TSON

image Transistor Mounting: Surface Mount

image Rds(on) Test Voltage Vgs: 10V

image  Threshold Voltage Vgs: 1.6V

image  Power Dissipation Pd: 107W

image No. of Pins: 8

image Operating Temperature Max: 175°C

image Product Range: OptiMOS Series

image MSL:  MSL 1 - Unlimited

Giveaway: Register here to win Infineon’s SHIELDBTS70041EPZTOBO1 PROFETTm+2 12V Grade0 evaluation board which is high-temperature resistant up to 175°C and comes with one high-side switch of BTS7004-1EPZ

For more information: about Infineon power management products, click here for more information.

Test Your KnowledgeBack to Top

image

Are you ready to demonstrate your knowledge of DC-to-DC Converters? Then take this 5-question pop quiz to see how much you've learned. To earn the DC Power I Badge, read through the learning module, attain 100% on the Quiz, leave us some feedback in the comments section, and give the learning module a star rating.

 

Attachments:
image DCPower1.pdf
  • infineon
  • power_management
  • essentials
  • source_technology
  • dc-to-dc_converter
  • ess_module
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 5 years ago +4
    Managed 100% on my first attempt - which is a first for me. The quiz was a little bit disappointing being only 6 questions. There is lots of stuff that could have been asked about. I liked the more general…
  • beacon_dave
    beacon_dave over 5 years ago +4
    Nice overview of DC-to-DC converters.
  • fmilburn
    fmilburn over 5 years ago +3
    Nicely written with an easy quiz
Parents
  • NigelB
    NigelB over 5 years ago

    An interesting article, and a relevant topic for my work, as I am often looking at designing power supplies, and efficiency is certainly critical. I have not looked at Infineon chipsets previously. I have downloaded it for further follow-up image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • NigelB
    NigelB over 5 years ago

    An interesting article, and a relevant topic for my work, as I am often looking at designing power supplies, and efficiency is certainly critical. I have not looked at Infineon chipsets previously. I have downloaded it for further follow-up image