Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Documents Static Control: Electrostatic Discharge and Prevention
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 5 Aug 2021 3:03 PM Date Created
  • Last Updated Last Updated: 27 Feb 2022 8:17 PM
  • Views 16003 views
  • Likes 20 likes
  • Comments 45 comments
Related
Recommended

Static Control: Electrostatic Discharge and Prevention

element14 Learning Center

 

image

Static Control I: Electrostatic Discharge and Prevention

Sponsored byDESCO INDUSTRIES INC.


1. Introduction | 2. Objectives | 3. Basic Concepts | 4. Analysis | 5. Glossary | Related Components | Test Your Knowledge image

 

1. Introduction

In a technologically integrated environment, static electricity can be damaging, expensive, and in some cases, lethal. Most people know static electricity as the minor shocks encountered in everyday life when touching metals like door knobs, after walking over lushly carpeted floors, or even when sliding over a car seat. These shocks are static discharge events known as electrostatic discharge (ESD). While a shock from a door knob is seemingly harmless, in the industrial setting ESD can be a severe problem, potentially causing damage to electronic components. The use of ESD products such as wrist straps, foot grounders, grounded work surfaces, ESD shielding packaging, ionization products and other measures can help in preventing ESD events. This learning module discusses the main causes of ESD, its damages, and prevention techniques with a few application examples.

2. Objectives

Upon completion of this module, you will be able to:

image Explain static electricity and electrostatic discharge (ESD)

image Describe the leading causes of electrostatic discharge and damages due to ESD

image Discuss the prevention of ESD using protection devices

image Understand control programs to avoid electrostatic discharge

3. Basic Concepts
Back to Top

Electrostatic discharge (ESD) is an unsolicited electrostatic charge transfer when imbalanced electrical charges induce a high electrostatic field on or within a material surface. Visible sparks are created when individually charged objects touch or are brought into close proximity. One familiar example is lightning, a massive-scale ESD event. Even in its less dramatic form, an ESD can be sufficiently large to damage sensitive electronic devices, and because of this ESD influences product reliability and productivity in every industry. The electronics industry uses a variety of ESD-safe antistatic products to prevent damage from ESDs.

image

Figure 1: IC design engineer in antistatic clothing

At its most basic level, ESD occurs when imbalanced and opposite electrostatic charges accumulate due to two surfaces coming into close contact. These charges may accumulate on or within both surfaces to generate an electrostatic field. These accumulated charges are at rest and are termed static electricity.

Static electricity may also be caused by electrostatic induction or tribocharging. Electrostatic induction is the dispersal of an electric charge on a material caused by a charged object nearby. The presence of electric force between charged material particles causes a negatively charged object brought in proximity to an electrically neutral object to induce a positive charge on the neutral object's near side, and a corresponding negative charge on the far side. Additionally, the neutral object may become positively charged via induction if its negative side is briefly grounded to permit the negative charge to escape. Electrostatic induction is unavoidable if an object is put within an electric field.

Triboelectric charging occurs when an electrostatic charge is formed due to contact followed by separation of two or more materials. For example, walking over a carpet involves multiple contacts and separations between shoes and carpet. The atoms of a zero static charge material contain an equal number of positive image protons inside the nucleus and negative image electrons in orbit outside the nucleus. Figure 2 shows the triboelectric charging process between two materials, "A" and "B." Both materials consist of atoms with equal numbers of protons and electrons, and thus they are electrically neutral.

image

Figure 2: Triboelectric Charging (Contact & Separation). Image Source: EOS/ESD Association, Inc.

image Positive image Negative
Fur Sealing Wax
Glass Nickel, Copper, Brass, Silver
Mica Gold, Platinum
Human Hair Sulfur
Nylon Acetate Rayon
Wool Polyester
Lead Silicon
Silk Teflon

Table 1: Triboelectric series table

When both materials are touched and then parted, negatively charged electrons are transferred between the two material surfaces. The nature of these two materials determines which material loses electrons and which one gains electrons. Positively charged materials lose electrons, while negatively charged materials gain electrons. The amount of triboelectric-generated charge depends on the contact area, separation speed, surface work function, relative humidity, material chemistry, and other factors. The newly produced electrostatic-charged object transfers this charge and generates an electrostatic discharge event.

Charges of any magnitude or polarity will seek to balance that charge. Conductive objects will do this very readily. When two conductive objects with different charges come into contact, they will balance their charges. This is an Electrostatic Discharge.

The material’s characteristics affect the magnitude and polarity of the charge generated by the triboelectric charging process. Table 1 illustrates the triboelectric series and how different materials create charges.

- 3.1 ESD Types

Generally, three types of ESD events cause damage: direct ESD to the device, ESD from the device, or field-induced discharges. The device's endurance determines the harm suffered by an ESD-susceptible item (ESDS) against abnormal voltage levels. A device's ESD susceptibility or ESD sensitivity refers to its failure threshold.

image Direct ESD to the device occurs when a charged material directly transfers an electrostatic charge to an ESDS. An individual walking over a floor may accumulate electrostatic charge on their body. ESD damage is possible when this individual physically touches or even comes close to an ESDS or an assembly lead with a different electrical potential. The body may discharge and cause ESD to harm the ESDS. The model employed to simulate such an event is termed the Human Body Model (HBM).  The other model is known as the Charged Device Model (CDM), which describes the metal-to-metal contact that was formerly associated with the Machine Model (See Glossary). The CDM voltage level as used in this document is based on managing process essential insulators to mitigate field induced voltages on devices that could lead to damage.

image ESD from the device occurs when an ESDS transfers the charge to a conductor. The ESDS may accumulate static charge by coming into contact or rubbing against packaging materials, machine surfaces, or work surfaces. This frequently happens when a device vibrates inside a package or moves over a surface. The model employed to simulate such an event is termed the Charged-Device Model (CDM). Automated assemblies may suffer from CDM.

image Field-Induced Discharges: Field induction is yet another electrostatic charging process that may directly or indirectly harm devices. Any electrostatically charged object produces an electrostatic field, and when a grounded ESDS is placed inside this field, a CDM event occurs. A second CDM event may happen if the item is removed from the electrostatic field and then grounded again.

- 3.2 Harmful Effects of ESD and Failure Types

ESD damages electronic components in multiple ways. Large static voltages may burn the internal circuitry of a device. Extremely high voltages may wreak havoc in the compact conductor and insulating barrier. Because of miniaturization, the miniscule sizes of integrated circuits and other components has made devices more vulnerable to static electricity damage. High input impedances enabled by metal oxide semiconductor (MOS) technology hamper voltage dissipation and have only amplified the ESD effects.

ESD damage can occur at any point, from manufacture to field service. The damage is usually classified as either a latent defect or a catastrophic failure. ESD-related catastrophic failures include metal melt, junction breakdown, or oxide failure within the device. The terminally damaged device circuitry can cripple the equipment. In a latent failure, the ESD may cause partial device degradation, even as it executes its desired function. Latent defects are difficult to detect and special attention should be paid to identifying them; as such, ESD damage may culminate in equipment failures down the line, thus reducing reliability.

- 3.3 ESD Standards and Testing

The ESD Association approves and publishes the Electrostatic Discharge Control Program (ANSI/ESD S20.20), an ANSI standard. The ANSI/ESD 20.20 includes both technical and administrative provisions customized to specific applications or requirements. The administrative sections cover the progress of an ESD Control Program Plan, Training Plan, and Compliance Verification Plan with routine audits. The technical requirements cover grounding, personal grounding, protected areas, packaging, labeling, equipment, and handling. ESD testing refers to the process in which a device is tested for its resistance to ESD. It is classified into three main categories: human body model (HBM), machine model (MM), and charged device model (CDM). The EN/IEC 61000-4-2 is the most common standard for ESD testing.

4. Analysis
Back to Top

We will now analyze how to protect a device from ESD, discuss various ESD protective devices, and describe control programs in the electronics manufacturing environment.

- 4.1 Basic Principles of ESD Prevention

It is a challenge to control electrostatic discharge (ESD) in electronics. However, there are four basic principles for ESD control:

image Ground all conductors, including people and work surfaces.

image Use ionization when using process essential insulators or un-grounded conductors.

image Shield ESDS when they are removed from an ESD-controlled area (EPA).

image Manage a compliance verification program to ensure that the controls measures used are working.

image

Figure 3: Ionization Process. Image Source: EOS/ESD Association, Inc.

In the EPA, electrostatic discharges should be safely dissipated or neutralized, as it is impossible to eliminate electrostatic charge generation. Proper grounding and conductive materials should achieve this objective. Because nonconductive parts, such as common plastics and other insulators, cannot be grounded to reduce the charge in a reasonable time, an ionization process that generates negative and positive ions (Figure 3) can be employed.

ESD protection products should be used to shield susceptible parts and assemblies from inevitable random discharges. Various ESD control packaging and material handling products are available for extensive EPA use. These materials reduce in-container movement of products and, consequently, accidental charge production.

- 4.2 ESD Control Programs

Most environments require a judicious mix of ESD control programs. A single procedure is not a cure-all. Although each company is unique concerning its ESD control needs, at least six crucial elements are necessary to successfully develop, implement, and maintain an effective ESD control program.

image

Figure 4: Six Elements of an ESD Control Program. Image Source: EOS/ESD Association, Inc.

image Establish ESD teams and Appoint an ESD Coordinator

A team approach is particularly applicable to ESD, as problems and solutions involve different functions, suppliers, departments, and divisions. The ESD team composition should include a wide variety of personnel from the company, including people with responsibilities overseeing incoming inspection, automation, packaging quality, and training. The ESD coordinator leads the ESD team efforts.

image Assess Organization, Facility, Processes, and Losses

The next step is to gain a thorough understanding of the environment and its impact on ESD. Facilities and procedures should be evaluated, paying special attention to ESD sensitivity data, in order to find areas that may cause ESD problems. The focus should include static generating materials, personnel handling procedures for ESDS components, and the presence of conductors which could come into contact with ESDS components.

image Establish and Document an ESD Control Program Plan

After completing the assessment, a plan should be created, documenting all tasks, activities, and procedures necessary to protect ESDS items. Specifications and procedures should be written and distributed to all departments.

image Justify Your Activity for Top Management Support

Given the severity of ESD risk, ESD programs are typically supported by management. Quality and reliability must be highlighted in reports, and the costs and pitfalls of ESD damage clearly demonstrated, including the potential effect of ESD on customer service and product performance.

image Develop and Implement a Training Plan

All affected personnel must be properly trained to support the organization's ESD control strategies and programs. A written training plan is required for ANSI/ESD S20.20 documented procedures; however, companies have the flexibility of designing plans as they see fit.

image Develop a Proper Compliance Verification Plan and Implement It

An ESD Control Program must be constantly reviewed, audited, and developed, with adjustments made based on feedback or changes in environment or procedures.

- 4.3 Related Components: ESD Protective DevicesBack to Top

image

The potential for ESD events can be mitigated by using ESD protection solutions, such as those provided by Desco Industries. ESD solutions include personnel grounding, grounded mats, testing equipment, ionization products, shielding bags/packaging, and coating and laminating with specialty products.

Personnel Grounding

Products include wrist straps, foot grounders, and ground cords with multiple variations, designed to attach the body to ground.

 

logo
image

09070 - Anti Static Wrist Strap, Grounder, Adjustable, 330mm, 6ft Cord

Buy Now

 

image Extra wide, soft elastic band

image Has silver impregnated polypropylene knitted on inside for superior conductivity

image Reliably removes generated static charges. Additionally, silver fibers are antibacterial to help keep the band and operator clean.

image Date coded: providing lot traceability to ensure quality control.

image UL listed: meets UL & OSHA requirements to ensure operator safety.

For more available products Shop Desco

 

Packaging Products

 

Products include static shielding, moisture-vapor-barrier, clear dissipative, unique bag-in-bag, bags on a roll, and vacuum sealers.

 

logo
image

10068 - 1000 Series Metal-In Static Shield Bag, 6" x 8", 100 EA

Buy Now

 

image Metal-in film laminate 0.0028" thick (2.8 mil) protects ESD sensitive contents from electrostatic fields and electrostatic discharges (ESD).

image <10 nJ discharge shielding energy limit test per ANSI/ESD STM11.31. Meets ANSI/ESD S20.20 and ANSI/ESD S541 requirements for ESD shielding packaging inside and outside an ESD Protected Area (EPA).

image Dissipative inner and outer surfaces Rs 1 x 104 to 11 ohms per ANSI/ESD STM11.11 and static control bag ANSI/ESD S11.4 Level 3. Allows bag to be used throughout an ESD protected area and grounded when placed on a grounded surface or handled by a grounded operator

image OpenTop and ZipTop styles are available

image Lead-free RoHS 2, REACH and conflict minerals compliant

For more available products Shop SCS

 

 

logo
image

38851 - PlastekTm Circuit Board Shipper

Buy Now

 

image Economical and efficient method of shipping or storing circuit boards and other static sensitive electronic devices

image Constructed from conductive (1 x 102 to < 1 x 105 ohms) extruded high impact polypropylene plastic; provides superior strength and durability

image Chemical and moisture resistant

image Economical alternative to injection molded products

image Meets ANSI/ESD S20.20 and packaging standard ANSI/ESD S541

For more available products Protektive Pak

 

 

Dissipative Work Surfaces

These surfaces are designed to provide a surface that does not generate a static charge and will control the discharge rate from all conductors (including ESD susceptible items) that are placed on the surface. They include work surfaces such as 2-layer rubber, homogeneous vinyl, 3-layer, and field service kits.

 

logo
image

66428 - StatfreeRegistered T2 Plus Dissipative Dual Layer Rubber Mat Top Kit, Blue, .060" x 24" x 48"

Buy Now

 

image Dissipative dual layer ESD worksurface: provides a worksurface that does not generate a static charge and will control the discharge rate from all conductors (including ESD susceptible items) that are placed on the surface. (worksurfaces mats must be properly grounded to remove ESD charges.)

image NEW Nitrile rubber oil resistant compound: improved material compound limits oil absorption to improve electrical and physical properties through the lifespan of the material. May be used in soldering applications with flux and other chemicals.

image Dissipative (1 x 106 to <1 x 109 ohms Rtt) top layer - limited lifetime warranty: meets ANSI/ESD S20.20 worksurface required limit and recommendation of ANSI/ESD S4.1 for contact with ESD susceptible items.

image Conductive (<1 x 106 Rtt) bottom layer - limited lifetime warranty: reduces the resistance to ground (Rtg) from the top of the surface to the groundable point ground and allows the material to be used with ESD workstation monitors.

image Ultraviolet (UV) stabilizer additives

For more available products Shop Desco

 

 

ESD Flooring

Products are designed to prevent static electricity from building up as people that are wearing foot grounders work and move about the environment. They include flooring products such as rolled matting, floor finish, cleaners, and rubber tiles.

 

logo
image

46032 - ESD Floor Cleaner, 2.5 Gal

Buy Now

 

image ESD flooring cleaner

image Cleans conductive/dissipative floor tile, paint, latex, floor finish and other ESD flooring substrates.

image Does not contain silicone or other insulative substances: standard cleaners with silicone or other insulative substances may leave residue which inhibits the performance of ESD flooring.

image Bag-in-box packaging available

image Lead-free RoHS compliant

For more available products Statguard Flooring

 

 

ESD Test Equipment

ESD test equipment is used to verify that the ESD control devices in use are functioning correctly. These devices include ESD event meters, data acquisition systems, continuous monitors, personnel grounding testers, static field meter, ionization test kit, and surface resistance meters.

 

logo
image

724MO - ESD Tester, Workstation Monitor for 2 Operators and 1 Work Surface

Buy Now

 

image Single workstation continuous monitor: meets ANSI/ESD S20.20 in accordance with ESD TR1.0-01-01

image Continuously monitors 2 operator dual-wire wrist straps and 1 work surface mat. Visible and audible alarms indicate improper grounding of the operator and work surface.

image Adjustable operator test voltage and upper limit. Test voltage can be set to 9 or 16 volts; test limit can be set to 10 or 35 megohms.

image Adjustable audible alarm, buzzer volume may be disabled or set to loud or soft.

image UL safety certified. Complies UL category code number NYOK

image NIST calibrated with certificate included

For more available products Shop SCS

 

 

ESD Brushes

 

ESD brushes are used to remove dust, dirt, and other leftover materials from PCBs and other static sensitive components. The brushes are designed to minimize charge generation and remove electrostatic charges when held by a grounded user.

 

logo
image

36092 - Conductive, Flat Handle, Black Soft Nylon Bristles, 2"

Buy Now

 

image Allows thorough cleaning of ESD sensitive assemblies without the danger of high charges generated by conventional brushes when held by grounded personnel

image Conductive carbon loaded polypropylene handle

image ESD properties of conductive handles are not affected by humidity as are wooden handle brushes

image Conductive bristles made of black soft carbon nylon

image Firm bristles are mainly for electronics, especially on circuit boards used for removing solder and/or rework debris

image Rtt resistance: 1 x103 to <1 x105 ohms

For more available products Shop Menda

 

 

Ionization Products

Ionization products neutralize charges on insulators preventing induction and charged device model defects to static sensitive devices. Ionizers come in several designs, such as overhead, benchtop, and compressed air.

 

logo
image

980E - Ionizer, Air Gun, Bench Top, 130VAC, Calibrated

Buy Now

 

image Point-of-use compressed air ionizer. Neutralize electrostatic charges to eliminate Electrostatic Attraction (ESA), visual imperfections, and contamination by dislodging charged dust and debris

image Fast < 1 second discharge times with ±30 volt offset voltage balance tested per ANSI/ESD STM 3.1 and ESD TR53. Meets ANSI/ESD S20.20 ionizer required limits

image Modular design with 7 foot ESD protective hose with trigger switch. Allows operators freedom of motion and minimizes awkward or unsupported positions

image Use filtered air or nitrogen – no adjustment required. Allows for quick change between compressed gas supply

image NIST calibrated with certificate included

image cULus, CE, RoHS2

For more available products Shop SCS

 

 

Garments

 

Garments are designed to shield static sensitive devices from static electricity that may build up on a person’s clothing.

 

logo
image

221430 - StatshieldRegistered Smock, Black Jacket with Knitted Cuffs

Buy Now

 

image Groundable static control garment system tested per ANSI/ESD S20.20-2014 (Rtg < 3.5 X 107 ohms) requirements, per ANSI/ESD STM2.1. Allows operators and smock to be bonded or electrically connected to ground to prevent ESD events in ESD protected areas.

image Minimum of 9% carbon conductive nylon fibers woven in Chain-Link Design. Provides continuous and consistent charge dissipation throughout lifetime of smock.

image Creates Faraday Cage Effect around torso and arms of operator. Shields ESD charges on operators' clothing from damaging ESD sensitive items.

image Panel-to-panel conductivity. Prevents isolated charged conductor in ESD protected area.

image Hip-to-cuff grounding. Grounds operator with no need for a cord to be attached to the operator's wrist.

For more available products Shop Desco

 

5. Glossary
Back to Top

image American National Standards Institute (ANSI):  a non-profit organization that coordinates the development of voluntary standards for several industries in the U.S.

image Charged Device Model (CDM): a test model that simulates an ESD when a component comes into contact with a conductive material or electric field, such as in a manufacturing environment, and is charged either directly or indirectly.

image Electrostatic Discharge (ESD): the rapid, sudden flow of electrostatic charge that occurs when two objects come into contact or close proximity with each other.

image Electrostatic Induction: the induction of an electrical charge in a material when brought into proximity with another charged object.

image Electrostatic Protected Area (EPA): a designated area where all surfaces, people, objects, and ESDS devices are kept at the same electrical potential.

image ESD Susceptible or Sensitive (ESDS): components or devices that are easily affected or damaged by even small amounts of ESD.

image Human Body Model (HBM): a test model that simulates how a component might be affected when an ESD generated by a human contact occurs.

image Machine Model (MM): a test model designed to simulate an ESD from equipment, such as electrical devices, components, or empty sockets, to the component being tested.

image Metal Oxide Semiconductor (MOS): a structure for creating electronic components, like transistors, where the insulator layer is typically an oxide of the substrate layer.

image Static Electricity: a charge caused by the imbalance between negative and positive charges on the surface of or within an object.

image Triboelectric Charging: a type of electrical charging where materials become charged after coming into contact and then being separated from a different material.

*Trademark. Desco Industries is a trademark of Desco Industries Inc. Other logos, product and/or company names may be trademarks of their respective owners.


 

Test Your KnowledgeBack to Top

image

Are you ready to demonstrate your knowledge of Electrostatic Discharge and Prevention? Then take a quick 10-question quiz to see how much you've learned. To earn the Static Control I Badge, read through the learning module, attain 100% on the Quiz, leave us some feedback in the comments section, and give the learning module a star rating.

 

Attachments:
image Static Control 1.pdf

  • electrostatic_discharge
  • static_control
  • desco
  • ess_module
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • kmikemoo
    kmikemoo over 5 years ago +7
    It's so easy to ignore - until you snap an IC that you only had one of.
  • Fred27
    Fred27 over 5 years ago +7
    My kids recently discovered they can generate a lot of charge jumping on a trampoline with a safety net around it, so I taught them what was going on. Rather than minimizing ESD they prefer maximizing…
  • shabaz
    shabaz over 5 years ago +6
    Very useful information. The mat kit looks really good, seems like a reasonable price too. Regarding brush, I currently use a record player antistatic brush, it comes in handy to remove charges from insulators…
Parents
  • kmikemoo
    kmikemoo over 5 years ago

    It's so easy to ignore - until you snap an IC that you only had one of.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kmikemoo
    kmikemoo over 5 years ago

    It's so easy to ignore - until you snap an IC that you only had one of.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hifromkatie
    hifromkatie over 5 years ago in reply to kmikemoo

    We were doing a group project in uni, had a budget for parts and have to submit part orders to the lab technician on paper, to be ordered at the end of the week, and arrive the next.

    We ordered 1 pic microcontroller... I'll put my hand up and say I removed my jumper, went and pointed at something in the circuit, got a big static shock off the table leg at the same time as I touched the pic, and it didn't work again.

    I've never forgotten, important lesson learnt, and our coursework was then put back by a week as at had to order another part

    • Cancel
    • Vote Up +4 Vote Down