555 Timers
  • Technologies
  • More
555 Timers
Forum Understanding 555 timer in astable mode but stuck on capacitors
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 7 answers
  • Subscribers 53 subscribers
  • Views 9262 views
  • Users 0 members are here
  • capacitor
  • 555 timer
Related

Understanding 555 timer in astable mode but stuck on capacitors

opalko
opalko over 5 years ago

So I am still plowing my way through Platt's Make: Electronics and into chapter 4 working with the 555 timer IC.  The astable mode of the timer is giving me trouble as I don't understand how

 

When C1 acquires 2/3 of the positive voltage powering the circuit, the 555 reverses its output on Pin 3 from positive to negative and forces C1 to discharge itself through R2.

(This last sentence is actually from Make Magazine issue 10 where Platt is explaining the same thing as in chapter 4 of his book - see image below)

 

image

 

What I am confused about is the discharging through R2.  I am obviously stuck on what is going on with C1. As I understand it, it first gains a positive charge on what I will call the top plate in the picture above, and a negative charge on the bottom plate (next to where the label C1 is).  Maybe I have read too many analogies of water with electricity but I think of the capacitor as a balloon (in fact there are many analogies in Platt's book like this).  So how is the balloon releasing the pressure in what seems like a reverse direction back through R2?  Here is a similar circuit I found on circuitlab albeit the pins arranged differently and it shows that reversing of "flow":

 

image

 

Is there not +5V into R2 from R1 at the same time C1 is discharging??

Finally here is Platt's "internal" view of the 555 timer in astable mode.  I assume pin 7 gets grounded to pin 3 but I am still confused about the seemingly reversal of flow through R2.

 

image

I've read through this many times and still stuck. Any additional help is appreciated!

 

Cheers

 

Message was edited by: Robert Opalko same day

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +6 verified
    Hi Robert, During the discharge part of the cycle the Pin 7 is attached to ground. (see the blue - in the last picture). Once pin 7 is connected to Ground the electricity in C1 starts to move through R2…
  • jw0752
    jw0752 over 5 years ago in reply to opalko +6 suggested
    Hi Robert, The polarized capacitors must be used in the correct polarity as they will fail if more than a token voltage is applied in the reverse direction. The polarity on the capacitor is not like that…
  • jw0752
    jw0752 over 5 years ago +5
    PS you are doing an excellent job of presenting your questions. I would bet that several times you have actually answered them yourself in the process of preparing the question. John
Parents
  • jc2048
    0 jc2048 over 5 years ago

    When you charge a capacitor, the increasing imbalance of charge causes the voltage between the plates to increase and

    the resulting electric field between the plates then stores energy. When you discharge the capacitor, that

    energy is then powering the discharge circuit.

     

    Personally, I don't much like bucket [water] and balloon [air] analogies. A capacitor isn't simply a

    container that you to pour something in to. When you add charge to one plate, you always remove the same

    charge from the other. It's the resulting imbalance between the two that stores energy and it can be either

    way round (leading to a voltage in either direction across the capacitor). Negative amounts of water and

    negative pressures are a bit weird, when you think about it. [Yes, the maths works with 'negative water'

    too, but what's the point? You're then struggling to explain an analogy that's supposed to make things

    easier to understand.]

     

    When we charge or discharge a capacitor, that flow of charge constitutes a current. Current paths are loops

    'driven' by voltage sources.

     

    Here is the current path [red] when the capacitor charges

     

    image

     

    and here is what happens when the 555 connects pin 7 to ground [black] and the capacitor discharges

     

    image

     

    There are now two paths. The current through R1 [red] now flows back to the supply through the 555. At the

    same time, the capacitor voltage drives a current through R2 [green] that returns to the other side of the

    capacitor through the 555. That current discharges the capacitor. [As it discharges, the voltage across the

    capacitor reduces until it reaches the lower threshold, at one third the supply voltage, at which point the

    555 removes the connection from pin 7 to gound and the capacitor starts charging again.]

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to jc2048
    'negative water'

     

    I'm not a big fan of the analogy either, but it helps to get the discussion started.

    I try to explain negative water with a "very empty" bucket. Again not a good example, just a hook to get the discussion going without having the attendee's eyes glaze over or have them walk away after a few seconds.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to jc2048
    'negative water'

     

    I'm not a big fan of the analogy either, but it helps to get the discussion started.

    I try to explain negative water with a "very empty" bucket. Again not a good example, just a hook to get the discussion going without having the attendee's eyes glaze over or have them walk away after a few seconds.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer