STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Blog Access Raspberry pi GUI and command line from your windows machine using SSH and VNC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: deepankarmaithani
  • Date Created: 7 Jul 2015 5:43 PM Date Created
  • Views 19223 views
  • Likes 3 likes
  • Comments 16 comments
  • raspberrypi
  • stem space
Related
Recommended

Access Raspberry pi GUI and command line from your windows machine using SSH and VNC

deepankarmaithani
deepankarmaithani
7 Jul 2015

Access Raspberry pi GUI and command line from your windows machine using SSH and VNC

At times you might face a situation when you cannot connect your Raspberry pi to a monitor ,like in a situation when you actually don't have a monitor or when you have your pi working in a project like say a weather monitor and it is not possible to physically access. There is a possible solution to this using SSH  and VNC(Virtual network computing) and you only need to satisfy one condition for this and that is you should have your pi connected to the network using LAN or wifi. Here in this post i will show you how to do this.

 

Step1: know the IP address of your pi,

for getting the IP address there are several methods you can follow any of them

Method-1

If you know the admin password of your wifi router open your browser and enter the adddress of your router it is generally if you enter 192.168.l.l in your browser on a computer connected to your router you will be prompted or admin password and username once you enter it you can get the IP addres of your connected devices

Method-2

If you donot have admin details of your routerConnect your android phone to your home network .install an app like wifi inspector from the google store and run it it will give you the ip address and mac address of al the connected device. This is the simplest method.

 

Method-3

This method require good understanding of commands and network.

In the command prompt

you can use ping raspberrypi and it will give you the IP address it may or may not work for you.

you can also use netstat -r in the command prompt this will give you IP address of all your network routes and one of the ip address in the list will be of your pi but for this you need to be sure that the pi has successfully connected to the network.Or else you can use a software like nmap.

 

 

 

Step2: Download putty. It is a small softwae that lets you establish an SSH connection.Run putty and type this IP address of your pi in the host name under the sessions. and click open

image

 

 

Then login using login ID and password. Default is pi and raspberry respectively.

 

image


Step3: install VNC server using the command sudo apt-get install tightvncserver

image

 


Step4: type tightvncserver to start the server socket.It will prompt you for password enter the password. this password that you will set will be required to be fed into the VNC client.It would also ask you if you would like to set another readonly password press N to dismiss


Step5: Setup a socket by using the command vncserver :1 -geometry 800X600 -depth 24
(The part after the 1 is optional)
Step6: Install a VNC client like the real VNC view https://www.realvnc.com/download/viewer/

 


Step7: open putty enter the host IP(the ip of raspberrypi) in the host field under sessions. Then go to tunnels under the SSH tab.add source to be 5901 and destination to be hostIP:5901. then click add.Finally  click open.

image

 

 

Step 8: log in into the pi using putty
step9: Open real VNC  view. Under the VNC server name add localhost:5901. click connect. then click continue on the next popup.

image

image

 

 

 

 

 

After this you will be prompted for password. Enter password that you have setup while setting up the vnc server and you will get the screen of your Pi.

 

image

  • Sign in to reply

Top Comments

  • rolandl
    rolandl over 11 years ago +3
    Another command that might be of interest is: mosh https:// mosh .mit.edu/ Remote terminal application that allows roaming , supports intermittent connectivity , and provides intelligent local echo and…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to deepankarmaithani +1
    Hello Deepankar, ffrankly I think no. There are several levels accessing a remote machine via ssh that is the securing tunnel. VNC is just the application. In a linea of principle, AFAIK it is not needed…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to deepankarmaithani +1
    In your local lan you don't need a DNS, instead you need to setup a static IP address that will remain the same at every boot. Enrico
Parents
  • ted.chankt
    ted.chankt over 10 years ago

    Anyone have experience using direct cable connection and internet connection sharing?

     

    I frequently conduct workshops where there is no LAN, only WiFi with Internet access. I do not want to invest on switches and cables and do not want attendees to buy WiFi dongle. 

     

    My preferred setup will be direct cable connection where Pi gets internet access from a LAN cable connected laptop with WiFi internet access. Exploring this option where Windows and Ubuntu laptop can use the "internet connection sharing" feature under network settings configuration of the respective OS.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to ted.chankt

    With Windows, the PC can eventually auto-obtain an IP address (feature known as APIPA), if there is no DHCP server. The Pi could be set up with a fixed IP address on that network. However if you're using a Linux PC then I don't think linux supports that feature, so you'd have to explicitly configure a static IP address on the Linux PC. It is all described here: https://pihw.wordpress.com/guides/direct-network-connection/

    Or you could run a DHCP server on the Pi, means no config needed on the PC end, provided the PC is set up for DHCP which it usually is.

    Info here (PDF): http://my-music.mine.nu/images/rpi_raspbianwheezy_dhcp_server.pdf

     

    Edit: Just read the last sentence of your post, referring to Internet Connection Sharing. So just to be clear, will the PC be connected to the Internet via WLAN too? And you wish the Pi to access the Internet?

    If so, now things are messier and your attendees now need to configure their PC in different ways depending on if they have Windows or Linux running on it.

    For Windows, see here: Carbon Stone: Connecting to Pi from Laptop's Ethernet Port

    For Linux, see here: https://www.raspberrypi.org/forums/viewtopic.php?t=6997&p=87671

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 10 years ago in reply to ted.chankt

    With Windows, the PC can eventually auto-obtain an IP address (feature known as APIPA), if there is no DHCP server. The Pi could be set up with a fixed IP address on that network. However if you're using a Linux PC then I don't think linux supports that feature, so you'd have to explicitly configure a static IP address on the Linux PC. It is all described here: https://pihw.wordpress.com/guides/direct-network-connection/

    Or you could run a DHCP server on the Pi, means no config needed on the PC end, provided the PC is set up for DHCP which it usually is.

    Info here (PDF): http://my-music.mine.nu/images/rpi_raspbianwheezy_dhcp_server.pdf

     

    Edit: Just read the last sentence of your post, referring to Internet Connection Sharing. So just to be clear, will the PC be connected to the Internet via WLAN too? And you wish the Pi to access the Internet?

    If so, now things are messier and your attendees now need to configure their PC in different ways depending on if they have Windows or Linux running on it.

    For Windows, see here: Carbon Stone: Connecting to Pi from Laptop's Ethernet Port

    For Linux, see here: https://www.raspberrypi.org/forums/viewtopic.php?t=6997&p=87671