CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog 10 CodeBug Projects in 10 Days: Raspberry Pi Controlled CodeBug with I2C
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: element14Dave
  • Date Created: 7 Oct 2015 8:01 PM Date Created
  • Views 1915 views
  • Likes 20 likes
  • Comments 4 comments
  • codebug_advanced
Related
Recommended

10 CodeBug Projects in 10 Days: Raspberry Pi Controlled CodeBug with I2C

element14Dave
element14Dave
7 Oct 2015
imageIntroducing CodeBug!

image  What is CodeBug

image  10 CodeBug Projects in 10 Days

image  Are You a STEM Educator?

 


This project will actually be a little different than our previous projects. Rather than taking advantage of the Blockly interface and emulation plug in on

http://www.codebug.co.uk. we'll be bringing the Raspberry Pi into the mix.


Follow the steps below to get started on this advanced project Thomas Macpherson-Pope pulled together from CodeBug.org.uk


What you need:

CodeBug

Micro USB Cable

Raspberry Pi

Computer

 


The Project


Connecting CodeBug to your Raspberry Pi can unleash it’s full potential. Your programs can:

  • Make CodeBug respond or control Minecraft
  • Display your Tweets on CodeBug
  • Control CodeBug from hundreds of miles away remotely over the web
  • Turn CodeBug’s LEDs on and respond to its buttons
  • Create games, and anything you can imagine, and program in Python
  • Hook up with Internet of Things devices

 

CodeBug tethering works by putting a special project file onto your bug and plugging CodeBug onto your Raspberry Pi’s GPIO pins. To learn how to put the special project file for teather on to the CodeBug please see 10 CodeBug Projects in 10 Days: Teathering CodeBug with Python.

Next we will need to fit the CodeBug onto the Raspberry Pi. CodeBug connects straight to Raspberry Pi's GPIO header through CodeBug''s expansion connector. While the Pi is diconnected from power, align CodeBug to the pins shown in the diagrams below and gently push CodeBug's connector onto the GPIO pins. Make sure to NEVER connect the Micro USB or use a battery with CodeBug while it is fitted to a Raspberry Pi.

Make sure you select the appropriate Raspberry Pi model, the Raspberry Pi expanded its GPIO header from 26 pins to 40  with the Raspberry Pi Model B+

        imageimage

If you are still unsure which Raspberry Pi GPIO pins to connect CodeBug to, note the pin labels on the back of CodeBug, and connect these to the corresponding pins on your Raspberry Pi.

image

Now it's time to power up the Raspberry Pi !

First, let's make sure to enable I2C by opening a Terminal window and running

 

sudo raspi-config

Next let's choose:

Advanced Options > Would you like the I2C interface to be enabled? > Yes Would you like the I2C kernel module to be loaded by default? > Yes


Next we will install the Python libraries that will talk to the CodeBug using the I2C GPIO pins.
In the Terminal window, type

 

sudo apt-get update sudo apt-get install python3-codebug-i2c-tether

 

Download this example to your Raspberry Pi (right click Save Link As…)

We'll run the example in the Terminal with the following command

python3 example.py

We should see an arrow pointing up-left on the CodeBug’s LED display!

image

We  can write our  own Tethered CodeBug programs using Python and a few simple commands to control  CodeBug. In the next steps we will start an interactive Python session and enter commands to interact with the tethered CodeBug.

Open a Terminal and type

python3

There will be a python prompt appear >>>. Let's import the CodeBug I2C library by entering

import codebug_i2c_tether cb = codebug_i2c_tether.CodeBug() cb.open() cb.set_pixel(2,2,1)

We should see the center LED light up on CodeBug.

Next we'll try setting a row of CodeBug’s LEDs at the same time

cb.set_row(3,0b10100)

We should  see the third row of LEDs light up in the sequence we gave. 0b10101 is a binary value. The 0b shows that it is binary and the 10100 determines which LEDs are on. 1 represents on and 0 represents off. This means that the LED to the far left is on (column 0), the next LED is off and the next on (column 2), and the other two LEDs are off.

image

Now its time to write text on the CodeBug’s LEDs, using the command

cb.write_text(0, 0,'A')

An A will appear on the CodeBug LEDs

Write scrolling text on the CodeBug’s LEDs, using the command

for i in range(0,-30,-1): cb.write_text(i, 0, 'Hello', direction="right")  time.sleep(.1)

The text "Hello" will scroll

Check whether a button is pressed, by giving get_input either an ‘A’ or a ‘B’ or numbers 0-3.

cb.get_input('A')

This will return True if the button is pressed, otherwise it will return False.

To access the full list of command available we can type the following on the interactive Python shell with the codebug_i2c_tether library imported.

help(codebug_i2c_tether.CodeBug)

We can write long programs for Tethered mode CodeBug by writing commands in the text editor and saving and running the file in the way we did with the examples earlier, (python yourfile.py).

Tethered mode gives CodeBug access to the full computing power, functionality and network connectivity of the Raspberry Pi!

Make the most of the variety of powerful yet easy to use Python modules allow the CodeBug to generate random numbers, create email alerts or even post to Twitter!



See more CodeBug projects and learn how you can get one of your own by visiting: 10 CodeBug Projects in 10 Days

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 11 years ago +3
    "To learn how to put the special project file for teather on to the CodeBug please see 10 CodeBug Projects in 10 Days: Teathering CodeBug with Python ." The I2C tether project is different to the USB one…
  • volly
    volly over 10 years ago +2
    Adding the Raspberry Pi makes this so powerful.....I better stop now, else I won't get any sleep....
  • steve76
    steve76 over 8 years ago +2
    How to combine the simplicity of CodeBug with the power of the Raspberry. Very interesting ideas to create new projects.
Parents
  • volly
    volly over 10 years ago

    Adding the Raspberry Pi makes this so powerful.....I better stop now, else I won't get any sleep....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • volly
    volly over 10 years ago

    Adding the Raspberry Pi makes this so powerful.....I better stop now, else I won't get any sleep....