CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog CodeBug 'show n tell' - Spinny blocks
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 29 Sep 2015 3:59 AM Date Created
  • Views 4480 views
  • Likes 10 likes
  • Comments 31 comments
  • codebug
  • codebug_intermediate
Related
Recommended

CodeBug 'show n tell' - Spinny blocks

e14 Contributor
e14 Contributor
29 Sep 2015

Spinny Blocks

image

A CodeBug had made itself at home in my mail this morning; so I took the little guy in and decided to look after him!

 

Above is the CodeBug simulator showing a short sprite animation, you can see the animation running on a live CodeBug in the video below. All was done in the 'blocky' graphical code blocks editor which is intuitive to use and has the option of switching into a traditional text style editor.

 

I haven't tried the text editor yet, hopefully switching between the 2 will preserve true changes (graphical style editors have a habit of erasing or overwriting things entered manually).

 

I'm going to try using the iic and spi port soon but don't think those features have been enabled as yet, there is a download to allow it to act as a slave device but not in conjunction with the programs we can create, hopefully the firmware interpreter will mature overtime to allow things like this and also maybe inline asm or c for adding a bit of efficiency!

 

The mcu is a pic18f2550 and there are pogo pads for reprogramming the pic which opens up the option of using microchips C18 c compiler and programming your own firmware to it with an appropriate pickit programmer of some sort if the interpreter becomes too restrictive, however Im going to work as much with the installed interpreter, even considering trying to get a copy of the hex file so I can put it onto one of the 2550's in my dev box.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +3
    Sometimes going back to basics and being restricted can lead to much more simple and fun things! and generate alternative solutions to problems! Remember that the led's are multiplexed and blinking on…
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics +2
    It's a good challenge to do some IoT with these things Perhaps we should leave them as simple easy to program devices. I do wish there was an offline editor, and maybe it will come. Unfortunately the…
  • mcb1
    mcb1 over 11 years ago in reply to gregoryfenton +2
    The comment above disappeared ... I think Enrico has one arriving so problem solved. Mark
Parents
  • mcb1
    mcb1 over 11 years ago

    They are slightly adictive aren't they?

     

    Have you come up with a clever way to fasten to to clothes as a wearable.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    It's a good challenge to do some IoT with these things image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics

    It's a good challenge to do some IoT with these things

    Perhaps we should leave them as simple easy to program devices.

    I do wish there was an offline editor, and maybe it will come.

    Unfortunately the NZD makes them expensive at $34.35 compared with some other more capable boards.

     

    The BBC Micro has many more capabilities, which may suit IoT.

     

    However some interactivity between Codebugs might be worth looking at ... maybe IR.

     

    mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    I agree Mark,

     

    but the problem is that at the actual date we have really few infos on this device. For example: what is the program space, ram and so on? Should check on the PIC IC datasheet? Maybe yes. This is essential to know the limits of the hardware. You mention IR, I have already though to this but the problem in this case - I suppose - it will the memory for programming space. What does it remain for the rest of the app ?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    Ir was also an immediate thought! a little idea i've been working out in my head recently is the possibility of using ir to transmit the 1-wire bus protocol, could be fun trying!

     

    It might be fun to get him to respond to ir remote commands too, and most mobiles and tablets come with a never used ir dataport..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Maybe it is a delusion but I think that it is (sadly) very difficult to find an "old" IR port on the last two or three generations of smartphones and tablets. Amazon sells food multi-protocol IR devices full of buttons for 3-5$ image (while Sparkfun sells its own with veeeery few buttons for almost the same price (5$) https://www.sparkfun.com/products/11759 ) Less buttons higher price?


    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    Im sat writing this on my galaxy tab with a sony xperia next to me both sporting ir ports. As a point of interest, there are apps you can download that allows you to turn your phone/tab into a remote control!

     

    Maybe the cheap chinese knock off replicas dont have them as a way of saving costs..

     

    The only question is whether the ir ports are bidirectional

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    Im sat writing this on my galaxy tab with a sony xperia next to me both sporting ir ports. As a point of interest, there are apps you can download that allows you to turn your phone/tab into a remote control!

     

    Maybe the cheap chinese knock off replicas dont have them as a way of saving costs..

     

    The only question is whether the ir ports are bidirectional

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    AFAIK the IR ports are always bidirectional in computer(ised) devices as these are used instead of a traditional serial communication to exchange data with the remote unit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    I use that IR app on the Samsung a lot.

    (because the rubber volume control on the otherwise-excellent TV remote control have lost their conductivity.

    when I asked for a replacement, Amazon wanted me to ship the entire TV to them for a replacement!

    It felt wrong to do that..).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gregoryfenton
    gregoryfenton over 11 years ago in reply to shabaz

    Know the feeling with regard to the loss of conductivity.

     

    Easy fix, normally comes down to one screw.

    Strip the remote down (remove the batteries first!)

    Clean the crud out (how do chips get in there?!)

    Remove the rubber surface.

    Clean it in a sink with warm soapy water.

    Dry it with a towel.

    Reassemble everything.

    Profit!