CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog CodeBug 'show n tell' - Spinny blocks
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 29 Sep 2015 3:59 AM Date Created
  • Views 4461 views
  • Likes 10 likes
  • Comments 31 comments
  • codebug
  • codebug_intermediate
Related
Recommended

CodeBug 'show n tell' - Spinny blocks

e14 Contributor
e14 Contributor
29 Sep 2015

Spinny Blocks

image

A CodeBug had made itself at home in my mail this morning; so I took the little guy in and decided to look after him!

 

Above is the CodeBug simulator showing a short sprite animation, you can see the animation running on a live CodeBug in the video below. All was done in the 'blocky' graphical code blocks editor which is intuitive to use and has the option of switching into a traditional text style editor.

 

I haven't tried the text editor yet, hopefully switching between the 2 will preserve true changes (graphical style editors have a habit of erasing or overwriting things entered manually).

 

I'm going to try using the iic and spi port soon but don't think those features have been enabled as yet, there is a download to allow it to act as a slave device but not in conjunction with the programs we can create, hopefully the firmware interpreter will mature overtime to allow things like this and also maybe inline asm or c for adding a bit of efficiency!

 

The mcu is a pic18f2550 and there are pogo pads for reprogramming the pic which opens up the option of using microchips C18 c compiler and programming your own firmware to it with an appropriate pickit programmer of some sort if the interpreter becomes too restrictive, however Im going to work as much with the installed interpreter, even considering trying to get a copy of the hex file so I can put it onto one of the 2550's in my dev box.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +3
    Sometimes going back to basics and being restricted can lead to much more simple and fun things! and generate alternative solutions to problems! Remember that the led's are multiplexed and blinking on…
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics +2
    It's a good challenge to do some IoT with these things Perhaps we should leave them as simple easy to program devices. I do wish there was an offline editor, and maybe it will come. Unfortunately the…
  • mcb1
    mcb1 over 11 years ago in reply to gregoryfenton +2
    The comment above disappeared ... I think Enrico has one arriving so problem solved. Mark
Parents
  • spannerspencer
    spannerspencer over 11 years ago

    Wow, fast work Lucie! It only just went in the post image

     

    Along similar lines to your idea for IR communication between CodeBugs, I was wondering if there was any way to make some simplified QR Code-type images, using its LED display, which could then be read by a smartphone app. Maybe they could even cycle through a few such codes, to increase the amount of info it's transmitting.

     

    It's one way communication, admittedly, and I don't know quite what it'd be useful for, but it's something to think about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to spannerspencer

    spannerspencer

    I like the 'almost QR code' thing.

    I think it has some potential.

     

    Now if we could only encourage some app developer ...say ntewinkel to advise on some options, we might be able to have something.....

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Hi Mark & Spanner,

     

    I have a certain experience in barcode and Qr code reading. Maybe that the source of a Qr code library can be modified to accept a led coding. But how do you think it is possible - maybe I don't know - to generate a Qr code with the LEDs only?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics

    balearicdynamics

    I have a certain experience in barcode and Qr code reading

    Perfect.

    Maybe that the source of a Qr code library can be modified to accept a led coding

    I think replicating the QR code might be difficult ... but it might be possible to provide something in an app that will read a coded message.

     

    ie it starts with the three corner LED's on.

    Then flashes all LEDs, then provides a series of LEDs on.

    The punch tapes were 5 bit, so maybe that might be an option ...show 5x 5 bits then wait and another 5x 5 bits ..

    ie

     

    image

    borrowed from here   http://www.lauftext.de/cybernetic-computer/punched-information.htm

     

    Mark

     

    BTW this is well worth a visit. I'm glad I did while in England

    https://www.picotech.com/library/application-note/colossus-the-worlds-first-computer

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Mark,

     

    what you say is true. In effect I was thinking just to the Barcode/Qr Code. Using the old punch card reader technique, that some of us knows very well it is more than possible. This LED matrix of the CodeBug remember me just the "modern" (around 1982) punch reader heads where the demodé sliding contacts was replaced by photo diodes...

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 11 years ago in reply to mcb1

    Maybe it could work in an even more simplified manner, by flashing the whole LED matrix semaphore/Morse code style? It'd work at much greater distances then, as the LEDs are plenty bright!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • spannerspencer
    spannerspencer over 11 years ago in reply to mcb1

    Maybe it could work in an even more simplified manner, by flashing the whole LED matrix semaphore/Morse code style? It'd work at much greater distances then, as the LEDs are plenty bright!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to spannerspencer

    Have you seen the electric imp? its an "iot" microcontroller with the form factor of an sd card. from what i understand it can be programmed by blinking a mobile phone screen on and off to transmit data. presumably this can be done in reverse by using the mobile camera.

     

    Just a thought for some inspiration!