CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Forum Heavy Load Switching with CodeBug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3070 views
  • Users 0 members are here
  • codebug
  • transistor
  • relay
Related

Heavy Load Switching with CodeBug

spannerspencer
spannerspencer over 11 years ago

Has anyone tried switching slightly heavier loads using the CodeBug's legs, either using a transistor or a relay? I'm working on something that'll need to switch two loads on and off that I'm pretty sure would melt the CodeBug if I did it directly (maybe 1-2 amps each). I'm thinking that something as simple as a transistor, switched from one of the legs, would do the job, but thought I'd ask if anyone's experimented this as yet?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +4
    The 'GPIO Explained' schematic with the transistor and relay should work too. (For some reason the editor is mangling the URL - will raise a feedback & support request. Circuit is below): ( Finder 32.21…
  • michaelkellett
    michaelkellett over 11 years ago in reply to jc2048 +2
    Oh John, you're such an optimist I read the same data sheet and come away with 40 - 50 mOhms (40 @ 2.5V gate drive + about 30% for being hot). But still good for 3A (just about at ambient = 25) MK
  • mcb1
    mcb1 over 11 years ago +1
    At the risk of a certain intervention ... http://www.itead.cc/electronic-brick-5v-relay.html?___SID=U http://www.itead.cc/2-channels-5v-relay-module.html?___SID=U If you check the wiki they include a transistor…
Parents
  • mcb1
    0 mcb1 over 11 years ago

    At the risk of a certain intervention ...

    http://www.itead.cc/electronic-brick-5v-relay.html?___SID=U

    http://www.itead.cc/2-channels-5v-relay-module.html?___SID=U

     

    If you check the wiki they include a transistor driving the relay.

     

    The other thought is Terry King has optocoupled units.

    http://yourduino.com/sunshop2/index.php?l=product_detail&p=218

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 11 years ago

    At the risk of a certain intervention ...

    http://www.itead.cc/electronic-brick-5v-relay.html?___SID=U

    http://www.itead.cc/2-channels-5v-relay-module.html?___SID=U

     

    If you check the wiki they include a transistor driving the relay.

     

    The other thought is Terry King has optocoupled units.

    http://yourduino.com/sunshop2/index.php?l=product_detail&p=218

     

    Mark