STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum Wind turbine design
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 59 subscribers
  • Views 4257 views
  • Users 0 members are here
  • stem space
Related

Wind turbine design

e14 Contributor
e14 Contributor over 11 years ago

OK not sure whether this should be here or in power management, but I am choosing engineering

 

This is a new subject to me in relation to the physical build of a turbine

 

I wonder if anyone can tell me why the vanes are perpendicular to the wind direction instead of parallel to the flow of wind

 

In my eyes it may be easier to build a turbine with variable direction blades depending on the speed of the wind so that they are facing the sky, which would reduce the directional workings from the complexity of the design

  • Sign in to reply
  • Cancel

Top Replies

  • dragonstyne
    dragonstyne over 11 years ago in reply to mcb1 +1
    I agree, over reving is a big issue also, more surface area provides better performance in lower wind situations. Larger wind turbines tend to create RF noise due the varying capacitance between the blades…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to dragonstyne +1
    Are now we are getting into different area of problems that I had forgotten about EMF and RF interference, I remember testing equipment against that (in an old employment) but had not even thought about…
  • jw0752
    jw0752 over 11 years ago

    Hi Mike,

    The wind turbine works by absorbing some of the momentum of the air molecules in the wind with the vanes or impellers of the turbine. The design with the impellers perpendicular to the wing provides a means of offering a reasonable cross section of surface to the wind and not having to bring any of the surfaces against the direction of the wind. Many of the more sophisticated turbines have a way to feather the impellers so that they can react to higher speed winds.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    Hi John

     

    My original idea was to use something like the wind speed sensors on a larger scale, and ovalled a bit to look like a deep tablespoon, but then was not sure if it would work and not having the time to experiment at the moment thought I would throw the idea open

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    The wind cup design is very functional if you do not have an appreciable load. The power comes from the difference between the effect of the moving air on the front and back of the cups. If you are looking for power however the negative effect of the back of the cup moving against the wind is very expensive energy loss. You could design a type of cup that collapses when moving up wind but still you are only capturing power from one cup at a time. You can pretty much bank on the perpendicular design as the best one for capturing power from the wind.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    I have admit I knew some of the arguments against the design but like a little boy hoping that there might have been slightly more plausabilty in the idea

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 11 years ago

    The main reason for the configuration you see in windmill is efficienc. That's the same reason why you don't see anymore the steamboats with the two big wheels: a propropeller is more efficient

    I don't what your aims are, but you could also have a look at windbelts

     

    http://www.tomsguide.com/us/wind-power-ene…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to amgalbu

    Thanks I will have to look into this in more detail

     

    Ok - had a look at this; it is on the principle of an electric guitar string, producing any real power from this looks very limited, but I might be wrong, an in depth look at technology of magnetic and piezo picks would have to be done

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    Done and done:

     

    Savonius wind turbine - Wikipedia, the free encyclopedia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    this may also provide an alternate approach, no need to align with the wind direction

     

    https://www.google.ca/search?q=Vertical+Wind+Turbine+Wind+Generator&es_sm=93&source=lnms&tbm=isch&sa=X&ei=sz3YVJHDKtWgyAS5jILAAw&ved=0CAkQ_AUoAg&biw=2560&bih=1339

     

    hey may even be more efficient but im not 100% sure

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Robert Peter Oakes

    Peter's vertical wind turbines have been used.

    I believe there are a few issues with speed regulation, since most cannot feather the blades, or turn out of the wind.

    (Interstingly the old fashion windmill for pumping water with the tail ... the tail pulled it out of the wind to stop it going too fast)

     

    From what I read windmills are designed to slow the wind, and since energy isn't lost, the resultant is transferred into the blades to turn the turbine/gearbox.

    It's easy to design windmills to function in high winds, but getting them to run in the lower winds that typically are present is the big problem.

     

    Vibrations from air being compressed between the blade and support pole are a problem, and in NZ we have a new design using only two blades to try counter that effect.

    http://www.nzwindfarms.co.nz/

     

     

    I applaude your choice of entering into Engineering, but the science of windmills is a really big first step to be taking.

    Having said that the option for very small lightweight units for domestic application 500-1000w (rather than solar) is worthy.

    There are many for nautical applications but require manual intervention in high winds, and unlike solar where they are happy to be open circuit if the battery is charged, windmills need a load to stop them overspeeding and flying apart.

     

    Good luck

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    I can remember a bit from the vibrations unit I did in my degree (in the mid 80's) but this was mainly aimed at electronic/motor theory, I would have thought by having 3 blades would have resulted in less vibration on the blade bearings; I know on the Island of Eigg in Scotland, they have to regularly tighten the base bolts

     

    It has proved to be an interesting start to a conversation that has proved some of my theories and destroyed others. I will continue the thoughts of small power generation, but also have to look into the small scale storage and at low cost

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>