STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum Project Ideas Needed: Environmental Science with Arduino or Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 58 subscribers
  • Views 7451 views
  • Users 0 members are here
  • sensing
  • raspberry
  • environment
  • oceanography
  • science
  • weather
  • aquarium
  • arduino
  • stem space
Related

Project Ideas Needed: Environmental Science with Arduino or Raspberry Pi

e14 Contributor
e14 Contributor over 12 years ago

I'm looking for ideas/projects we can design using an Arduino or Raspberry Pi with high school students. My students are participating in Make/Google's Summer Maker Camp and they just sent us a couple of Arduino Unos to build our projects around. Since I'm really new to single-board computers, I'd love to hear from everyone here for ideas..

 

It would be awesome if we could find projects related to:

  • Environmental Science (like the one mentioned in this post)
  • Oceanography
  • Animal Health

We just ordered a couple copies of this book about Environmental Sensing and Ardiuno from MakerShed.com.

image

We think these devices would be great for sensing things in the environment (such as temperature, pressure, water quality, etc.), but we are also looking for ways to output that data.

 

If anyone has links, suggestions or even just wants to brainstorm ideas for how an Arduino or Raspberry Pi might be used at an aquarium (I work at Shedd Aquarium in Chicago), then let me know!

 

 

 

 

Re: Ideas for using the Raspberry Pi in the classroom

  • Sign in to reply
  • Cancel

Top Replies

  • mikedavis
    mikedavis over 12 years ago +1 suggested
    Hey Wade. I am Mike Davis, and I work with the City Colleges of Chicago. I think you guys have a golden opportunity to do some fun things. One thing I'd recommend is making use of gspread. It is something…
  • gadget.iom
    gadget.iom over 11 years ago in reply to nbizzell +1
    That's an awesome project! Hamsters can cover some milage.
  • DAB
    DAB over 11 years ago +1
    One of the best ways to begin looking at issues in the environment is to measure and record the parameters in your local area. The Arduino provides a great way to set up sensors for data logging over a…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    I'm an agnostic on environmentalism.  People shouldn't make messes, sure.  But my deepening paranoia leads me to suspect that it has propaganda value, blaming the many for the decisions of the few.  My kids, however have sipped from the urn of this particular cool-aid. 

     

    My older son's grad work had some sponsorship by the EPA.  The plan was to develop a cheap an rugged-ized GCMS with a little sampler an radio set.  The original plan was to sample all of the rivers in the US in real time and relay anomalies to satellites.  An automatic system was to be set up to contact local law enforcement to nail dumpers in the act.  Funding was withdrawn.  Wars ain't cheap.  Now he helps with earthquake preparedness as an RF proposition in his free time.  He works to develop and maintain and fund-raise for and train people to operate analog and digital HF rigs (and get the feds to plan to listen) to use if/when cell phone fails in a public crisis and the protocols around their allocation. 

     

    My younger son is conducting some research with public and private money in his free time.  He works on and researches strains of fungus that eat petroleum that has been released to the environment unintentionally.  His specialties are probability theory and computer database.  His goal is to vet these organisms in vivo/vitro at different temperatures, humidities and salinity levels, molecular weights/types of sample, et c.so that appropriate samples can be stored pre-need at vulnerable sites, ready for deployment by local personnel.  He wants to grow some of it in calorimeters with measured amounts of input to gauge thermodynamic efficiency of his various strains versus nutrient and load.  An aerobic calorimeter seems to be no mean feat!  Basically, though, the technique works in that he can demonstrate the ability to remove motor oil (and most organics, AFIK) from things like straw and dirt more cheaply and thoroughly than mechanical or chemical methods.

     

    I live in an area that is strictly residential for miles and miles around embedded in a matrix of exclusively industrial farming.  If I lived in a town that had some sort of hazardous facility, monitoring it from the outside might be interesting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    I'm an agnostic on environmentalism.  People shouldn't make messes, sure.  But my deepening paranoia leads me to suspect that it has propaganda value, blaming the many for the decisions of the few.  My kids, however have sipped from the urn of this particular cool-aid. 

     

    My older son's grad work had some sponsorship by the EPA.  The plan was to develop a cheap an rugged-ized GCMS with a little sampler an radio set.  The original plan was to sample all of the rivers in the US in real time and relay anomalies to satellites.  An automatic system was to be set up to contact local law enforcement to nail dumpers in the act.  Funding was withdrawn.  Wars ain't cheap.  Now he helps with earthquake preparedness as an RF proposition in his free time.  He works to develop and maintain and fund-raise for and train people to operate analog and digital HF rigs (and get the feds to plan to listen) to use if/when cell phone fails in a public crisis and the protocols around their allocation. 

     

    My younger son is conducting some research with public and private money in his free time.  He works on and researches strains of fungus that eat petroleum that has been released to the environment unintentionally.  His specialties are probability theory and computer database.  His goal is to vet these organisms in vivo/vitro at different temperatures, humidities and salinity levels, molecular weights/types of sample, et c.so that appropriate samples can be stored pre-need at vulnerable sites, ready for deployment by local personnel.  He wants to grow some of it in calorimeters with measured amounts of input to gauge thermodynamic efficiency of his various strains versus nutrient and load.  An aerobic calorimeter seems to be no mean feat!  Basically, though, the technique works in that he can demonstrate the ability to remove motor oil (and most organics, AFIK) from things like straw and dirt more cheaply and thoroughly than mechanical or chemical methods.

     

    I live in an area that is strictly residential for miles and miles around embedded in a matrix of exclusively industrial farming.  If I lived in a town that had some sort of hazardous facility, monitoring it from the outside might be interesting.