STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum Project Ideas Needed: Environmental Science with Arduino or Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 58 subscribers
  • Views 7457 views
  • Users 0 members are here
  • sensing
  • raspberry
  • environment
  • oceanography
  • science
  • weather
  • aquarium
  • arduino
  • stem space
Related

Project Ideas Needed: Environmental Science with Arduino or Raspberry Pi

e14 Contributor
e14 Contributor over 12 years ago

I'm looking for ideas/projects we can design using an Arduino or Raspberry Pi with high school students. My students are participating in Make/Google's Summer Maker Camp and they just sent us a couple of Arduino Unos to build our projects around. Since I'm really new to single-board computers, I'd love to hear from everyone here for ideas..

 

It would be awesome if we could find projects related to:

  • Environmental Science (like the one mentioned in this post)
  • Oceanography
  • Animal Health

We just ordered a couple copies of this book about Environmental Sensing and Ardiuno from MakerShed.com.

image

We think these devices would be great for sensing things in the environment (such as temperature, pressure, water quality, etc.), but we are also looking for ways to output that data.

 

If anyone has links, suggestions or even just wants to brainstorm ideas for how an Arduino or Raspberry Pi might be used at an aquarium (I work at Shedd Aquarium in Chicago), then let me know!

 

 

 

 

Re: Ideas for using the Raspberry Pi in the classroom

  • Sign in to reply
  • Cancel

Top Replies

  • mikedavis
    mikedavis over 12 years ago +1 suggested
    Hey Wade. I am Mike Davis, and I work with the City Colleges of Chicago. I think you guys have a golden opportunity to do some fun things. One thing I'd recommend is making use of gspread. It is something…
  • gadget.iom
    gadget.iom over 11 years ago in reply to nbizzell +1
    That's an awesome project! Hamsters can cover some milage.
  • DAB
    DAB over 11 years ago +1
    One of the best ways to begin looking at issues in the environment is to measure and record the parameters in your local area. The Arduino provides a great way to set up sensors for data logging over a…
  • D_Hersey
    0 D_Hersey over 11 years ago

    I'm an agnostic on environmentalism.  People shouldn't make messes, sure.  But my deepening paranoia leads me to suspect that it has propaganda value, blaming the many for the decisions of the few.  My kids, however have sipped from the urn of this particular cool-aid. 

     

    My older son's grad work had some sponsorship by the EPA.  The plan was to develop a cheap an rugged-ized GCMS with a little sampler an radio set.  The original plan was to sample all of the rivers in the US in real time and relay anomalies to satellites.  An automatic system was to be set up to contact local law enforcement to nail dumpers in the act.  Funding was withdrawn.  Wars ain't cheap.  Now he helps with earthquake preparedness as an RF proposition in his free time.  He works to develop and maintain and fund-raise for and train people to operate analog and digital HF rigs (and get the feds to plan to listen) to use if/when cell phone fails in a public crisis and the protocols around their allocation. 

     

    My younger son is conducting some research with public and private money in his free time.  He works on and researches strains of fungus that eat petroleum that has been released to the environment unintentionally.  His specialties are probability theory and computer database.  His goal is to vet these organisms in vivo/vitro at different temperatures, humidities and salinity levels, molecular weights/types of sample, et c.so that appropriate samples can be stored pre-need at vulnerable sites, ready for deployment by local personnel.  He wants to grow some of it in calorimeters with measured amounts of input to gauge thermodynamic efficiency of his various strains versus nutrient and load.  An aerobic calorimeter seems to be no mean feat!  Basically, though, the technique works in that he can demonstrate the ability to remove motor oil (and most organics, AFIK) from things like straw and dirt more cheaply and thoroughly than mechanical or chemical methods.

     

    I live in an area that is strictly residential for miles and miles around embedded in a matrix of exclusively industrial farming.  If I lived in a town that had some sort of hazardous facility, monitoring it from the outside might be interesting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Capper
    0 Capper over 11 years ago

    Hi Wade,

    Since camps are short, and High School kids are not normally experienced embedded programmers, you may want to break up into two groups, one to set up a Linux LAMP HTML server using the Raspberry PI, and another reading various sensors from the Arduinos.  The Raspberry Pi org and The MagPi magazine along with this site and https://www.sparkfun.com/ can give you hundreds of project ideas.

    Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks to everyone for their input, we will definitely be looking into some of these resources for the coming year. Recently, we have been working on something a bit different in addition to the sensors. We have a team of students who are building an ROV (remotely operated vehicle) who are looking to expand their control of the vehicle's motors via an arduino. We have begun to explore this control and have made significant progress, but aren't completely there yet and would love any additional input or resources.  We'll also be looking into adding some sensors to the vehicle at some point!

     

    Current state of progress:

     

    We have played around with using a Sabertooth motor driver along with the Arduino to control the motors, using a small joystick button for the control. We have successfully gotten one motor to run with the controls correctly using this set up, but have run into some trouble coding the second motor commands to run simultaneously using the same control boards. 

     

    We also ran into a technical problem after some time with the computer- something along the lines of "unplug the USB device that is drawing too much power" and were unable to reconnect our Arduino via USB to that particular computer after that notification popped up. Any input on this issue would also be great- we are unsure if it will be a recurring problem, but definitely don't want to keep getting stuck while building if it does continue to happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    it sounds like your powering the motors from the USB as well as the controller, this is a bad idea

     

    Power the motors separately to ensure you don't overload the USB or the Controller supply

    this should eliminate the message your getting

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to Robert Peter Oakes

    Also

    Check the motor controller board for the minimum voltage.

    Sometimes its 7.5 or 9v.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<