microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog BBC micro:bit - Submit your Big Ideas
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 14 Jun 2016 4:23 PM Date Created
  • Views 7537 views
  • Likes 13 likes
  • Comments 47 comments
  • bit
  • micro:bit
  • bbc micro:bit
  • bbc
  • microbit
  • big ideas
  • ten bbc micro:bit projects
Related
Recommended

BBC micro:bit - Submit your Big Ideas

jlucas
jlucas
14 Jun 2016

image

 

Introduction

 

Our 10 BBC micro:bit Projects in 10 Days series introduced the incredible creative potential of this unique pocket sized computer system. But we've really only scratched the surface. Now we want to hear your ideas.

 

The BBC micro:bit is currently only available for sale in the UK through Farnell element14, CPC and our approved re-sellers, but we've managed to secure ten devices to give away to members of our global community.

How to Enter

 

For your chance to get hold of one of these sought-after devices, simply read our 10 BBC micro:bit Projects in 10 Days series and 'like' your two favourite projects to earn the BBC micro:bit badge. Then, leave a comment under this blog telling us about a project you'd like to try out using the BBC micro:bit.

 

The ten participants who submit the best, most creative project ideas will each receive a BBC micro:bit and will be invited to write about their project here on element14.

 

Submissions are open until 23:59 (BST) on Sunday 31st July 2016. Full terms and conditions can be in the attached PDF.

 

To find out more about the BBC micro:bit initiative and the unique functionality of the device, visit the official BBC micro:bit website or read our exclusive interview with Premier Farnell's Strategic Alliance Director Richard Curtin.

Attachments:
image10 BBC microbit projects in 10 days Terms Conditions.pdf
  • Sign in to reply

Top Comments

  • jlucas
    jlucas over 10 years ago +7
    Thanks for all of your submissions guys, some really excellent project ideas here. I'm happy to announce that the following ten members have been selected to receive a BBC micro:bit device to undertake…
  • dougw
    dougw over 10 years ago +5
    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends…
  • jlucas
    jlucas over 10 years ago +4
    Apologies for the delay guys. We had some shipping issues but these are now resolved and we'll be sending them out this week. Looking forward to seeing all of your projects.
Parents
  • dougw
    dougw over 10 years ago

    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends will reach further than even the optimistic expectations for the program. The features of the micro:bit have been carefully designed to include as much technology as possible for the lowest possible cost. This has resulted in a very impressive module, but there were necessary compromises that had to exclude more expensive displays and user interfaces.

    My big idea is to expand the micro:bit user interface to include a graphical LCD and keypad at the lowest possible cost.

    To do this I would use a Nokia 5110 LCD, which is an extremely low cost and popular display. It has an SPI interface which is also used by some larger LCDs, so expanding to even better displays is not  a huge leap from this low cost starting point.

    For the keypad, I would use a I2C capacitive keypad to eliminate the cost of a whole matrix of electro-mechanical switches.

    I have been avidly following micro:bit documentation as it becomes available and have already designed and printed a small PCB that implements this SPI LCD interface as well as an I2C interface for the keypad.

    It also has 3 analogue sensor connectors and a power switch for the micro:bit.

    I would also 3D print a case to make a complete hand-held computer.

    I am very much looking forward to testing this card out and showing how to implement a low cost user interface for the micro:bit.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to dougw

    That sounds like it could be an enabler for a whole range of interesting projects and activities.

     

    Not sure if it exists or not yet for the micro:bit but what might be quite good is something along the lines of the Pico Technology list of educational science projects/ideas

    https://www.picotech.com/library/experiments

    to try and get young people to start interacting with their wider environment. Project ideas from a wide range of subject areas that both can be done in the classroom as well as at home.

     

    Perhaps one of the interesting things about the micro:bit is that for once there is a captive audience that all have access to the same platform.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 10 years ago in reply to dougw

    That sounds like it could be an enabler for a whole range of interesting projects and activities.

     

    Not sure if it exists or not yet for the micro:bit but what might be quite good is something along the lines of the Pico Technology list of educational science projects/ideas

    https://www.picotech.com/library/experiments

    to try and get young people to start interacting with their wider environment. Project ideas from a wide range of subject areas that both can be done in the classroom as well as at home.

     

    Perhaps one of the interesting things about the micro:bit is that for once there is a captive audience that all have access to the same platform.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 10 years ago in reply to beacon_dave

    Does anyone know if they still use ticker tape timers in school physics experiments for measuring acceleration ?

     

    If so, just pondering if this could be modernised slightly with the likes of the micro:bit. Either by using the built-in accelerometer, however that may not be so clever when dropping weights, so alternatively by using a punched ticker tape with an optical sensor and a micro:bit as a data logger, giving near real-time analysis of that data without the need for the rather tedious measuring of dots and manually plotting graphs. The 'timer mechanics' could be a simple plug-on shield to the micro:bit containing a photodiode a couple of tape guides and even use the micro:bit's built in LED's as the light source. Might need to mount it on a weighted base to prevent it from flying off the table though.

     

    The likes of Douglas's LCD display idea could provide access to the data or alternatively it could be transferred to the teacher and displayed on a large screen.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to beacon_dave

    Phototransistor would be simpler than a diode. If there are pull-ups on the board you might even get away with just the transistor.

     

    Another way to modernise it would be to flash the LEDs 10 times a second and take a long-exposure photograph of the micro:bit falling whilst attached to a weight.

     

    The combination of accelerometer and Bluetooth would also allow for very easy analysis of a pendulum (the micro:bit and battery would be the weight). You could then turn it into a clock and even use the position information that you'd derived to do a persistence-of-vision style display.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to jc2048

    I have to say, I think the micro:bit is a game-changer, not just for technology classes, but for physics lab experiments too. It is a measurement tool in a pocket. Data logger, rich in sensors, wireless, and easily expandable. Incredible combination.

    I tried using it as a voltmeter when I had a few minutes spare, but rather than displaying the values on the screen or even using Bluetooth, there was a quick option, just make it beep a tone that depended on the input voltage. Basically nothing was needed except a pair of earphones, which everyone has, or could be purchased for sub-£1 for classes. Apparently speech API could be available at some point too, since the on-board processor has more than enough power for this.

    Possibly the micro:bit design could serve schoolkids well for many years to come due to its flexibility. Maybe it is like a swiss army knife for education.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to shabaz

    The likes of data logging in science labs is what I was thinking about as well. Back in the days of the BBC micro, there was one Physics teacher at my school who unleashed the BBC micro into some of his Physics experiments, so we had a side-by-side comparison of the results both doing it by hand and then doing it with the microcomputer. This had 'wow factor' as this was probably the first time that most schoolkids had seen a microcomputer interfaced to the real world as opposed to just being used for games at home. Back then it was one microcomputer for the whole of the sciences, however if done right with the micro:bit, then there is potential for one or more micro:bits per student and the ability to continue the experiments outside of the classroom.

     

    The user interface perhaps currently holds it back a bit but Douglas sounds as if he has a plan for that and speech API's could potentially change everything. The universal 'measurement tool in a pocket' concept is right on the mark but it perhaps needs a low cost enclosure with a user interface to help make this happen.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to beacon_dave

    Not really! With sound, I plan on playing music and flash LED's. Hope it is eerie enough. LOL

    Clem