microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog BBC micro:bit - Submit your Big Ideas
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 14 Jun 2016 4:23 PM Date Created
  • Views 7574 views
  • Likes 13 likes
  • Comments 47 comments
  • bit
  • micro:bit
  • bbc micro:bit
  • bbc
  • microbit
  • big ideas
  • ten bbc micro:bit projects
Related
Recommended

BBC micro:bit - Submit your Big Ideas

jlucas
jlucas
14 Jun 2016

image

 

Introduction

 

Our 10 BBC micro:bit Projects in 10 Days series introduced the incredible creative potential of this unique pocket sized computer system. But we've really only scratched the surface. Now we want to hear your ideas.

 

The BBC micro:bit is currently only available for sale in the UK through Farnell element14, CPC and our approved re-sellers, but we've managed to secure ten devices to give away to members of our global community.

How to Enter

 

For your chance to get hold of one of these sought-after devices, simply read our 10 BBC micro:bit Projects in 10 Days series and 'like' your two favourite projects to earn the BBC micro:bit badge. Then, leave a comment under this blog telling us about a project you'd like to try out using the BBC micro:bit.

 

The ten participants who submit the best, most creative project ideas will each receive a BBC micro:bit and will be invited to write about their project here on element14.

 

Submissions are open until 23:59 (BST) on Sunday 31st July 2016. Full terms and conditions can be in the attached PDF.

 

To find out more about the BBC micro:bit initiative and the unique functionality of the device, visit the official BBC micro:bit website or read our exclusive interview with Premier Farnell's Strategic Alliance Director Richard Curtin.

Attachments:
image10 BBC microbit projects in 10 days Terms Conditions.pdf
  • Sign in to reply

Top Comments

  • jlucas
    jlucas over 10 years ago +7
    Thanks for all of your submissions guys, some really excellent project ideas here. I'm happy to announce that the following ten members have been selected to receive a BBC micro:bit device to undertake…
  • dougw
    dougw over 10 years ago +5
    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends…
  • jlucas
    jlucas over 10 years ago +4
    Apologies for the delay guys. We had some shipping issues but these are now resolved and we'll be sending them out this week. Looking forward to seeing all of your projects.
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello, my idea is to create an watchdog for blind people or for people who have low vision.

     

    All this can be achieved thanks to the small size of the micro bit and:

     

    1. An array of infrared sensors 8 × 8 which serves to make a recognition of the person
    2. Ultrasonic sensor for the detection of possible obstacles and of the relative distance
    3. bluetooth module with the ability to interact via a cell so that if the person needs assistance have to press a button or connect to the voice recognition and sends its GPS coordinates to a fixed number, this advantage of the GPS module of the mobile
    4. pressure sensor to detect the heartbeat and possibly monitor it via your mobile phone
    5. conductive liquid sensor, this sensor provides the ability to tell if the visually impaired person is walking on a slippery surface and then take precautions

        3 motors for vibration

        a battery power supply

     

    Possible additions are 2:

     

    • integrate it to the glasses, all the sensors on the front of the eyeglasses in such a way that the micro can process the information in a specific direction and insert the 3 moped vibration on the lateral slats, this is because the type of vibration the person understands if it has a simple obstacle in front, or a slippery surface, or a person
    • The second alternative is to integrate it with a stick, this to ensure that we exploit the stick support to proactively report the presence of slippery surfaces and, if desired, you can use a combination of accelerometer, gyroscope and ultrasound sensor to understand if in the next few centimeters, there it will a step, and also because the stick can be integrated flexible photovoltaic panels to extend the life of the device.

     

    I thought to be able to integrate the stick also for a possible energy recovery through a piezoelectric placed under the stick, in such a way that every time the stick is placed on the ground there is a quantity of energy recovered.

     

     

     

    I hope I have explained to outline my idea and that it is of interest

     

    Good day

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello, my idea is to create an watchdog for blind people or for people who have low vision.

     

    All this can be achieved thanks to the small size of the micro bit and:

     

    1. An array of infrared sensors 8 × 8 which serves to make a recognition of the person
    2. Ultrasonic sensor for the detection of possible obstacles and of the relative distance
    3. bluetooth module with the ability to interact via a cell so that if the person needs assistance have to press a button or connect to the voice recognition and sends its GPS coordinates to a fixed number, this advantage of the GPS module of the mobile
    4. pressure sensor to detect the heartbeat and possibly monitor it via your mobile phone
    5. conductive liquid sensor, this sensor provides the ability to tell if the visually impaired person is walking on a slippery surface and then take precautions

        3 motors for vibration

        a battery power supply

     

    Possible additions are 2:

     

    • integrate it to the glasses, all the sensors on the front of the eyeglasses in such a way that the micro can process the information in a specific direction and insert the 3 moped vibration on the lateral slats, this is because the type of vibration the person understands if it has a simple obstacle in front, or a slippery surface, or a person
    • The second alternative is to integrate it with a stick, this to ensure that we exploit the stick support to proactively report the presence of slippery surfaces and, if desired, you can use a combination of accelerometer, gyroscope and ultrasound sensor to understand if in the next few centimeters, there it will a step, and also because the stick can be integrated flexible photovoltaic panels to extend the life of the device.

     

    I thought to be able to integrate the stick also for a possible energy recovery through a piezoelectric placed under the stick, in such a way that every time the stick is placed on the ground there is a quantity of energy recovered.

     

     

     

    I hope I have explained to outline my idea and that it is of interest

     

    Good day