microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog First Workshop with the Micro:bits from the "Micro:bit Summer Code Club Challenge
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gusmerckel
  • Date Created: 4 Jul 2019 7:17 PM Date Created
  • Views 2612 views
  • Likes 13 likes
  • Comments 8 comments
  • maker
  • micro:bit
  • education
  • summer code club challenge
  • water
  • beginner micro:bit projects
  • summer_code_club
  • mexico
  • steam
  • makered
  • beginner_microbit_projects
  • stem projects
  • oaxaca
  • ed
  • mixteca
Related
Recommended

First Workshop with the Micro:bits from the "Micro:bit Summer Code Club Challenge

gusmerckel
gusmerckel
4 Jul 2019

Aguaforence, analyzing water using art and technology:

 

The micro:bits finally arrived in our office in Mexico City. While we waited for the kitronics kit, we had an idea to do a project in the mexican mixteca, a region with beatiful landscapes but also with a lot of challenge.

 

For the last year we have been working in a community called Tamazulapam, very famous for it's river and clean water. In the community we work with 25 students,14-16 years old, in differente maker projects and english classes.

 

Inspired by the serbian artist Robertina Sebjanic and her project Aqua_forensic, we embarqued in an adventure to answer if the famous river was actually clean.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

So with the micro:bit, we created 3 experiments to asses the water quality:

  1. A thermometer to meassure the water temperature, as this could be an indicator for life in the river but also could help us detect if a company is throwing hot process water into the river. In the photo we see one student, dipping the microbit in a plastic bag inside of the a part of the river to meassure temperature.image
  2. A turbidity sensor using the lightsensor of the microbit, as a tool to meassure the PPM suspended in water.

image

 

3. A conductivity sensor to meassure the salt and mineral content in water.

image

In order to control this meassurements, we also used a professional 5 in 1 meter, a PHT-026, which could also meassure pH of each sample image

 

The students where particularly surprised that in 3 days, without a deeper knowledge in micro:bit besides writing their names on the LED Matrix, they could create tools that allowe them to asses the water quality and also do citizen science.

 

The results where very conforting, all the levels where compared with a study made by the mexican environmental agency a while ago and they were similar, so there hasnt been an pollutants coming the the river.

 

 

 

{gallery} River Checking

image

Using the "Baby legs": catch microplastics suspended in the water.

image

Waterfall group on field trip: Measuring water inside the canyon's waterfall.

image

Learning: programming

image

First steps: with micro:bit



We are still working on a video and the results of this programm, as we finished this intensive workshop yesterday, but I'm still super excited about the reaction of the students and the potential of this project,

 

Join The micro:bit Summer Code Club Challenge!

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +4
    This is the sort of science I wish I had done when I was at school. Dubbie
  • jlucas
    jlucas over 7 years ago +4
    Wonderful! Very inspiring - can't wait to see what you guys do next.
  • carlitos71
    carlitos71 over 7 years ago +4
    Great project, very inspirational! It would be great to find out more how you used the microbit to measure temperature, turbidity and conductivity, as we'd like to do similar measurements for a project…
  • mp2100
    mp2100 over 7 years ago

    Great use of the microbit sensors.  Good science can be done simply.  Beautiful photos.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago

    Great practical application of the microbit.  I especially like that you taught your students to verify their results against a reference standard.  Good training!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    What a great idea, learning about micro:bit and the ecosystem at the same time.  The future is bleak without educated children and without the vital natural resources that we need to live.

    Well done!

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<