microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
microbit Forum Neopixels & micro:bit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 52 subscribers
  • Views 3088 views
  • Users 0 members are here
  • micro:bit
  • beginner micro:bit projects
  • beginner_microbit_projects
Related

Neopixels & micro:bit

hilalgungor
hilalgungor over 7 years ago

Hi all,

 

I want to use NeoPixel and micro:bit together. But NeoPixels is required 5V and micro:bit provides 3V. Do I damage the micro:bit if i  use them together? I use a regulator to convert 5V and it works properly, but I'm wondering if is there any easy to use module/accessory for Microbit to use it with Neopixel, ultrasonic sensor?

 

Neopixel Ring: https://www.adafruit.com/product/1586

 

Sorry for my english, im not good in english,

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • tonydbeck
    tonydbeck over 7 years ago +3 verified
    Hi Hilal, According to the Adafruit website, the LED's used in the Neopixel rings are the SK6812 type. On page 4 of the data sheet it shows that the VDD supply voltage should be 5.2V. It does not seem…
  • stevesmythe
    stevesmythe over 7 years ago +3 suggested
    You should be safe if there are no more than eight neopixels lit at the same time or, as Tony says, you keep the brightness down. I have not had a problem. You might find, if you are powering the micro…
  • hilalgungor
    hilalgungor over 7 years ago in reply to tonydbeck +1 suggested
    Thank you so much for quick reply and all the explanations!
Parents
  • stevesmythe
    0 stevesmythe over 7 years ago

    You should be safe if there are no more than eight neopixels lit at the same time or, as Tony says, you keep the brightness down. I have not had a problem. You might find, if you are powering the micro:bit and neopixels from a USB socket, that effects like rainbows do not display correctly. I have never damaged a micro:bit if I follow the above guidelines.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • stevesmythe
    0 stevesmythe over 7 years ago

    You should be safe if there are no more than eight neopixels lit at the same time or, as Tony says, you keep the brightness down. I have not had a problem. You might find, if you are powering the micro:bit and neopixels from a USB socket, that effects like rainbows do not display correctly. I have never damaged a micro:bit if I follow the above guidelines.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer