microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
microbit Forum Genuine decimal numbers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 50 subscribers
  • Views 3254 views
  • Users 0 members are here
  • micro:bit
  • bbc micro:bit
  • microbit
  • bbc_microbit
  • micro bit
  • bbc microbit
  • microbit.
  • microbit bbc
Related

Genuine decimal numbers

rhubarbdog
rhubarbdog over 3 years ago

if floating point numbers are letting you down because of the gaps and rounding errors try my decimal numbers class decimal.py at https://github.com/rhubarbdog/decimal-numbers . There is a version for microbit called microbit.py follow the instructions in the README.md.
See example code decimal_math.py and pi.py for python 3 and other boards and for microbit it's microbit_pi.py microbit_root.py

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago in reply to rhubarbdog +2
    Hi, Most of us won't have a Micro:bit ready to test this immediately, so this is why I'd hoped for some example output. Sure, we could use the normal Python version instead of the Micropython version…
  • javagoza
    javagoza over 3 years ago +1
    Can you define precision and scale? Are precision and scale inferred by the constructors?
  • michaelkellett
    michaelkellett over 3 years ago +1
    I just looked at your code on Github (with a view to answering Shabaz's questions) You obviously want to share, which is great, but your code does not make it easy. decimal.py is 945 lines of code…
Parents
  • shabaz
    shabaz over 3 years ago

    Hi,

    It may be worth pasting in some output from an example or two on this discussion post, just to show the difference, so people can more easily understand the benefits.

    For instance, an error without the class, and the difference with it. I appreciate people could run the example code, but that entails them making the effort, and some people will not, unless they see some example output.

    A minor point (perhaps worth it for a later code revision) could be to change the name of it, because decimal.py already exists for normal Python, and it may get confusing for people if they expect it to be the same (or similar) thing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    Hi,

    It may be worth pasting in some output from an example or two on this discussion post, just to show the difference, so people can more easily understand the benefits.

    For instance, an error without the class, and the difference with it. I appreciate people could run the example code, but that entails them making the effort, and some people will not, unless they see some example output.

    A minor point (perhaps worth it for a later code revision) could be to change the name of it, because decimal.py already exists for normal Python, and it may get confusing for people if they expect it to be the same (or similar) thing.