microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
microbit Forum Some garbled serial comms from Micro:bit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 49 subscribers
  • Views 3511 views
  • Users 0 members are here
Related

Some garbled serial comms from Micro:bit

pmulvey
pmulvey over 2 years ago

My Serial writes are garbled when sent out to TeraTerm terminal program but Ok when viewed on the Serial monitor. Characters get dropped. This is quite useless as I want my class to receive the data in Python on the PC. I get this in both micro:bit Python editor and MS Makecode. I have used different micro:bits on different PCs, same result.

I tried Mu Editor and the micro:bit sends data across the serial port perfectly. I'm using V2. Is there an issue with the firmware used by MS Makecode and micro:bit Python editor?

I wrote a short Python program to read the serial port on the PC and I get the same results as with TeraTerm i.e. dropped characters, about 10% only, no major garbling.

 

  • Sign in to reply
  • Cancel

Top Replies

  • pmulvey
    pmulvey over 2 years ago +4 suggested
    Finally an answer: Thanks for contacting the Micro:bit Educational Foundation. When a WebUSB connection is used to send a program directly to micro:bit, MakeCode and the Python Editor stay connected…
  • Gough Lui
    Gough Lui over 2 years ago +2
    Are you sure you are matching the correct baud-rate, parity, bit-length and stop-bits? This needs to match what is used by the program running on the Micro:bit and should match whatever serial monitor…
  • pmulvey
    pmulvey over 2 years ago in reply to Gough Lui +1
    Later I will prepare a full report of what is happening and put code up here etc.
Parents
  • pmulvey
    0 pmulvey over 2 years ago
    Finally an answer:
    Thanks for contacting the Micro:bit Educational Foundation.
    When a WebUSB connection is used to send a program directly to micro:bit, MakeCode and the Python Editor stay connected and ready for incoming serial data.
    With a serial terminal program connected, for some reason an occasional character still finds it's way to WebUSB.
    ​
    Use the three dots menu on the Download/send to micro:bit button to Disconnect, or close the WebUSB connected browser tab.
    ​
    I have found this easy to forget. It's taken a while, but I finally now do think "shut MakeCode" when serial is misbehaving!
    For the same reason, having more than one tab with MakeCode or the Python Editor open can lead to errors.
    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • pmulvey
    0 pmulvey over 2 years ago
    Finally an answer:
    Thanks for contacting the Micro:bit Educational Foundation.
    When a WebUSB connection is used to send a program directly to micro:bit, MakeCode and the Python Editor stay connected and ready for incoming serial data.
    With a serial terminal program connected, for some reason an occasional character still finds it's way to WebUSB.
    ​
    Use the three dots menu on the Download/send to micro:bit button to Disconnect, or close the WebUSB connected browser tab.
    ​
    I have found this easy to forget. It's taken a while, but I finally now do think "shut MakeCode" when serial is misbehaving!
    For the same reason, having more than one tab with MakeCode or the Python Editor open can lead to errors.
    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • baldengineer
    0 baldengineer over 2 years ago in reply to pmulvey

    That's a really good tip (and one I would have never thought of!)

    Thanks for sharing your finding.