microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
microbit Forum Are ARM Cortex M0 peripherals standard across manufacturers?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 49 subscribers
  • Views 2369 views
  • Users 0 members are here
Related

Are ARM Cortex M0 peripherals standard across manufacturers?

jc2048
jc2048 over 10 years ago

The BLE chip on the micro:bit seems to be an ARM Cortex M0 but the datasheet looks very sketchy on the peripheral detail.

 

I don't know anything about ARM chips. Are the internal peripherals (timers, I2C, UARTs and so on) standard and defined by ARM or are they added by the particular chip manufacturer who has licenced the core design? If they're standard, what's my best route to learning about them?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago +1
    They are NOT standard - the NVIC controller and the system timer (only good for making a regular interrupt) are ARM standard but the other stuff is all manufacturer specific. I think it's the Nordic processor…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to michaelkellett +1
    This is the closest to a Ref Manual that I could find for that controller family: http://infocenter.nordicsemi.com/pdf/nRF51_RM_v3.0.pdf
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    They are NOT standard - the NVIC controller and the system timer (only good for making a regular interrupt) are ARM standard but the other stuff is all manufacturer specific.

     

    I think it's the Nordic processor that is connected to the IO pins (can't be sure without making more effort since there is no easy to find MicroBit schematic on the web - perhaps someone knows where there is one.).

     

    There is quite a bit of information on the Nordic website but its certainly at nothing like the level of detail that Atmel, Microchip, ST or TI (to name a few) offer. Shame on you Nordic - I hope you are listening !!

     

    Did you find the 1.5Mbyte "Reference Manual" ?

    You will need to work quite hard at getting these peripherals to do useful stuff.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 10 years ago

    They are NOT standard - the NVIC controller and the system timer (only good for making a regular interrupt) are ARM standard but the other stuff is all manufacturer specific.

     

    I think it's the Nordic processor that is connected to the IO pins (can't be sure without making more effort since there is no easy to find MicroBit schematic on the web - perhaps someone knows where there is one.).

     

    There is quite a bit of information on the Nordic website but its certainly at nothing like the level of detail that Atmel, Microchip, ST or TI (to name a few) offer. Shame on you Nordic - I hope you are listening !!

     

    Did you find the 1.5Mbyte "Reference Manual" ?

    You will need to work quite hard at getting these peripherals to do useful stuff.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to michaelkellett

    Your guess is as good as mine, but I'd think the NXP/Freescale KL26Z  is attached to IO, and the Nordic is the one handling wireless comms.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    no, I'm wrong image

     

     

    TFW the best specs are found on wikipedia:

    NXP/Freescale KL26Z [....] used as a communication interface between USB and main Nordic microcontroller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to michaelkellett

    Thanks. Suspected that would be the answer.

     

    It is the Nordic BLE chip that drives the IO pins. I've only looked at the device datasheet so far and it mysteriously refers to routing the peripherals to any IO pin without saying how to do it. I wanted to see if it could do PWM that could then be routed to the micro:bit edge connector.

     

    I'll dig around and see what else I can find on their site. I should be able to find a whole reference manual if I try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to michaelkellett

    This is the closest to a Ref Manual that I could find for that controller family:

     

    http://infocenter.nordicsemi.com/pdf/nRF51_RM_v3.0.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to Jan Cumps

    Thanks Jan. That looks like it has a fair amount of information about the peripherals and the interconnect.

     

    Next step will be to see if I'm allowed to talk to any of it from the code side. No point in learning how the peripherals work if there's no chance of talking to the registers.