microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
microbit Forum New release of MIT AppInventor supports BBC micro:bit and Arduino101
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 52 subscribers
  • Views 3664 views
  • Users 0 members are here
  • ble
  • bluetooth le
  • micro bit
  • bbc microbit
  • microbit bbc
  • arduino101
Related

New release of MIT AppInventor supports BBC micro:bit and Arduino101

neilk
neilk over 9 years ago

On 21st June 2017, MIT announced the release of a new version of their BLE extensions for AppInventor: iot.appinventor.mit.edu

 

As well as a completely revised set of general BLE functions, the release also includes a specific set of functions for the BBC micro:bit and the Arduino101 in which the Device Specific Service and Characteristic UUIDs are already built into the functions and therefore hidden from the user - so much simpler!

 

I spent a lot of time trying to get the original version of the BLE extension (released last year) to work with the micro:bit - it was tortuous and not everything worked! I was lucky enough to get asked to help beta test the second version and did find a couple of bugs!

 

Virtually everything you might want to do over BLE with the micro:bit is now fully supported (I can't comment on Arduino101 support because I don't have one) - all you need to do is load the the relevant extensions: BLE, Microbit, and Arduino101 into your AppInventor project and off you go.

 

I intend to publish a some tutorials on my blog, if anyone is interested.

 

Neil

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago in reply to notcuvtixo +2
    Hi Chris, Arduino 101 relied on a module from Intel, called Curie. However, it was discontinued by Intel around July of last year (and not many people were notified until it had occurred). The "Arduino…
  • gregconti
    gregconti over 7 years ago +2
    Hi Neil, I am encouraged to read your post. I've a project underway hoping to get an AI2 app to control a Micro:Bit peripheral over BLE. In order to make an 'intelligent' cordless drill - which will hopefully…
  • jlucas
    jlucas over 9 years ago +1
    Great stuff Neil - if you could share the tutorials here we'd love to see and share them.
Parents
  • gregconti
    gregconti over 7 years ago

    Hi Neil,

    I am encouraged to read your post.

    I've a project underway hoping to get an AI2 app to control a Micro:Bit peripheral over BLE.

    In order to make an 'intelligent' cordless drill - which will hopefully save my wrists from RSI !  A hazard for a professional bicycle wheel builder.

    I'm hoping you might help direct my next steps forward...

     

    I've got a basic Android app built using BluetoothLE  extension version 20181124  which finds the Espruino MicroBit successfully and connects.

    The Micro:Bit returns a list of supported services. Six items in the list with hexadecimal names eg    00001800-0000-1000-8000-00805f9b34fb Unknown Service.

    That is as far as i have got at the AI2 end.

     

    At the Micro:Bit end, I need code to toggle an I/O pin after 'n' revolutions of the drill chuck (tcrt5000 optical sensor and edge counting) where 'n' is supplied / updated by the Android app.

    Haven't written it yet but confident I can. I had something similar working on the RasPi as a standalone.

    I'm just a bit lost with the BLE comms

     

    Q.  Is it true that the Bluetooth stack uses up too much memory to co-exist with Python ?

    Thus I'm expecting to use Espruino on the Micro:Bit but I'm more familiar with Python.

     

    Q.  Do i need to get techy with GATT services and characteristics?

     

    regards,

    Greg

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 7 years ago in reply to gregconti

    Hi gregconti  good to hear from you.

     

    I see you are a very new member; out of interest, did you find this thread with a simple search on the internet? The reason I ask is because there have been some discussions here about the "visibility" of our postings.

     

    It sounds like a very interesting project you are working on and I look forward to reading more about it.

     

    I'm not familiar with the Espruino product, but I imagine it will do the job for you - I've only ever used the Microsoft makecode editor - https://makecode.microbit.org/#editor

     

     

     

    As I understand things, there is no way that the Bluetooth stack and micro-python can coexist on the micro:bit - pity!

     

    You shouldn't need to worry about the UUIDs for the BLE services and their corresponding Characteristics. They are nearly all handled (and hidden from you!) in the various micro:bit specific features of BluetoothLE  extension version 20181124 (which is the latest version!):

     

    I assume you've looked here for App Inventor  BLE and micro:bit -  MIT App Inventor + Internet of Things If not, all the documentation is there and there are some very useful examples and tutorials

     

    The message "00001800-0000-1000-8000-00805f9b34fb Unknown Service" represents the Generic Access Service, which has 3 characteristics: Device Name, Appearance and Peripheral Preferred Connection Parameters. These are not handled by App Inventor extension.

     

    If you want to see the BLE Services which are handled, you need to start them in the micro:bit code - look here for the details:

     

    http://iot.appinventor.mit.edu/#/microbit/microbitintro

     

    So finally, I don't think you will need to get techy with GATT services and characteristics!

     

    I hope this helps

     

    Best wishes - and let us know how you get on by posting a blog image

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • archit.jain
    archit.jain over 7 years ago in reply to neilk

    Hi Neil,

     

    I have been looking around google but could not find answer, posting it here with hope that you could help me.

     

    I have been trying to connect microbit with app inventor for accelerometer services. I could see microbit in app inventor, able to connect it but app is not able to receive any accelerometer data. Error I get is that data is not published by microbit. I have tried to connect microbit with bittysoftware app and it shows accelerometer data so I think microbit is working fine. I tried to print bluetooth message to see if it has received any data, nothing there too.

     

    I am stuck with this problem. Then I tried temperature also but same problem, same with magnetometer.

     

    Summary : Bluetooth device (microbit) is found, app able to connect with microbit BLE but not able to receive any data.

     

    Please suggest / advice.

     

    thanks

    Archit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 7 years ago in reply to archit.jain

    Hi archit.jain. Welcome to element 14 image

     

    I assume that you have started the accelerometer service on the micro:bit......

     

    If you have and you can see that it is active, say,by using nRF connect, then the problem will be in your App Inventor code. If you post this as a new question, I will do my best to help you.

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neilk
    neilk over 7 years ago in reply to archit.jain

    Hi archit.jain. Welcome to element 14 image

     

    I assume that you have started the accelerometer service on the micro:bit......

     

    If you have and you can see that it is active, say,by using nRF connect, then the problem will be in your App Inventor code. If you post this as a new question, I will do my best to help you.

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • archit.jain
    archit.jain over 7 years ago in reply to neilk

    Thanks Neil. I have started accelerometer services. I will use nRF and re-check. Thanks again. I will post the outcome and queries as a new question.

     

    Regards

    Archit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • archit.jain
    archit.jain over 7 years ago in reply to archit.jain

    Hi Neil, I have started new post but could not figure out how to tag you there. Appreciate if you can help.

    https://www.element14.com/community/message/276199/l/microbit-not-able-to-start-accelerometer-services#276199