Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Forum What impact does length of the leads have on an LED.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 4 answers
  • Subscribers 216 subscribers
  • Views 3605 views
  • Users 0 members are here
Related

What impact does length of the leads have on an LED.

burtamus
burtamus over 7 years ago

What impact does length of the leads have on an LED. I'm working with a live multi-camera system and want to send two LED's to a remote camera operator (Tally Lights). Yellow for "On Preview" and one red for "On Air". I was thinking of using Cat5 cable at varying lengths. Three leads in total (1 ground and the two +). What do I need to consider?

 

Sorry i this is in the wrong location. I'm not sure where it would go.

 

TIA, Burt

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +5 suggested
    Frank is right. Cat5 usually uses 24 gauge wire which is about 26 ohms per 1000 feet. If you are using anything over 200 ohms as a current limiting resistor for your LEDs, the apparent brightness difference…
  • fmilburn
    fmilburn over 7 years ago +4 suggested
    Hi Burt, You can use Ohm's Law to calculate how well the Cat5 cable would work along the lines of what Luis has described. Determine the resistance in the cable - Wikipedia gives DC loop resistance of…
  • darrelglisson
    darrelglisson over 7 years ago +1 suggested
    The main consideration should be the forward current specification of your selected LEDs. you didn’t mention your available bias supply, but if you monitor the current of each DC supply and adjust it to…
Parents
  • luislabmo
    0 luislabmo over 7 years ago

    Length of the "leads" as you ask probably won't have a direct impact since leads are usually short (few cms), in the other hand distance/length of wire -which is what most likely affect the outcome- definitely has effect on current and voltage. Resistance is directly proportional to length. As the length increases, resistance increases, as a result current decreases. This is known as Voltage Drop.

     

    There is a good reason why length of the wire is limited for certain applications, for example when using Cat5e cable on a network, there is a distance limitation of 100meters because the voltage drop, noise and other factors at a higher distances may have big impact on the quality of the signal. Since you are trying to light some LEDs, the best you can do is to measure the voltage at the end and compensate or you could try to carry a higher voltage, and have a voltage regulator at the end (part of the LED circuit) to produce clean and stable voltage for your LEDs.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 7 years ago

    Length of the "leads" as you ask probably won't have a direct impact since leads are usually short (few cms), in the other hand distance/length of wire -which is what most likely affect the outcome- definitely has effect on current and voltage. Resistance is directly proportional to length. As the length increases, resistance increases, as a result current decreases. This is known as Voltage Drop.

     

    There is a good reason why length of the wire is limited for certain applications, for example when using Cat5e cable on a network, there is a distance limitation of 100meters because the voltage drop, noise and other factors at a higher distances may have big impact on the quality of the signal. Since you are trying to light some LEDs, the best you can do is to measure the voltage at the end and compensate or you could try to carry a higher voltage, and have a voltage regulator at the end (part of the LED circuit) to produce clean and stable voltage for your LEDs.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer