Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Documents How Do You Make The Most of Renewable Energy?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 19 Aug 2022 10:17 PM Date Created
  • Last Updated Last Updated: 27 Nov 2023 4:24 PM
  • Views 21136 views
  • Likes 6 likes
  • Comments 15 comments
Related
Recommended

How Do You Make The Most of Renewable Energy?

Improving Renewable Energy

Renewable energy reduces our dependence on fossil fuels, which helps reduce our carbon footprint. Examples of renewable energy sources include wind and solar. While the technology has come a long way, renewable energy has not yet been able to replace fossil fuels and other traditional energy sources. A great deal of research and development is dedicated towards improving efficiency when generating clean power. Efficiency can be improved at various points, one of which is the power inverter. Inverters convert DC power to AC, typically utilizing power relays for grid interconnection. Relays can often be sources of inefficiency due to the generation of heat. This article discusses inverters, with a focus on power relays, and ways to improve their efficiency in renewable energy applications.

Renewable Energy and Applications

Renewable energy is energy that comes from naturally replenishable processes, such as sunlight, wind, the flow of water, and geothermal heat sources. Figure 1 depicts a block diagram of a solar power generation and management system. A photovoltaic (PV) inverter converts the DC power generated from the solar panels into AC power.

Solar Photovoltaic Power Generation Systems

Figure 1: Solar Photovoltaic Power Generation Systems
Source: Omron

What's the Difference between DC and AC power?

Direct Current (DC) flows in just one direction and at a constant magnitude. Figure 2 depicts graphs of the magnitude of DC versus Alternating Current (AC) voltage with respect to time. Because the electrons flow in only one direction with DC power, its magnitude is represented as a straight line. An example of a DC power source is a battery. A battery continuously transports electrical energy in one direction through a device until the battery energy depletes. Solar panels also produce direct current.

AC vs DC power

Figure 2: AC Power vs. DC Power
Source: ElProCus.com

An Alternating Current (AC) periodically switches its direction at 50/60 Hz, the standard powerline frequency for Europe and Asia/North America).. Because of this movement, the magnitude of Alternating Current appears as a sinusoidal wave, as shown in Figure 2. An example of AC power would be the residential electricity supply. Most electronics run on AC power, converting to DC power internally when necessary.

When it comes to sending energy through long distance transmission lines, AC power has several advantages. With AC power, voltage can be quickly stepped up or down with transformers, allowing a high voltage for transmission that can be stepped down at the end user’s point of supply. A high transmission line voltage allows high power levels to be sent with relatively small currents, leading to less power loss due to resistance in the wires.

How does an Inverter work?

Most devices are designed to use AC power, therefore, the DC power from a battery or solar power generator has to be converted to AC. This is done with an inverter. An inverter quickly switches the direction of a DC input back and forth (50‐60 times per second) to convert DC power to AC power. Mechanical inverters use either an automated switching mechanism or an electric motor to flip and swap the incoming direct current by reversing the contacts. Because this output waveform might be square shaped, filters are used to shape it into a clean, repeating sine wave. Sine waves produce less harmonic distortion than square waves, reducing the risk of damage to sensitive equipment. Items such as printers, scanners, monitors, and audio amplifiers also produce less glitches and electronic noise when powered with a sine wave power source. Additionally, some devices sense the phase or the zero voltage crossing  for applications such as motor control. For this purpose, the voltage from a sine wave has a much smoother rise and fall when compared with a square wave.

There are two types of inverters: true/pure sine wave (PSW) and modified/quasi sine wave (MSW) inverters. True inverters use electronic circuits and toroidal transformers to convert DC into a genuine sine wave, similar to the AC signal that is usually supplied to residences. Modified sine wave inverters are less expensive and produce an output that is more like a "rounded-off" square wave.

Figure 2 illustrates a PV inverter block diagram where an array of PV solar panels is connected with an MPPT (Maximum Power Point Tracking) block. The MPPT is an integrated feature in all grid-tied solar inverters that ensures solar panels are always working at their maximum efficiency, independent of the environmental conditions or the solar intensity. An MPPT is usually controlled by a microcontroller, which samples panel voltage and currents, and then adjusts the duty ratio, or impedance, that is seen by the solar cell. The DC power that is generated from the PV panels is then fed into an inverter for conversion to AC.

PV Inverter Block Diagram

Figure 2: PV Inverter Block Diagram
Source: Omron

Controlling High Power Loads with Relays

High power relays are used with inverters for the switching of high power loads. Relays are switches that use an electrical signal from one circuit to control another circuit that may be operating at a different voltage, for example, using a digital logic circuit operating at 5V to control machinery running at much higher voltages. With inverters, relays perform the switching between high power loads, such as batteries or PV cells. They are also used to safely shut down power grids. Relays, however, are one of the components where power loss can occur, due to factors such as contact resistance.

What is Contact Resistance?

The contacts of a relay are electrically conductive pieces of metal that connect to complete a circuit, allowing current to flow. In theory, closed relay contacts are equivalent to a short circuit, meaning there is zero contact resistance; however, all relay contacts have some amount of resistance. Contact resistance is a combination of several factors: the inherent resistance of the armature, terminals, and contacts, and the boundary resistance where the two contacts meet.

The higher the contact resistance is, the more heat is generated as current flows through the contact. In addition, the voltage drop across the contact grows larger as contact resistance increases, diminishing the actual load voltage. A lower contact resistance improves efficiency and reduces heat generation, allowing a smaller heatsink to be used, which in turn, conserves space and cost.

Under certain circumstances, contact-making or breaking under load can cause an electric spark. The super high temperature of these arcs can cause damage to the contact layers, causing other contaminants or particles near the point of contact to burn or disintegrate. During severe arcing, the contacts may even weld together, leading to a short, a dangerous condition that can lead to damage to surrounding circuits.

For best performance and long lifespan, modern contact tips can either be made from silver-based alloys or specially coated. When used as contact material, silver-based alloys have low contact resistance and reduce the potential of contact arcing. The characteristics of commonly used contact materials are listed in the following table.

Ag (fine silver)
  • Highest thermal and electrical conductivity among all metals
  • Exhibits low contact resistance, is inexpensive, and is widely used
  • Contacts tarnish easily through sulphuration influence
AgCu (silver copper)
  • Better wear resistance than Ag and less tendency to arc and weld, but have slightly higher contact resistance.
AgCdO (silver cadmium oxide)
  • Very little tendency to arc and weld, good wear resistance, and arc extinguishing properties
AgW (silver tungsten)
  • Hardness and melting point are high, and arc resistance is excellent
  • High contact pressure is needed to reduce resistance
  • Contact resistance is relatively high, and corrosion resistance is poor
AgNi (silver nickel)
  • Equals the electrical conductivity of silver and has excellent arc resistance
AgPd (silver palladium)
  • Low contact wear with high hardness, but expensive
Platinum, Gold, and Silver Alloys
  • Superb corrosion resistance, but primarily used for low-current circuits

Relays

Shop our wide variety of G9KA Power Relays by Omron.

Shop Now


Don't forget to take our poll.

Omron G9KA Relays

Omron G9KA series relays are AC-power, PCB relays designed for high power applications in the energy market, one example being PV inverters. They use a unique contact material that accommodates a maximum of 800VAC, with a 200A high current breaking capability, while keeping heat generation to a minimum due to a twin contact design and a low contact resistance of 0.2mΩ.  Reducing contact resistance and shunting the current through two contacts can suppress heat generation up to roughly 30%, even with high loads. The low contact resistance is maintained over the lifetime of the relay. G9KA series relays are available in a compact and low-profile package of 51mm x 51mm x 42.7mm.

Omron G9KA

Figure 3: Omron G9KA
 Buy Now

Figure 4 illustrates how heat generation can be reduced by using a twin contact configuration vs a single contact configuration. Instead of 200A going through a single contact, the current is dispersed through two contacts, each one carrying half the current. The equations in Figure 4 demonstrate how heat generation is halved with a twin contact configuration.

Heat Generation Single vs Twin Contact

Figure 4: Comparison of Heat Generation between Single Contact and Twin Contact configurations 
Source: Omron

Figure 5 depicts the results of a temperature rise simulation comparing two relays, a G9KA Series relay and a relay with higher contact resistance. The testing setup consisted of the relay and a terminal block, cooled by a fan, duct, and heat sinks. The simulation was performed at a 200A carry current. The results show that contact resistance clearly has a measurable effect in reducing heat stress.

Temperature rise simulation

Figure 5: Temperature rise simulation comparing contact resistance in relays
Source: Omron

For more information on the Omron G9KA, check out element14's webinar on the G9KA.

Summing up: Maximizing Efficiency in Renewable Energy

in partnership with

logo

One of the biggest challenges with renewable energy is efficiency; how to make the most of the energy that is generated. Several factors can contribute to energy loss, one of which is heat generation in the power inverter. Relays play an important role in inverters; however, they can be a source of heat. To help improve efficiency in inverters, Omron has created the G9KA series of high power relays, which improve efficiency by reducing the amount of heat generated as current passes through the contacts. To this end, the G9KA series features ultra-low contact resistance and a twin contact design, both of which minimize the generation of heat in power applications.  

  • contact resistance
  • omron
  • tech spotlight
  • AC power
  • g9ka
  • inverter
  • dc power
  • renewable
  • power
  • summer of green technology
  • solar
  • high power
  • relay
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • 1Patriot
    1Patriot over 3 years ago

    The issues with many of the renewable sources is the reliability factor.

    Everyone looks at a single source for power, even those off-grid have this shortcoming at times.

    I myself tend to rely on my battery bank, but have managed quite well with only 600Ah operating our 30A rig, but I refuse to, "put all my eggs in one basket", as they say.

    Instead of relying solely on my 750W of solar, I hybrid my system with a 100W wind turbine, which can easily be re-engineered for hydropower, if available, or even geared and belted to a bicycle to help keep some fitness running.

    (Yes, they have low voltage water heating elements which can heat water after the bank is full, but my next project is to attempt to run black ABS to snake below the PV cell, and use several check valves to help move the water without using electrical power, while increasing efficiency by cooling the panels and diverting the heated water through holding tanks, or use during the evening hours. (Also can be set to reverse as to heat the panels and melt any accumulated snow if run underground to use/abuse geothermal storage options for the heat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago in reply to ralphjy

    The systems we built would get the water close to boiling temperature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to ralphjy

    I can well imagine but you could perhaps also use anti-scald valves to prevent the super hot stored water from reaching the user by mixing with cold water. I think they are starting to be fitted as standard these days.

    I was in much colder climes and even there the pipes could quickly get too hot to touch with mid-day sun. Unfortunately there were no Arduinos in those days to allow you to easily log temperatures reached throughout the day/year to monitor the system performance.

    I guess you could switch in and out additional tanks if you wanted to regulate the maximum stored heat without wasting the potential to collect energy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 4 years ago in reply to beacon_dave

    Also needed to inhibit circulation if the inner tank sensor was above the set point.  I never measured the temperature, but in full sun the water was super HOT!.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to ralphjy

    The system I grew up with had a basic differential temperature controller connected to two temperature sensors. One was located in one of the solar panels outside and the other on the side of the hot water cylinder. Once the outer panel sensor was showing around 3degC above the inner tank sensor, the circulation pump turned on and circulated the water around the panels and then back through a standard copper heating coil in the hot water cylinder.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 4 years ago in reply to beacon_dave

    My parents put a two panel solar water heating system on their house roof back in the 90’s.  It was attached to 50 gallon electric water heater with a special controller that managed the circulation.  Seemed like the only power required was to run the circulation pump, but this was in Hawaii Relaxed.

    It started having problems after about 20 years (both the heater and the controller).  The company that had installed it and the manufacturer were both no longer in business, so I put in a conventional water heater.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to ralphjy

    I was thinking the same but after looking up the size of a typical 10kl water tank and it's the sort of thing that an architect could perhaps design into the foundations of a new house at a relatively low cost. No insulated outhouse required either.

    The windmill might be more of an issue however. Although if the construction of the roof was designed to as a solar collector then might be an option. Orientation of the roof could be aligned to maximise solar collection as well.

    Back in the 80's I recall some experimental housing estates that incorporated solar heating systems and thermal insulation into the architectural design, however it doesn't appear to have been adopted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to dougw

    It seemed to be a lot more popular in the 80's. I grew up in a house retrofitted  with a small solar water heating system. A solar cylinder heated by five roof-mounted panels fed the existing hot water cylinder to preheat the water reducing the heat input required from a gas boiler. 

    Even with that small set-up, if you adjusted your life style a bit to spread the demand for hot water over the day, you could potentially run off of solar alone for hot water during the summer months.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 4 years ago in reply to michaelkellett

    Water storage is interesting, but would not be possible for individual homes in the suburban area where I live.  Or maybe I should say not practical due to our small lot sizes.  I actually don’t know if our city code would allow it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago in reply to michaelkellett

    Hot water is a great way to store energy inexpensively as michaelkellett points out. We built several big systems in the 80's that used (liquid) solar panels to heat the water and learned there can be lots of issues, but it is easy to collect enough heat to keep the whole tank hot, even in winter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>