Learning Center
  • Learn
  • More
Learning Center
Documents Capacitive Touch Tutorial from James Lewis - Bald Engineer
  • Blog
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Learning Center to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 20 Jun 2018 6:58 PM Date Created
  • Last Updated Last Updated: 27 Jun 2018 6:17 PM
  • Views 4630 views
  • Likes 18 likes
  • Comments 12 comments
Related
Recommended

Capacitive Touch Tutorial from James Lewis - Bald Engineer

image
A Capacitive Touch Tutorial

Bald Engineer's VCP Profile  |  Online Learning

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Prepare to drink from the firehose!  James opens this video with:

"Push buttons do not work without pull-up or pull-down resistors."

 

But what if you what a button without a physical button?

If you need a brush-up on Pull-up resistors,

check out this AddOhms Tutorial (also done by James).

link to here

In this video you'll learn about capacitors.

Capacitors are, at their most basic, two conductive electrode plates separated by a non-conductive dielectric.

 

An electric field forms between the plates. Different dielectric materials change how much charge can be stored in that field.

 

image

 

A dielectric (or dielectric material) is an electrical insulator that can be polarized by an applied electric field.

In this video you'll learn about:

  • the variables to consider in defining capacitance
  • the equation for defining capacitance
  • how to measure capacitance in a circuit
  • and what is different about capacitance when designing with capacitive touch.

 

James rounds out the video with a review of the TI CapTIvate Dev KitTI CapTIvate Dev Kit - which TI sent him to review.

 

Have more questions on capacitance or the Texas Instruments kit?  Ask them in the comments below!

baldengineer

  • capacitve touch
  • e14presents_baldengineer
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 8 years ago +2
    Very clear explanation and well done tutorial. Good good ! Enrico
  • Workshopshed
    Workshopshed over 8 years ago +2
    I did like the high quality of the CapTIvate board. Just discovered that the ESP32 supports capacitive sense so will be trying that out.
  • kellyhensen
    kellyhensen over 8 years ago in reply to jc2048 +1
    jc2048 wrote: How does charge get stored in the field between the plates? Don't the electrons put up a bit of a fight if you try and take away their charge? I know, electrons are so negative!
Parents
  • Fred27
    Fred27 over 8 years ago

    A really nice overview video, although I did find the comparison table between self and mutual capacitance wasn't clear - and I'm already familiar with this kit.

     

    You asked viewers to say what they'd use it for. Well, I've just started a custom design for an NFC enabled lock as this is great for initial prototyping. The proximity / guard channel will wake the device up to scan for my NFC implant and also enable a keypad for another way to open the door. I was going to use the simpler capacitive touch features of the CC1310's Sensor Controller, but decided an auxiliary keypad would be useful too. My wife won't let me get the kids chipped. (Only kidding.)

     

    The one thing I found odd about the CAPTIVATE-FR2633 development board is that it's set up to be used as a booster pack for another launchpad. For prototyping I would have found it far more useful if I could have used it as a launchpad and used a TRF7970A booster pack with it. Obviously this is possible with a load of jumper wires, but the pinout is all wrong to just plug them together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 8 years ago

    A really nice overview video, although I did find the comparison table between self and mutual capacitance wasn't clear - and I'm already familiar with this kit.

     

    You asked viewers to say what they'd use it for. Well, I've just started a custom design for an NFC enabled lock as this is great for initial prototyping. The proximity / guard channel will wake the device up to scan for my NFC implant and also enable a keypad for another way to open the door. I was going to use the simpler capacitive touch features of the CC1310's Sensor Controller, but decided an auxiliary keypad would be useful too. My wife won't let me get the kids chipped. (Only kidding.)

     

    The one thing I found odd about the CAPTIVATE-FR2633 development board is that it's set up to be used as a booster pack for another launchpad. For prototyping I would have found it far more useful if I could have used it as a launchpad and used a TRF7970A booster pack with it. Obviously this is possible with a load of jumper wires, but the pinout is all wrong to just plug them together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • baldengineer
    baldengineer over 8 years ago in reply to Fred27

    Fred27  wrote:

     

    although I did find the comparison table between self and mutual capacitance wasn't clear

    In what way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 8 years ago in reply to baldengineer

    I'll watch it again and try to pick it apart. Don't get me wrong, the rest of it is great so I'm trying to be constructively critical of the only bit I thought wasn't as good!

     

    Layout

    I have no idea what "layout is a wash" means. I'm from the UK so it may be obvious to others. When you say "you can use more pins with mutual" it isn't clear if you mean this it takes up more pins for the same number of buttons or if it allows you to use more. (In reality you tend to use less pins for mutual as it's generally used for a matrix layout.)

    Why are the guard bands on mutual stronger?

     

    Pins

    Showing mutual as using 2 pins per pad is a bit misleading without the explanation of using a matrix, which is a not really explained.

    "Mutual has a potential advantage which I'll hit on in a just a second." It isn't clear what this was or when you got to it.

     

    Pads

    Is it correct to describe he mutual pads as interdigitated (i.e. interleaved as when the fingers of one hand are laced between those of the other)? That feels wrong. One pad is inside the other. They are often in a matrix. But I don't see how they're interdigitated. Actually, does interdigitated refer to the slider and scroll wheel designs? I've not used those but the description seems to fit.

    "Interdigited pads make it a wash". Again, I have no idea what this means!

     

    Matrix

    If the test said single touch and multi-touch this would be clearer.

     

     

    I suppose the problem I had with it is the fact that mutual capacitance tends to be linked with multiplexing. Whilst you can multiplex with self capacitance the ghosting issue means you probably shouldn't and won't. That tends to flip around many of the things like mutual using more pins than self. That meant a lot of it was technically correct but felt practically a bit confusing.

     

    All in all though, a good video. I hope these comments were helpful.