Publications
  • Learn
  • More
Publications
Blog 555 v The Microcontroller:
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: pjclarke
  • Date Created: 20 Apr 2011 10:31 AM Date Created
  • Views 1342 views
  • Likes 2 likes
  • Comments 1 comment
  • jeri
  • blogzone
  • contest
  • ellsworth
  • 555
Related
Recommended

555 v The Microcontroller:

pjclarke
pjclarke
20 Apr 2011

To  co-inside with the results of the 555 contest ( 20th April 2011 - 9pm  EST ) I have decided to release what I said I would do. That was to look  at what is better, The 555 Timer IC or a Microcontroller? If you do not  know about the contest then you should head over to the site and see  the great work that's been done and also see what prizes are up on  offer!image

 

 

element14 are proud sponsors of the contest and are giving away a  full copy of the Eagle PCB design tool along side lots of others  including my own firm ebm-papst UK Ltd who are giving away a fluke  meter.

 

Back  at the beginning of the year I was online when Jeri Ellsworth was  hatching the idea of the 555 contest. One of the things that was commented  on was that a Micro could do everything a 555 could, and better. So  over the last few months while everyone has been building there contest  entries I’ve been looking into seeing if a Micro can really out do a  555.

 

I  started off by looking at the LM555 and the NE555 data sheets and  picking out the key features. These were as follows (other ICs may  differ):

 

Supply  voltage of 4.5 to 16 volts, 3mA at 5V, 0-70’C working range, 8 pin and  about 100ns rise / fall time on output capable of 200mA. These devices  also cost between 42p and 62p (UK 1off prices).

 

So  then it came to select a microcontroller - I’m a big fan of Microchip  so had a look at the smallest chips they have. I started with the PIC10  range but after looking at pin outs, the device even when in a 8 pin  package only used 6 pins, so could not match all the pin functions of  the 555.

 

So my final choice was the PIC12F615 that has the following Spec:

 

Supply  2.0 to 5.5 volts, 1.1mA at 5 volts, -40 to 85’C working range, 8 pin  better than 100ns rise / fall response time with 100mA output pin. cost  wise I found the device for around 71p.

 

So  how did it compare - well first off the PIC12F615 is not pin  compatible, so you can’t go swapping out a 555 for a PIC. Its also very  obvious that the working voltage ranges are very different. The 555 is a  good fit for analogue circuits as well at logic 5 volts, but the PIC is  a pure logic device - obviously! While on the supply side of things -  we can see the PIC will draw less current than a standard 555, but I  have found 555s that will work with less current since my initial  selection.

 

Temperature  is always an interesting question with a 555 as they are know to drift  at extremes, however the PIC is much more stable and also has a better  temperature range. You could spec in the SE555 which will match the PIC  on temperatures, but then PIC could always play the +125’C card and  still out do it.

 

Functional  wise the PIC worked really well and I got almost identical results from  the standard circuits show in the data sheets. This was a Monostable  with a 1ms output and a astable of 1kHz and 75% duty. In fact at 5volts  there was nothing to select between them. However the PIC took  programming time and is consumed with just doing this role. Also I felt  the ADC inputs would not as sensitive as the comparators in the 555’s as  I was only seeing +/- 19mV steps.

 

I  then for may last tasked asked myself, could I use my PIC12F615 in the  projects I have seen entered in the 555 contest. To be honest I’d have  to say no. Why? well the voltage the PIC can work at just did not match  that of some of the entries, its not sensitive in my view and its more  expensive and difficult to use as you have to generate code.

 

Therefore  I can say that Jeri was 100% right in saying that the 555 can not be  replaced by a microcontroller. Yes you could in some cases and it may  even be better in some cases but on the whole there is no real reason to  use anything other than a 555 Timer IC.

 

I've not seen the results of the contest at the time of writting this blog post - but want to wish everyone the best of luck and to say that the entries have all been really good.! They have been great to look at and have given me lots of ideas for project os my own. Well done!

  • Sign in to reply
Parents
  • fustini
    fustini over 15 years ago

    Another advantage of the 555 is that it can go down to 1V in the 551 variant.  Not too shabby.  It makes applications like the Drawdio possible which uses 1 AAA.

     

    However, someone on the #fmcg channel on freenode pointed out that TI's 16-bit uC, the MSP430, will go as low as 1.8V.  It can even run off grapes.  However, keeping with Paul's theme, 555 still beats microcontrollers on the high and low end of operating voltage.

     

    Cheers,

    Drew

    http://twitter.com/pdp7

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fustini
    fustini over 15 years ago

    Another advantage of the 555 is that it can go down to 1V in the 551 variant.  Not too shabby.  It makes applications like the Drawdio possible which uses 1 AAA.

     

    However, someone on the #fmcg channel on freenode pointed out that TI's 16-bit uC, the MSP430, will go as low as 1.8V.  It can even run off grapes.  However, keeping with Paul's theme, 555 still beats microcontrollers on the high and low end of operating voltage.

     

    Cheers,

    Drew

    http://twitter.com/pdp7

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data