Publications
  • Learn
  • More
Publications
Blog Artificial cerebellum successfully used in rats
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 29 Sep 2011 8:28 PM Date Created
  • Views 449 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • eavesdropper:dit
  • hmi
  • medtronic
  • robotics
  • robot
  • on_campus
  • measurement
  • university
  • medical
  • technology_for_the_disabled
  • innovation
  • communication
Related
Recommended

Artificial cerebellum successfully used in rats

Eavesdropper
Eavesdropper
29 Sep 2011
image
 
At the University of Tel Aviv, Matti Mintz with a team has constructed a digital cerebellum that restored motor function in rats. Working with Robert Prueckl of Guger Technologies in Graz, Austria, Mintz analyzed brainstem signals both feeding in and out of a real cerebellum. Using this base data, the team constructed a synthetic version housed outside the rat's skull, electrodes on the brain relay the digital signals.
 
One of the cerebellum's functions is motor control. The goal was to replicate one such reflex. The test setup  was a rat that had its cerebellum disabled. They tried to teach the rat a conditioned response to an audio sound, by puffing air into the rat's eye. When the sound is heard, a normal rat would blink. The disabled one did not blink to the sound. Once the artificial system was connected to the rat, it would then blink to the sound after being conditioned as in normal rats.
 
Prueckl's next step with the system is software tuned to filter out noise, improved electrode connections, mapping of a larger area of the cerebellum, and embedding the chip below the skull. In particular, to teach an animal a series of movements to greater challenge the system.
 
This is the first step towards a digital replacement of failing brain functions. Alternatively, full external control over someone's movement is also on the way. The tech sounds on the cusp of a science fiction "cyberpunk" type upgrade for the human body. Perhaps a better connection to the rat's cerebellum would come from the recent proton transistor discovery.
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    This effort reminds me of the research done in the 1970's where they had inserted wires directly into a rats brain and were able to control its movements.  I also think there was a report where someone had taken a rat brain and linked it to a robot via wires to do some simple food finding tasks.

     

    I agree about the Proton interface.  They may be able to access a lot more aspects about the physiology, which could have usefulness in dealing with paralized or disabled people.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    Dab,

     

    Thanks for pointing thins out. I will have to do some research on the rat brain control.

    image

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    Dab,

     

    Thanks for pointing thins out. I will have to do some research on the rat brain control.

    image

    E