Publications
  • Learn
  • More
Publications
Blog chipKIT MAX32 product review - Arduino clone?
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: pjclarke
  • Date Created: 29 Jun 2011 9:36 AM Date Created
  • Views 687 views
  • Likes 4 likes
  • Comments 3 comments
  • microchip
  • blogzone
  • chipkit
  • digilent
Related
Recommended

chipKIT MAX32 product review - Arduino clone?

pjclarke
pjclarke
29 Jun 2011

I’ve  been a big fan of Microchip PICs for some time now, possible because I  use them everyday at ebmpapst. My passion for them seams to have not gone on  noticed as Microchip have supplied me we the latested Arduino clone or  look a like - The chipKIT Max 32. However Microchip have been a bit hit  or miss with development kits so I was intrigued to see how well this  would stand up to review especially as they are not developed by  themselves but by Digilent.image

 

The  two new boards which are avalible are the UNO32 which is aimed at being  the alternative to the Arduino UNO and the MAX32 which is up against  the Arduino Mega2560. The boards follow the exact same board profile pin  layout and connector pitch making Shields designed for the Arduinos fit  the new chipKITs. The main selling point as I see it however is that  the chipKIT boast a 32bit microcontroller making them a lot faster than  standard Arduino clones.

 

image

Out  the box you get nothing more than the board and a few instruction on  the box - so having a original Arduino UNO at home I decided to compare  and see if the chipKIT is a true clone?

 

First  off is the USB connector, this may be a fuss about nothing but the new  chipKIT has the much smaller USB socket than is used on the Arduino. So I  first had to find my camera cable to plug it in. So after plugging it  in I then wondered off to get the new IDE you need. This is because the  standard Arduino IDE will not support the chipKIT, BUT the new IDE is  fully backward compatible and looks and feels 100% the same so you will  instantly feel at home with it. I am interested to see if Microchip and  or Digilent have a nice talk with Arduino and get themselves on the next  IDE release - otherwise I can see two IDEs running along side each  other.

 

Downloading  the IDE was not a fluid as I’d hoped. The key thing for me is that the  files are not on the Microchip site - who are helping to push this  product - but are sort of out the back door and round the corner from the  Digilent site. One of the downloads gives a error 404 file not found  which can’t inspire confidence in me. I would have liked to see Microchip have  a better support page with lots of Digilent logos to support them too.

 

Keeping  the coding till last I next looked at the physical hardware closer. All  is pretty good I have to say, well built and very well labeled up with  whats what on the board. There are two sets of jumpers, one that allow  you to select the power input, bypassing the regulator allowing a higher  voltage to the power connector. The other is to allow putting the PIC32  into either master or slave SPI mode due to a little pin shuffling  that's required. Both are good however the links stand taller than the  connectors around the outside of the board. So plugging in a shield is  not going to go home fully and solid. It may only be millimeters but  still a design oversight in my view.

 

On  the subject of shields then I have found that the community have been  having problems - the chipKIT is not claiming to be 100% compatible and  that's because its not. Some of the pin mapping from what I have read  manes that some shields will not work. My advice is to visit the chipKIT  community - which is very good - and check for compatibility. There is  also no Ethernet shield available (at the time of writing this) but  Digilent are designing one that is chipKIT compatible. That I think will  disappoint some and the other for me was that there is nowhere to fit a  32kHz crystal so I could use the already on chip RTCC and last of all, why is  the ICSP socket (not fitted) have staggered holes?

 

Dispite  these minor annoying design features shall we say - I still like the  board a lot and think there are going to be a lot of people who will buy  these over the Arduino. On reason is price - the chipKIT board comes in  under the cost or the original Arduino boards and also less than some of  the clones. The difference is not massive but its there.

 

Running  code on the board I have to say is really simple - in fact I’ve written  so little because it works so well. From my own experience I was able  to write code for my Arduino, run and test - then swap boards and  without fault the same code runs on the chipKIT. From reading the  community pages I found people running tests of the speed difference of  the to boards. This seamed the best comparison to me to show you; its  quite simply toggling a pin as fast as possible. The Arduino UNO was  able to generate a frequency of 120kHz and the UNO32 clocked up 628kHz,  that's around six times faster.

 

Personally  I like the new chipKIT but I don't see it as a 100% replacement for the  Arduino clones. For me when you bring out a product designed to compete  with another, unless your 100% compatible then you will always be  compared for your failings. I do feel the chipKIT has features above  that of the Arduino however. Maybe if it was not so close to the design of the Arduino, like  comparing mbed to Arduino, then I would not be picking up on small  point above.

 

So  if you are considering which was to go - then good luck and there are  lots of pro and cons in both camps. For me and looking at the cost - I’d  buy both!

 

Thanks
Paul - aka @monpjc

  • Sign in to reply
Parents
  • awinning
    awinning over 14 years ago

    Cheers Paul, a really good read. I don't think the ChipKIT is designed to work with any existing shields other than the 3.3V ones and AFAIK you will still have to check the copatibility. I do fancy getting myself a ChipKIT to mess around with.


    Ally

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • awinning
    awinning over 14 years ago

    Cheers Paul, a really good read. I don't think the ChipKIT is designed to work with any existing shields other than the 3.3V ones and AFAIK you will still have to check the copatibility. I do fancy getting myself a ChipKIT to mess around with.


    Ally