Publications
  • Learn
  • More
Publications
Blog Chirps – Modelling the Spectral Components of Signals Whose Frequency Is Changing
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 29 Oct 2011 5:04 PM Date Created
  • Views 1009 views
  • Likes 1 like
  • Comments 4 comments
  • cgervasi:dit
  • dsp
Related
Recommended

Chirps – Modelling the Spectral Components of Signals Whose Frequency Is Changing

gervasi
gervasi
29 Oct 2011

People who have had a class on DSP or Signals and Systems are aware that any signal can be broken down into a sum of sinusoids of various amplitudes and frequencies.  The Fourier Transform (FT) can break down a signal into its frequency-domain spectral components.  The FT is typically run on a short window of data within which the signal is stationary, i.e. its statistical parameters are not changing.  An example is a speech recognition algorithm analyzing a few milliseconds of a speech phoneme to work out which vowel sound it is.  The window being analyzed must be short enough that the vowel sound and the spectral components present are not changing during the window.  image


What if the frequency of a spectral component is continuously varying over time?  (The signal to the right is an example.)  For example, consider the sound of a siren passing by.  The Doppler shift decreases slowly to zero when the siren is beside you.  Then it increases in the other direction as the siren moves away.  

image

Doppler-Shifted Frequency of a Siren at Locations Around It


You need a long window of time for the FT to provide good resolution in the frequency domain.  But the longer the window, the more time the frequency components have time to change.  Resolution in frequency and resolution in time always come at the other's expense.  Models that provide an instantaneous frequency as a function of time attempt to get around this uncertainty principle.  This was the subject of the talk Dr. Patrick Flandrin's gave to my local section of the IEEE yesterday.  

 

It turns out these continuously varying signals are ubiquitous in nature and engineering problems.  An interesting example is a bat's echolocation.

(Time is on the horizontal axis.  Frequency is on the vertical axis.)

image

When the bat is scanning the environment, its sonar signals' frequency is constant for much of the time.  This allows it get good speed information by looking at the Doppler shift in the echos.  When it is catching its prey, it sends out short burst of broad spectrum sound. The echos from these signals are good at determining distance but not Doppler shift.  There is an intermediate pursuit period during which the bat emits chirp signals whose frequency vs. time graph is a hyperbola.  The mathematics work out such that this allows the bat to get a balance of some speed information and some position information.   It's amazing that such a complicated system came about through selective pressures.   image


 

The IEEE Distinguished Lecturer program provides funding for local sections of IEEE to get esteemed event speakers.  If you want more details on chirps, you local IEEE section may be able to get Dr. Flandrin to visit and give a talk in your area.   You can also download his Chirps Everywhere talk and other talks from his website. 

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Very interesting.

     

    I would have thought that the frequency would increase as the bat got closer to get more rapid updates.  Clearly the sound processing inside the bat has some unique capabilities.

     

    Thank you for bringing this discussiion to the group.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    Very interesting.

     

    I would have thought that the frequency would increase as the bat got closer to get more rapid updates.  Clearly the sound processing inside the bat has some unique capabilities.

     

    Thank you for bringing this discussiion to the group.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • gervasi
    gervasi over 14 years ago in reply to DAB

    I understand why a steady tone works best for Doppler: it can just look at the frequency shift and disregard time.  I understand why it needs short bursts for ranging.  I'm not as clear why those short bursts have to be widespectrum, unless it's just the fact that a very short impulse in the time domain looks like the sinc function (sin x / x) in the frequency domain.  The approach during the pursuit phase of transmitting a tone whose frequency changes with time according to a hyperbolic curve gives distance and speed info, as far as I understand, because a Doppler shift sort-of rotates upward or downward the echo's freq vs time graph.  This rotation is independent of the delay, so it gets a good value for distance and speed.  What I'm not clear on is why the bat can't transmit a steady high-pitch tone (as you suggest) for only a few oscillation periods, long enough to get meaningful Doppler shift info but not so long that it doesn't get good distance info.

     

    It's funny that I'm talking about hypothetical waveforms a bat could transmit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago in reply to gervasi

    If you really want to blow your mind, look into how the Sperm Whale uses its oil filled head to generate a huge amount of low frequency sound through the water.  When I first saw the numbers I did not believe that any animal could generate that much energy.

     

    It would be a good research project for someone to look at the chirps produced by Bats and those produced by whales.  I suspect that there might be some coincidental use of technique at different frequencies.  Both are trying to accomplish the same task, just in different environments.

     

    Just a thought.

    DAB